This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0218 [03 Nov 2017 05:05] – update Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0218 [03 Jan 2021 21:56] – fix links Robin Getz | ||
---|---|---|---|
Line 15: | Line 15: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp:// | * [[ftp:// | ||
* Power Supply | * Power Supply | ||
Line 29: | Line 29: | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
{{ : | {{ : | ||
- | * The [[http:// | + | * The [[adi>EVAL-CN0150-SDPZ|EVAL-CN0150-SDPZ]] **(CN-0150 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* Terminal block **J1** is the SDP connector | * Terminal block **J1** is the SDP connector | ||
* Terminal block **J2** is the +6 V barrel connector for wall wart supply input | * Terminal block **J2** is the +6 V barrel connector for wall wart supply input | ||
Line 42: | Line 42: | ||
{{ : | {{ : | ||
- | - Connect the 120-pin connector on the [[adi> | + | - Connect the 120-pin connector on the [[adi> |
- Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above | - Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above | ||
- With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | ||
Line 53: | Line 53: | ||
\\ | \\ | ||
<WRAP center round important 60%> | <WRAP center round important 60%> | ||
- | Do **not** connect | + | Connect the **system ground** and the **PCB isolated ground** |
</ | </ | ||
\\ | \\ | ||
Line 61: | Line 61: | ||
- Click **Next** to view the installation review page\\ \\ {{: | - Click **Next** to view the installation review page\\ \\ {{: | ||
- Click **Next** to start the installation\\ \\ {{: | - Click **Next** to start the installation\\ \\ {{: | ||
- | - Upon completion of the installation of the **CN-0188 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%> | + | - Upon completion of the installation of the **CN-0218 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%> |
- Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: | - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: | ||
- Press **“Install”** to install the **SDP Drivers** and complete the installation of all software. | - Press **“Install”** to install the **SDP Drivers** and complete the installation of all software. | ||
Line 67: | Line 67: | ||
---- | ---- | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
- | ====Test Setup Tab==== | + | ==== Main Window |
- | {{ : | + | {{ : |
- | | + | - **Connect** Button - Starts the connection between the [[ADI> |
+ | - **Reset and Disconnect** - Resets the board and ends the connection between the [[ADI> | ||
+ | - **Stop** Button - Stop collecting data from the CN0218 Board | ||
+ | - **Test Setup** Tab - Shows the acquired measurement data in terms of shunt voltage with respect to the samples\\ {{ : | ||
+ | * **Shunt Voltage** - Shunt voltage measurement output from ADC | ||
+ | * **Click to Start Sampling** - Starts acquisition of measurement data | ||
+ | * **Clear Data** - Clear all data collected from the chart history | ||
+ | * **Save Data to File** - Save measurement data to file | ||
+ | | ||
+ | * **Flash LED** - Flashes the LED on the SDP controller board | ||
+ | * **Read Firmware** - Reads the firmware of CN0218 Evaluation Board | ||
+ | - **Plot** Options - Edit plot display and options like interpolation and color of output waveform \\ {{ : | ||
\\ | \\ | ||
+ | ==== Running the System ==== | ||
+ | -Open the CN0218.exe application from the default installation location | ||
+ | -Click the Connect Button | ||
+ | -Upon successful connection, start and control data acquisition through the data acquisition control buttons | ||
+ | -Output data will be shown in the graph. Edit graph through plot options and check boxes provided | ||
+ | -Click Disconnect if finished | ||
+ | -Click Quit to exit the program | ||
---- | ---- | ||
Line 77: | Line 95: | ||
* [[ftp:// | * [[ftp:// | ||
* [[ADI> | * [[ADI> | ||
- | * [[http:// | + | * [[adi>media/ |
* [[ADI> | * [[ADI> | ||
* [[ADI> | * [[ADI> | ||
Line 87: | Line 105: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>media/ |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout |