This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0216 [12 Mar 2013 16:56] – created James Fitzgerald | resources:eval:user-guides:circuits-from-the-lab:cn0216 [15 Feb 2022 05:08] (current) – [Schematic, PCB Layout, Bill of Materials] erbe reyta | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== CN-0216 Software User Guide====== | ||
+ | ===== Overview ===== | ||
+ | [[adi> | ||
+ | Ultralow noise, low offset voltage, and low drift amplifiers are used at the front end for amplification of the low-level signal from the load cell. The circuit yields 15.3 bit noise-free code resolution for a load cell with a full-scale output of 10 mV. | ||
+ | |||
+ | This circuit allows great flexibility in designing a custom low-level signal conditioning front end that gives the user the ability to easily optimize the overall transfer function of the combined sensor-amplifier-converter circuit. The [[adi> | ||
+ | |||
+ | This user guide will discuss how to use the evaluation software to collect data from the [[adi> | ||
+ | |||
+ | {{: | ||
+ | ===== Required Equipment ===== | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[ftp:// | ||
+ | |||
+ | * PC with the following //Minimum Requirements// | ||
+ | * Windows XP Service Pack 2 (32-bit) | ||
+ | * USB type A Port | ||
+ | * Processor rated at 1GHz or faster | ||
+ | * 512 MB RAM and 500 MB available hard disk space | ||
+ | * USB type A to USB type mini-B cable | ||
+ | * Tedeah Huntleigh Model 1042 Load Cell | ||
+ | <WRAP round info 60%>\\ **__NOTE__** - Any 4 or 6 wire load cells can be used with the **CN-0216 Board**.\\ This guide was written with the Tedeah Huntleigh Model 1042 in mind. | ||
+ | </ | ||
+ | |||
+ | ===== General Setup ===== | ||
+ | * The [[adi> | ||
+ | * The [[adi> | ||
+ | * The [[adi> | ||
+ | * The Tedeah Huntleigh Model 1042 load cell connects to the [[adi> | ||
+ | {{: | ||
+ | ---- | ||
+ | ===== Installing the Software ===== | ||
+ | - Extract the file **CN0216 Eval Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> | ||
+ | - Click **Next** to view the installation review page\\ \\ {{: | ||
+ | - Click **Next** to start the installation\\ \\ {{: | ||
+ | - Upon completion of the installation of the **CN0216 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%> | ||
+ | - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: | ||
+ | - Press **“Next”** to install the **SDP Drivers** and complete the installation of all software. | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== Connecting the Hardware ===== | ||
+ | - Connect the **Tedeah-Huntleigh (Model 1042)** Load Cell to **8-pin header** of the [[adi> | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== Using the Evaluation Software ===== | ||
+ | ==== Software Control and Indicator Descriptions ==== | ||
+ | {{: | ||
+ | {{: | ||
+ | -**Connect/ | ||
+ | * When this button is pressed, the SDP-B Board makes a USB connection to the CN-0216 Board. | ||
+ | -**Run Button** | ||
+ | * When this button is pressed, the SDP-B Board will collect conversion data and present the acquisitions in the chart. | ||
+ | -**Stop Button** | ||
+ | * When this button is pressed, the software stop collecting data from the CN-0216 Board | ||
+ | -**Clear Chart Button** | ||
+ | * When this button is pressed, the software will clear all data collected from the chart history. | ||
+ | -**Control Tabs** | ||
+ | * __Main__ - Clicking this tab brings the data collection chart to the front. | ||
+ | * __Calibrate System__ - Clicking this tab bring the system configuration settings to the front. | ||
+ | -**Current Weight Numerical Indicator** | ||
+ | * This indicator displays the mass (in grams) on the load cell. | ||
+ | -**Chart Controls** | ||
+ | * These controls allow the user to zoom-in, zoom-out, and pan through the data collected. | ||
+ | -**Select Units Radio Buttons** | ||
+ | * This control determines the Y-Axis units of the data displayed in the chart. | ||
+ | -**System Status String Indicator** | ||
+ | * This indicator displays a message to the user detailing the current state of the software. | ||
+ | -**System Status LED Indicator** | ||
+ | * This indicator displays the current state of the software in the form of an LED. There are three status LED colors.\\ {{: | ||
+ | -**Calibration Weight Numerical Control** | ||
+ | * Set this control to the weight of the object used to calibrate the load cell. | ||
+ | -**Calibrate Button** | ||
+ | * Pressing this button initiates the calibration of the load cell. | ||
+ | -**ADC Mode Radio Buttons** | ||
+ | * This control is used to set the mode of the [[adi> | ||
+ | * __Buffered Mode__ - Selecting this mode turns the on-chip analog input channel buffer of the [[adi> | ||
+ | * __Unbuffered Mode__ - Selecting this radio button turns the on-chip analog input channel buffer of the [[adi> | ||
+ | -**ADC Channel Select Radio Buttons** | ||
+ | * This control is used to select the analog input channel of the [[adi> | ||
+ | * __AIN(+)-AIN(-)__ - Selecting this radio button allows for normal operation of the [[adi> | ||
+ | * __AIN(-)-AIN(-)__ - Selecting this radio button shorts the analog input channels of the [[adi> | ||
+ | * __Vdd Monitor__ - Selecting this radio button monitors the voltage applied to the Vdd pin of the [[adi> | ||
+ | -**Update Rate Radio Buttons** | ||
+ | * This control is used to change the output word rate of the [[adi> | ||
+ | -**Configure ADC Button** | ||
+ | * When this button is pressed the current value of the **ADC Mode Radio Buttons**, **ADC Channel Select Radio Buttons**, and **Update Rate Radio Buttons** are used to configure the [[adi> | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ==== Establishing a USB Connection Link ==== | ||
+ | - Follow the instructions to properly install the software and connect the hardware as described in the previous sections. | ||
+ | - Open the file named **CN0216.exe** in the installation directory.\\ \\ <WRAP left info round box 60%> | ||
+ | - Click the **Connect/ | ||
+ | - Upon success, the **System Status String Indicator** will display __SDP Board Ready to Acquire Data__ | ||
+ | ==== Capturing Data ==== | ||
+ | - **Establish a USB Connection Link**. | ||
+ | - Click the **Run Button** | ||
+ | - Click the **Stop Button** when acquisition is complete. | ||
+ | ==== Calibrating the Load Cell ==== | ||
+ | - **Establish a USB Connection Link**. | ||
+ | - Click the **Calibrate System Control Tab**. | ||
+ | - Set the **Calibration Weight Numerical Control** to the weight (in grams) of the weight to be used for calibration. | ||
+ | - Place the calibration weight on the Load Cell. | ||
+ | - Click the **Calibrate Button** and Wait for calibration to complete.\\ \\ {{: | ||
+ | - Remove the calibration weight when prompted to do so.\\ \\ {{: | ||
+ | - Click the **Continue Button**. | ||
+ | - Wait for calibration to complete.\\ \\ {{: | ||
+ | |||
+ | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | |||
+ | {{ : | ||
+ | * Schematics | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * Gerber Files | ||
+ | * Allegro/ | ||
+ | </ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | |||
+ | |||
+ | // End of document // |