Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:circuits-from-the-lab:cn0203 [25 Jul 2017 04:52] – Angelo Nikko Catapang | resources:eval:user-guides:circuits-from-the-lab:cn0203 [30 Jul 2021 07:20] (current) – Victor Calinao, Jr |
---|
The [[ADI>AD5750-1]] are single-channel, low cost, precision voltage/current output drivers developed to meet the requirements of industrial process control applications. The voltage output range can be programmed for the standard output ranges for PLC and DCS applications: 0 V to 5 V, 0 V to 10 V, −5 V to +5 V, and −10 V to +10 V. A 20% overrange setting is also provided for the standard ranges, giving the following options: 0 V to 6 V, 0 V to 12 V, −6 V to +6 V, and −12 V to +12 V. The current output, which is provided on a separate pin, can be programmed for the ranges of 4 mA to 20 mA, 0 mA to 20 mA, −20 mA to +20 mA, 0 mA to 24 mA, and −24 mA to +24 mA. The unipolar ranges have a 2% overrange setting. The voltage and current output pins can be tied together to configure the end system as a single-channel output if desired. | The [[ADI>AD5750-1]] are single-channel, low cost, precision voltage/current output drivers developed to meet the requirements of industrial process control applications. The voltage output range can be programmed for the standard output ranges for PLC and DCS applications: 0 V to 5 V, 0 V to 10 V, −5 V to +5 V, and −10 V to +10 V. A 20% overrange setting is also provided for the standard ranges, giving the following options: 0 V to 6 V, 0 V to 12 V, −6 V to +6 V, and −12 V to +12 V. The current output, which is provided on a separate pin, can be programmed for the ranges of 4 mA to 20 mA, 0 mA to 20 mA, −20 mA to +20 mA, 0 mA to 24 mA, and −24 mA to +24 mA. The unipolar ranges have a 2% overrange setting. The voltage and current output pins can be tied together to configure the end system as a single-channel output if desired. |
| |
The [[ADI>AD5660-1]] is a single channel, low cost, low power, rail-torail voltage buffered output nanoDAC integrated with an onchip 1.25 V, 5 ppm/°C reference. The [[ADI>AD5660-1]] incorporates a power-on reset circuit to ensure that the DAC output powers up to 0 V and remains there until a valid write command takes place. | The [[ADI>AD5660|AD5660-1]] is a single channel, low cost, low power, rail-torail voltage buffered output nanoDAC integrated with an onchip 1.25 V, 5 ppm/°C reference. The [[ADI>AD5660|AD5660-1]] incorporates a power-on reset circuit to ensure that the DAC output powers up to 0 V and remains there until a valid write command takes place. |
The output voltage range of the [[ADI>AD5660-1]] is 0 V to 2.5 V, which matches the input range of the [[ADI>AD5750-1]]. In addition, the reference output voltage of the [[ADI>AD5660-1]] is 1.25 V, which precisely matches the reference input requirement of the [[ADI>AD5750-1]]. | The output voltage range of the [[ADI>AD5660|AD5660-1]] is 0 V to 2.5 V, which matches the input range of the [[ADI>AD5750-1]]. In addition, the reference output voltage of the [[ADI>AD5660|AD5660-1]] is 1.25 V, which precisely matches the reference input requirement of the [[ADI>AD5750-1]]. |
| |
The [[ADI>CN0203]] needs +15 V, -15 V and +6 V power supply inputs and thus, needs a triple output DC power supply. The board also connects to a ADI's System Demonstration Platform (**SDP**). | The [[ADI>CN0203]] needs +15 V, -15 V and +6 V power supply inputs and thus, needs a triple output DC power supply. The board also connects to ADI's System Demonstration Platform (**SDP**). |
| |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0203:cn0203-hw-1024.jpg?nolink&600 |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0203:cn0203-hw-1024.jpg?nolink&600 |}} |
| |
---- | ---- |
| |
==== Required Equipment ==== | ===== Required Equipment ===== |
* [[ADI>CN0203|EVAL-CN0203-SDPZ Evaluation Board]] | * [[ADI>CN0203|EVAL-CN0203-SDPZ Evaluation Board]] |
* [[ADI>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z Controller Board (**SDP-B Board**)]] | * [[ADI>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z Controller Board (SDP-B Board)]] |
* [[ftp://ftp.analog.com/pub/cftl/CN0203/CN0203%20SDP%20Eval%20Software.zip|CN0203 Evaluation Software]] | * [[ftp://ftp.analog.com/pub/cftl/CN0203/CN0203%20SDP%20Eval%20Software.zip|CN0203 Evaluation Software]] |
* ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**) | * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**) |
* Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**) | * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**) |
* PC (Windows 2000 or Windows XP) with USB interface | * PC with USB interface |
| * Windows 7 or higher |
| |
---- | ---- |
==== General Setup ==== | |
| |
| ===== General Setup ===== |
| ==== Block Assignments ==== |
| {{ :resources:eval:user-guides:circuits-from-the-lab:cn0203:cn0203-hw-1024_-_edited.jpg?nolink&600 |}} |
| * The [[ADI>CN0203|EVAL-CN0203-SDPZ]] **(CN0203 Board)** connects to the [[ADI>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin Connector **(SDP-B CONN)** |
| * The [[ADI>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable |
| * Terminal block **CN1** is the +/- 15 V power supply input |
| * Terminal block **CN2** is the +6 V power supply input |
| * Terminal block **CN3** is for the voltage output measurement |
| * **Optionally** if **JP3** and **JP4** are open, **VSENSE+** and **VSENSE-** can be connected across a selected branch in the load circuit for feedback. **VSENSE-** should be within +/- 3.0 V of the GND |
| * Terminal block **CN4** is for the current output measurement |
| <WRAP center round important 60%>Power on the **(EVAL-CN0203-SDPZ)** through the triple output power supply and the **(SDP-B Board)** through the PC **SEPARATELY** before connecting the two boards together.</WRAP> |
| |
| ==== Jumper Settings ==== |
| See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI>CN0203|EVAL-CN0203-SDPZ]]. |
| |
| {{ :resources:eval:user-guides:circuits-from-the-lab:cn0203:cn0203_table2_4.jpg?nolink&600 |}} |
| |
| ---- |
| |
| ===== Installing the Evaluation Software ===== |
| - Extract the file **[[ftp://ftp.analog.com/pub/cftl/CN0203/CN0203%20SDP%20Eval%20Software.zip|CN0203 Evaluation Software]]** and open **setup.exe**\\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you install the [[ftp://ftp.analog.com/pub/cftl/CN0203/CN0203%20SDP%20Eval%20Software.zip|CN0203 Evaluation Software]] to the default directory path **C:\Program Files (x86)\Analog Devices\CN0203\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP>\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0203:7-27-2017_10-18-25_am.png?nolink&600|}} |
| - Press **Next** to view the National Instruments Software License Agreement\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0203:7-27-2017_10-18-49_am.png?nolink&600|}} |
| - Select the option which **accepts** the License Agreement and press **Next** to view the installation review page\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0203:7-27-2017_10-19-16_am.png?nolink&600|}} |
| - Press **Next** to start the installation\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0203:7-27-2017_10-20-21_am.png?nolink&600|}} |
| - Upon completion of the installation of the **CN0203 Evaluation Software**, the installer for the ADI SDP Drivers will execute\\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you close all other applications before clicking **“Next”**. This will make it possible to update relevant system files without having to reboot your computer.</WRAP>\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0203:7-27-2017_10-21-00_am.png?nolink&600|}} |
| - Press **“Next”** to set the installation location for the **SDP Drivers**\\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C:\Program Files\Analog Devices\SDP\Drivers**</WRAP>\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0203:7-27-2017_10-21-13_am.png?nolink&600|}} |
| - Press **“Next”** to install the **SDP Drivers**. When prompted by Windows Security, just press **Install**\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0203:7-27-2017_10-22-01_am.png?nolink&600|}} |
| - Press **Finish** to complete the installation\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0203:7-27-2017_10-22-23_am.png?nolink&600|}} |
| |
| ---- |
| ===== Using the Evaluation Software ===== |
| ==== Main Window ==== |
| {{ :resources:eval:user-guides:circuits-from-the-lab:cn0203:7-27-2017_10-29-07_am.png?nolink&600 |}} |
| * **Title Bar** <fc #9400d3>(Highlighted Violet)</fc> |
| * **Connect Button** |
| * Starts the connection with the [[ADI>CN0203|CN0203 Evaluation Board]] |
| * **Disconnect Button** |
| * Ends the connection with the [[ADI>CN0203|CN0203 Evaluation Board]] |
| * **System Configuration** <fc #ffa500>(Highlighted Orange)</fc> |
| * **Connector** |
| * Selects which 120-pin connection of the **SDP-B Board** to use |
| * **SCLK (Hz)** |
| * Sets the SPI clock frequency used by the evaluation board |
| * **AD5750-1 Configuration** <fc #4682b4>(Highlighted Blue)</fc> |
| * **JP1 Configuration** |
| * Sets the SPI address of the AD5750-1 based on the position of JP1 |
| * **Range Select** |
| * Sets the voltage/current output range |
| * **Toggle CLEAR** |
| * Sets the outputs to the zero/midscale voltage value or the minimum value of the selected current range |
| * **AD5750-1 Error Indicator** <fc #ffff00>(Highlighted Yellow)</fc> |
| * **Vout Fault** |
| * There is a short circuit on the VOUT pin |
| * **Iout Fault** |
| * There is an open circuit on the IOUT pin |
| * **Over Temp** |
| * The AD5750-1 core temperature exceeds 150 °C |
| * **PEC Error** |
| * CRC-8 error checking detected an interface error |
| * **Output Setting** <fc #ff0000>Highlighted Red</fc> |
| * **Write AD5660-1** |
| * Writes the hexadecimal value in the left field to the AD5660-1 output voltage |
| * **Reset AD5750-1** |
| * Resets the AD5750-1 to its power-on state |
| * **Quit** |
| * Exits the software application |
| ==== Running the System ==== |
| - Open the **CN0203.exe** application from the default installation location. |
| - Set the correct connector and SCLK settings for the board in the System Configuration section. |
| - Click the **Connect Button** |
| - Upon successful connection, select the desired range of output on the Range Select drop-down menu. |
| - Input a hex value equivalent of the desired output level in the Output Setting section. |
| - Click **Write AD5660-1** |
| - Click **Disconnect Button** if finished. |
| |
| ---- |
| |
| ===== More Information and Useful Links ===== |
| * [[ftp://ftp.analog.com/pub/cftl/CN0203/CN0203%20SDP%20Eval%20Software.zip|CN0203 Evaluation Software]] |
| * [[ADI>CN0203|CN0203 Circuit Note Page]] |
| * [[ADI>CN0203 -DesignSupport|CN0203 Design Support Package]] |
| * [[ADI>AD5660|AD5660-1 Product Page]] |
| * [[ADI>AD5750-1|AD5750-1 Product Page]] |
| |
| ===== Schematic, PCB Layout, Bill of Materials ===== |
| |
| <WRAP round 80% download> |
| [[adi>media/en/reference-design-documentation/design-integration-files/CN0203-DesignSupport.zip|EVAL-CN0203-SDPZ Design & Integration Files]] |
| * Schematics |
| * PCB Layout |
| * Bill of Materials |
| * PADS project |
| </WRAP> |
| |
| =====Registration===== |
| <WRAP round tip 80% > |
| Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. [[reg>EVAL-CN0203-SDPZ?&v=Rev B|Register]] to receive all these great benefits and more!</WRAP> |
| |
| //End of Document// |