| Previous revisionNext revision |
— | resources:eval:user-guides:circuits-from-the-lab:cn0202 [01 Aug 2017 08:56] – update Trisha Cabildo |
---|
| ====== CN0202 Evaluation Board Guide ====== |
| ===== Overview ===== |
| [[ADI>CN202]] a full function, flexible, programmable analog output solution that meets most requirements for programmable logic controller (PLC) and distributed control system (DCS) applications. It provides all the typical voltage and current output ranges with 16-bit resolution and no missing codes, 0.05% linearity, and less than 0.2% total output error. The circuit also contains key features for industrial applications, such as on-chip output fault detection and protection (short circuit, under voltage output, open circuit current output, and over temperature), CRC checking to prevent packet error (PEC), and flexible power-up options, making it an ideal choice for robust industrial control systems. |
| |
| The [[ADI>AD5750/AD5750-1]] are both single-channel, low cost, precision voltage/current output drivers developed to meet the requirements of industrial process control applications. The voltage output range can be programmed for the standard output ranges for PLC and DCS applications: 0 V to 5 V, 0 V to 10 V, −5 V to +5 V, and −10 V to +10 V with a 20% overrange setting provided for the standard ranges. The current output, which is provided on a separate pin, can be programmed for the ranges of 4 mA to 20 mA, 0 mA to 20 mA, −20 mA to +20 mA, 0 mA to 24 mA, and −24 mA to +24 mA. The unipolar ranges have a 2% overrange setting. |
| |
| The [[ADI>AD5662]] is a single channel, low cost, low power (0.75 mW @ 5 V), rail-to-rail voltage buffered output nanoDAC® device. It guarantees ±1 LSB DNL under a wide range of reference voltages that can vary from 0.75 V to the VDD supply so that it can operate with [[ADI>AD5750]] from a common reference source of 4.096 V, provided by the [[ADI>ADR444]]. |
| The [[ADI>ADR444]] low drift (3 ppm/°C maximum for B-grade ), high initial accuracy (0.04% maximum for B-grade), and low noise (1.8 µV p-p typical, 0.1 Hz to 10 Hz) provides the reference voltage for both the [[ADI>AD5750]] and [[ADI>AD5662]] and guarantees ultralow noise, high accuracy, and low temperature drift for the circuit. |
| |
| The EVAL-CN0202-SDPZ board connects to ADI’s System Demonstration Platform (SDP) and is powered by a triple output DC power supply of +15 V, -15 V and 6 V. |
| {{ :resources:eval:user-guides:circuits-from-the-lab:cn0202:cn0202-hw-1024.jpg?nolink&600 |}} |
| \\ |
| ---- |
| ===== Required Equipment ===== |
| * [[adi>EVAL-CN0202-SDPZ|EVAL-CN0202-SDPZ Evaluation Board]] |
| * [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
| * [[ftp://ftp.analog.com/pub/cftl/CN0202/|CN0202 Evaluation Software]] |
| * Triple Output DC Power Supply (6 V, +15 V and -15 V) |
| * PC with the following //Minimum Requirements// |
| * Windows 2000 or Windows XP |
| * USB interface |
| * USB type A to USB type mini-B cable |
| |
| ---- |
| ===== General Setup ===== |
| ==== Block assignments ==== |
| {{ :resources:eval:user-guides:circuits-from-the-lab:cn0202:bbbb.png?nolink&600 |}}\\ |
| * The [[http://www.analog.com/EVAL-CN0202-SDPZ|EVAL-CN0202-SDPZ]] **(CN-0202 Board)** connects to the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
| * The [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
| * Terminal block CN1 is the +/- 15 V power supply input |
| * Terminal block CN2 is the +6 V power supply input |
| * Terminal block CN3 is for the voltage output measurement |
| * Terminal block CN4 is for the current output measurement |
| |
| \\ |
| |
| <WRAP center round important 60%> |
| Power on the **(EVAL-CN0202-SDPZ)** through the triple output power supply and the **(SDP-B Board)** through the PC **separately** before connecting the two boards together. |
| </WRAP> |
| |
| ==== Jumper settings ==== |
| See image below for jumper settings. The bolded values are the default settings for the EVAL-CN0202-SPDZ. |
| {{ :resources:eval:user-guides:circuits-from-the-lab:cn0202:202_jumper.png?nolink&700 |}} |
| ---- |
| ===== Installing the Evaluation Software ===== |
| - Extract the file **CN0202_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you install the [[ftp://ftp.analog.com/pub/cftl/CN0202/|CN0202 Evaluation Software]] to the default directory path **C:\Program Files (x86)\Analog Devices\CN0202\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP> {{:resources:eval:user-guides:circuits-from-the-lab:cn0202:7-28-2017_2-20-06_pm.png?nolink&500|}} |
| - Click **Next** to view the installation review page\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0202:7-28-2017_2-20-18_pm.png?nolink&500|}}\\ \\ |
| - Click **Next** to start the installation\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0202:7-28-2017_2-20-57_pm.png?nolink&500|}}\\ \\ |
| - Upon completion of the installation of the **CN-0202 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you close all other applications before clicking **“Next”**. This will make it possible to update relevant system files without having to reboot your computer.</WRAP>\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0202:7-28-2017_2-22-03_pm.png?nolink&500|}}\\ \\ |
| - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C:\Program Files\Analog Devices\SDP\Drivers**</WRAP>\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0202:7-28-2017_2-22-13_pm.png?nolink&500|}}\\ \\ |
| - Press **“Next”** to install the **SDP Drivers** and complete the installation of all software. Click **"Finish"** when done.\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0202:7-28-2017_2-23-12_pm.png?nolink&500|}} |
| |
| ---- |
| ===== Using the Evaluation Software ===== |
| ===Main Tab=== |
| {{ :resources:eval:user-guides:circuits-from-the-lab:cn0202:8-1-2017_2-27-52_pm.png?nolink&500 |}}\\ |
| - **Connect** |
| * Connect and communicate with the evaluation board |
| - **Connector** |
| * Selects connector A or connector B of the SDP-B Board used |
| - **SCLK** |
| * Sets the clock frequency used by the AD5750, AD5662 and SDP |
| - **JP1 Configuration** |
| * Sets the address of AD5750 |
| - **Range Select** |
| * Sets the voltage/current output range |
| - **Clear AD5750** |
| * Sets the outputs to a zero scale/midscale voltage output or the low end of the selected current range |
| - **Write AD5662** |
| * Writes to AD5662 the hex value in the Output Setting corresponding to the desired output level |
| - **Reset AD5750** |
| * Resets AD5750 to its power-on state |
| - **AD5750 Error Indicator** |
| * Displays errors in AD5750 |
| - **Disconnect** |
| * Stop communication with the evaluation board |
| - **Quit** |
| * Exit the application |
| \\ |
| === Running the System === |
| - Open the **CN0202.exe** application from the default installation location. |
| - Set the correct connector and SCLK settings for the board in the System Configuration section. |
| - Click the **Connect Button** |
| - Upon successful connection, select the desired range of output on the Range Select drop-down menu. |
| - Input a hex value equivalent of the desired output level in the Output Setting section. |
| - Click **Write AD5662** |
| - Click **Disconnect Button** if finished. |
| |
| |
| ---- |
| |
| ===== More Information and Useful Links ===== |
| * [[ftp://ftp.analog.com/pub/cftl/CN0202/|CN0202 Evaluation Software]] |
| * [[ADI>CN0202|CN0202 Circuit Note Page]] |
| * [[ADI>CN0202 -DesignSupport|CN0202 Design Support Package]] |
| * [[ADI>AD5662|AD5662 Product Page]] |
| * [[ADI>AD5750|AD5750 Product Page]] |
| * [[ADI>ADR444|ADR444 Product Page]] |
| |