Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision |
resources:eval:user-guides:circuits-from-the-lab:cn0202 [08 Aug 2017 05:53] – Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0202 [03 Jan 2021 21:55] – fix links Robin Getz |
---|
====== CN0202 Evaluation Board Guide ====== | ====== CN0202 Evaluation Board Guide ====== |
===== Overview ===== | ===== Overview ===== |
[[ADI>CN0202]] a full function, flexible, programmable analog output solution that meets most requirements for programmable logic controller (PLC) and distributed control system (DCS) applications. It provides all the typical voltage and current output ranges with 16-bit resolution and no missing codes, 0.05% linearity, and less than 0.2% total output error. The circuit also contains key features for industrial applications, such as on-chip output fault detection and protection (short circuit, under voltage output, open circuit current output, and over temperature), CRC checking to prevent packet error (PEC), and flexible power-up options, making it an ideal choice for robust industrial control systems. | [[ADI>CN0202]] is a full function, flexible, programmable analog output solution that meets most requirements for programmable logic controller (PLC) and distributed control system (DCS) applications. It provides all the typical voltage and current output ranges with 16-bit resolution and no missing codes, 0.05% linearity, and less than 0.2% total output error. The circuit also contains key features for industrial applications, such as on-chip output fault detection and protection (short circuit, under voltage output, open circuit current output, and over temperature), CRC checking to prevent packet error (PEC), and flexible power-up options, making it an ideal choice for robust industrial control systems. |
| |
The [[ADI>AD5750]] is a single-channel, low cost, precision voltage/current output driver developed to meet the requirements of industrial process control applications. The voltage output range can be programmed for the standard output ranges for PLC and DCS applications: 0 V to 5 V, 0 V to 10 V, −5 V to +5 V, and −10 V to +10 V with a 20% overrange setting provided for the standard ranges. The current output, which is provided on a separate pin, can be programmed for the ranges of 4 mA to 20 mA, 0 mA to 20 mA, −20 mA to +20 mA, 0 mA to 24 mA, and −24 mA to +24 mA. The unipolar ranges have a 2% overrange setting. | The [[ADI>AD5750]] is a single-channel, low cost, precision voltage/current output driver developed to meet the requirements of industrial process control applications. The voltage output range can be programmed for the standard output ranges for PLC and DCS applications: 0 V to 5 V, 0 V to 10 V, −5 V to +5 V, and −10 V to +10 V with a 20% overrange setting provided for the standard ranges. The current output, which is provided on a separate pin, can be programmed for the ranges of 4 mA to 20 mA, 0 mA to 20 mA, −20 mA to +20 mA, 0 mA to 24 mA, and −24 mA to +24 mA. The unipolar ranges have a 2% overrange setting. |
===== Required Equipment ===== | ===== Required Equipment ===== |
* [[adi>EVAL-CN0202-SDPZ|EVAL-CN0202-SDPZ Evaluation Board]] | * [[adi>EVAL-CN0202-SDPZ|EVAL-CN0202-SDPZ Evaluation Board]] |
* [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp://ftp.analog.com/pub/cftl/CN0202/|CN0202 Evaluation Software]] | * [[ftp://ftp.analog.com/pub/cftl/CN0202/|CN0202 Evaluation Software]] |
* Triple Output DC Power Supply (6 V, +15 V and -15 V) | * Triple Output DC Power Supply (6 V, +15 V and -15 V) |
* //Agilent 34401A 6.5 Digital Multimeter// | * //Agilent 34401A 6.5 Digital Multimeter// |
* PC with the following //Minimum Requirements// | * PC with the following //Minimum Requirements// |
* Windows 2000 or Windows XP | * Windows 7 or higher |
* USB interface | * USB interface |
* USB type A to USB type mini-B cable | |
| |
---- | ---- |
==== Block assignments ==== | ==== Block assignments ==== |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0202:bbbb.png?nolink&600 |}}\\ | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0202:bbbb.png?nolink&600 |}}\\ |
* The [[http://www.analog.com/EVAL-CN0202-SDPZ|EVAL-CN0202-SDPZ]] **(CN-0202 Board)** connects to the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector | * The [[adi>EVAL-CN0202-SDPZ|EVAL-CN0202-SDPZ]] **(CN-0202 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
* The [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* Terminal block **CN1** is the +/- 15 V power supply input | * Terminal block **CN1** is the +/- 15 V power supply input |
* Terminal block **CN2** is the +6 V power supply input | * Terminal block **CN2** is the +6 V power supply input |
* Terminal block **CN3** is for the voltage output measurement | * Terminal block **CN3** is for the voltage output measurement |
* **Optionally**, the [[ADI>AD5750]] output voltage feedback can be configured by connecting **VSENSE+** and **VSENSE-** across a selected branch in the load circuit. **VSENSE-** should be within +/- 3.0 V of the GND | * **Optionally**, if JP3 and JP4 are open, the [[ADI>AD5750]] output voltage feedback can be configured by connecting **VSENSE+** and **VSENSE-** across a selected branch in the load circuit. **VSENSE-** should be within +/- 3.0 V of the GND |
* Terminal block **CN4** is for the current output measurement | * Terminal block **CN4** is for the current output measurement |
| |
| |
==== Jumper settings ==== | ==== Jumper settings ==== |
See image below for jumper settings. The bolded values are the default settings for the EVAL-CN0202-SPDZ. | See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI>CN0202|EVAL-CN0202-SDPZ]]. |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0202:202_jumper.png?nolink&700 |}} | |
| {{ :resources:eval:user-guides:circuits-from-the-lab:cn0202:9-11-2017_2-59-26_pm.png?nolink&600 |}} |
---- | ---- |
===== Installing the Evaluation Software ===== | ===== Installing the Evaluation Software ===== |
* [[ADI>AD5750|AD5750 Product Page]] | * [[ADI>AD5750|AD5750 Product Page]] |
* [[ADI>ADR444|ADR444 Product Page]] | * [[ADI>ADR444|ADR444 Product Page]] |
| |
| ===== Schematic, PCB Layout, Bill of Materials ===== |
| |
| <WRAP round 80% download> |
| [[adi>media/en/reference-design-documentation/design-integration-files/CN0202-DesignSupport.zip|EVAL-CN0202-SDPZ Design & Integration Files]] |
| * Schematics |
| * PCB Layout |
| * Bill of Materials |
| * PADS project |
| </WRAP> |
| |