This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0196 [07 Dec 2017 08:04] – Glaizel Arinuelo | resources:eval:user-guides:circuits-from-the-lab:cn0196 [29 Sep 2021 05:23] (current) – design support link update Trisha Cabildo | ||
---|---|---|---|
Line 2: | Line 2: | ||
[[ADI> | [[ADI> | ||
- | Modern microprocessors and microconverters | + | Modern microprocessors and micro converters |
The [[ADI> | The [[ADI> | ||
Line 36: | Line 36: | ||
===== Connectors and Jumper Configurations ===== | ===== Connectors and Jumper Configurations ===== | ||
- | {{: | + | {{: |
==== Description ==== | ==== Description ==== | ||
- | 1. Switch S1: ON state provides an isolated side PWM pulses, OFF states makes the PWM disappears\\ | + | 1. **Switch S1**: ON state provides an isolated side PWM pulses, OFF states makes the PWM disappears\\ |
- | 2. Jumper Link LK1: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\ | + | 2. **Jumper Link LK1**: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\ |
- | 3. Header J1: Provides connection of the controlling signals between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ as seen in below table | + | 3. **Header J1**: Provides connection of the controlling signals between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ as seen in below table |
^EVAL-ADuC7061MKZ^EVAL-CN0196-EB1Z^ | ^EVAL-ADuC7061MKZ^EVAL-CN0196-EB1Z^ | ||
| PWRIN J1-1 | +5V_2 J1-1 | | | PWRIN J1-1 | +5V_2 J1-1 | | ||
Line 48: | Line 48: | ||
| PWM0 J2-26 | PWM0_I J1-5 | | | PWM0 J2-26 | PWM0_I J1-5 | | ||
| DVDD J2-28 | +2V5 J1-3 | | | DVDD J2-28 | +2V5 J1-3 | | ||
- | 4. Jumper Link LK2: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\ | + | 4. **Jumper Link LK2**: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\ |
- | 5. Jumper Link LK3: If pin 1 and 2 is shorted, disabling the ADUM7234 for under voltage condition is generated on board. Shorting pin 2 and 3 will provide externally disabling the isolator via J1-6 header. \\ | + | 5. **Jumper Link LK3**: If pin 1 and 2 is shorted, disabling the ADUM7234 for under voltage condition is generated on board. Shorting pin 2 and 3 will provide externally disabling the isolator via J1-6 header. \\ |
- | 6. Connector J3: See below table | + | 6.** Connector J3**: See below table |
^Pin Number^Description^ | ^Pin Number^Description^ | ||
| J3-1 | VDD: Power Supply of the load | | | J3-1 | VDD: Power Supply of the load | | ||
Line 59: | Line 59: | ||
| J3-6 | GND: Ground connection | | J3-6 | GND: Ground connection | ||
- | 7. Connector J4: Connects +12V power supply and Ground return | + | 7. **Connector J4**: Connects +12V power supply and Ground return |
- | 8. Connector J2: Connection of an external supply up to +20V if jumper link LK4 is not shorted \\ | + | 8. **Connector J2**: Connection of an external supply up to +20V if jumper link LK4 is not shorted \\ |
- | 9. Jumper link LK4: Shorting this pin sets the VDD voltage to +12V | + | 9. **Jumper link LK4**: Shorting this pin sets the VDD voltage to +12V |
===== Software and Driver Installation ===== | ===== Software and Driver Installation ===== | ||
Line 68: | Line 68: | ||
* Follow the on screen prompts to install the software | * Follow the on screen prompts to install the software | ||
- | {{: | + | {{: |
- | {{: | + | {{: |
- | {{: | + | {{: |
- | {{: | + | {{: |
+ | {{: | ||
===== Downloading Firmware to EVAL-ADuC7061-MKZ ===== | ===== Downloading Firmware to EVAL-ADuC7061-MKZ ===== | ||
- | * Connect the EVAL-ADuV7061-MKZ to the PC using USB cable, then find the port assigned to this board in the Device Manager. | + | * Connect the EVAL-ADuC7061-MKZ to the PC using USB cable, then find the COM port assigned to this board in the Device Manager. |
{{: | {{: | ||
* Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. | * Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. | ||
Line 95: | Line 96: | ||
* **STOP APP**: Closing the CN0196 Evaluation Software | * **STOP APP**: Closing the CN0196 Evaluation Software | ||
2. Provides control to the following: | 2. Provides control to the following: | ||
- | * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms < | + | * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms |
+ | < | ||
* **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width | * **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width | ||
* **Start/ | * **Start/ | ||
Line 111: | Line 113: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http://www.analog.com/ | + | [[adi> |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
* Bill of Materials | * Bill of Materials | ||
* PADS project | * PADS project | ||
+ | |||
</ | </ | ||
- | + | =====Registration===== | |
- | + | <WRAP round tip 80% > | |
- | + | Receive software update notifications, | |
- | + | ||
- | + | ||
- | + | ||
+ | // End of Document // |