This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0196 [07 Dec 2017 03:59] – Glaizel Arinuelo | resources:eval:user-guides:circuits-from-the-lab:cn0196 [29 Sep 2021 05:23] (current) – design support link update Trisha Cabildo | ||
---|---|---|---|
Line 2: | Line 2: | ||
[[ADI> | [[ADI> | ||
- | Modern microprocessors and microconverters | + | Modern microprocessors and micro converters |
The [[ADI> | The [[ADI> | ||
Line 24: | Line 24: | ||
===== General Setup ===== | ===== General Setup ===== | ||
- | * Connect the controlling signal from [[ADI> | + | * Connect the controlling signal from [[ADI> |
* Connect the jumpers LK1 pin 1 and 2, LK2 pin 2 and 3, LK3 pin 1 and 2 and short LK4 pin | * Connect the jumpers LK1 pin 1 and 2, LK2 pin 2 and 3, LK3 pin 1 and 2 and short LK4 pin | ||
* Apply +12V power supply to J4 of CN0196 board | * Apply +12V power supply to J4 of CN0196 board | ||
Line 36: | Line 36: | ||
===== Connectors and Jumper Configurations ===== | ===== Connectors and Jumper Configurations ===== | ||
- | {{: | + | {{: |
==== Description ==== | ==== Description ==== | ||
- | + | 1. **Switch S1**: ON state provides an isolated side PWM pulses, OFF states makes the PWM disappears\\ | |
- | 1. Switch S1: ON state disables | + | 2. **Jumper Link LK1**: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\ |
- | 2. Jumper Link LK1: \\ | + | 3. **Header J1**: Provides connection of the controlling signals between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ as seen in below table |
- | 3. Header J1: Provides connection of the controlling signals between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ as seen in below table | + | |
^EVAL-ADuC7061MKZ^EVAL-CN0196-EB1Z^ | ^EVAL-ADuC7061MKZ^EVAL-CN0196-EB1Z^ | ||
| PWRIN J1-1 | +5V_2 J1-1 | | | PWRIN J1-1 | +5V_2 J1-1 | | ||
Line 49: | Line 48: | ||
| PWM0 J2-26 | PWM0_I J1-5 | | | PWM0 J2-26 | PWM0_I J1-5 | | ||
| DVDD J2-28 | +2V5 J1-3 | | | DVDD J2-28 | +2V5 J1-3 | | ||
- | 4. Jumper Link LK2: \\ | + | 4. **Jumper Link LK2**: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\ |
- | 5. Jumper Link LK3: \\ | + | 5. **Jumper Link LK3**: If pin 1 and 2 is shorted, disabling the ADUM7234 for under voltage condition is generated on board. Shorting pin 2 and 3 will provide externally disabling the isolator via J1-6 header. |
- | 6. Connector J3: | + | 6.** Connector J3**: See below table |
- | 7. Connector J4: Connects +12V power supply and Ground return | + | ^Pin Number^Description^ |
- | 8. Connector J2: Connection of an external supply up to +20V if jumper link LK4 is not shorted | + | | J3-1 | VDD: Power Supply of the load | |
+ | | J3-2 | VDD: Power Supply of the load | | ||
+ | | J3-3 | OUT1: Connection of the inductor load| | ||
+ | | J3-4 | OUT2: Connection of the inductor load| | ||
+ | | J3-5 | GND: Ground connection | ||
+ | | J3-6 | GND: Ground connection | ||
+ | |||
+ | 7. **Connector J4**: Connects +12V power supply and Ground return | ||
+ | 8. **Connector J2**: Connection of an external supply up to +20V if jumper link LK4 is not shorted | ||
+ | 9. **Jumper link LK4**: Shorting this pin sets the VDD voltage to +12V | ||
===== Software and Driver Installation ===== | ===== Software and Driver Installation ===== | ||
Line 60: | Line 68: | ||
* Follow the on screen prompts to install the software | * Follow the on screen prompts to install the software | ||
- | {{: | + | {{: |
- | {{: | + | {{: |
- | {{: | + | {{: |
- | {{: | + | {{: |
+ | {{: | ||
===== Downloading Firmware to EVAL-ADuC7061-MKZ ===== | ===== Downloading Firmware to EVAL-ADuC7061-MKZ ===== | ||
- | * Connect the EVAL-ADuV7061-MKZ to the PC using USB cable, then find the port assigned to this board in the Device Manager. | + | * Connect the EVAL-ADuC7061-MKZ to the PC using USB cable, then find the COM port assigned to this board in the Device Manager. |
{{: | {{: | ||
* Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. | * Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. | ||
Line 85: | Line 94: | ||
* **Connect**: | * **Connect**: | ||
* **Disconnect**: | * **Disconnect**: | ||
- | * **STOP APP**: Closing the CN0196 Evaluation | + | * **STOP APP**: Closing the CN0196 Evaluation |
2. Provides control to the following: | 2. Provides control to the following: | ||
- | * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8mz \\ < | + | * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms |
+ | < | ||
* **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width | * **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width | ||
* **Start/ | * **Start/ | ||
Line 96: | Line 106: | ||
4. Displays the current status/ | 4. Displays the current status/ | ||
5. Provides control to the following: | 5. Provides control to the following: | ||
- | * **VDD**: Controls the supply voltage up to 48V | + | * **VDD**: Controls the supply voltage up to 20V |
* **Inductor**: | * **Inductor**: | ||
- | 6. Displays the Inductor (A) vs Time(s) waveform | + | 6. Displays the Inductor (A) vs Time(s) waveform |
- | + | ||
- | + | ||
+ | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
+ | <WRAP round 80% download> | ||
+ | [[adi> | ||
+ | * Schematics | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * PADS project | ||
+ | </ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | // End of Document // |