This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0196 [06 Dec 2017 10:03] – Glaizel Arinuelo | resources:eval:user-guides:circuits-from-the-lab:cn0196 [29 Sep 2021 05:23] (current) – design support link update Trisha Cabildo | ||
---|---|---|---|
Line 2: | Line 2: | ||
[[ADI> | [[ADI> | ||
- | Modern microprocessors and microconverters | + | Modern microprocessors and micro converters |
The [[ADI> | The [[ADI> | ||
Line 24: | Line 24: | ||
===== General Setup ===== | ===== General Setup ===== | ||
- | * Connect [[ADI>CN0196]] board to [[ADI>EVAL-ADuC7061]] board according to the table below \\ | + | * Connect |
- | + | | |
- | ^ EVAL-ADuC7061MKZ ^ EVAL-CN0196-EB1Z | + | |
- | | PWRIN J1-1 | +5V_2 J1-1 | | + | * Connect the USB cable from PC to the USB mini connector on the EVAL-ADuC7061-MKZ board |
- | | GND J1-2 | GND2 J1-2 | | + | |
- | | PWM1 J2-25 | PWM1_I J1-4 | | + | |
- | | PWM0 J2-26 | PWM0_I J1-5 | | + | |
===== Test Setup Functional Block Diagram ===== | ===== Test Setup Functional Block Diagram ===== | ||
Line 38: | Line 36: | ||
===== Connectors and Jumper Configurations ===== | ===== Connectors and Jumper Configurations ===== | ||
- | {{: | + | {{: |
- | **Description** | + | ==== Description ==== |
+ | 1. **Switch S1**: ON state provides an isolated side PWM pulses, OFF states makes the PWM disappears\\ | ||
+ | 2. **Jumper Link LK1**: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\ | ||
+ | 3. **Header J1**: Provides connection of the controlling signals between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ as seen in below table | ||
+ | ^EVAL-ADuC7061MKZ^EVAL-CN0196-EB1Z^ | ||
+ | | PWRIN J1-1 | +5V_2 J1-1 | | ||
+ | | GND | ||
+ | | PWM1 J2-25 | PWM1_I J1-4 | | ||
+ | | PWM0 J2-26 | PWM0_I J1-5 | | ||
+ | | DVDD J2-28 | +2V5 J1-3 | | ||
+ | 4. **Jumper Link LK2**: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\ | ||
+ | 5. **Jumper Link LK3**: If pin 1 and 2 is shorted, disabling the ADUM7234 for under voltage condition is generated on board. Shorting pin 2 and 3 will provide externally disabling the isolator via J1-6 header. \\ | ||
+ | 6.** Connector J3**: See below table | ||
+ | ^Pin Number^Description^ | ||
+ | | J3-1 | VDD: Power Supply of the load | | ||
+ | | J3-2 | VDD: Power Supply of the load | | ||
+ | | J3-3 | OUT1: Connection of the inductor load| | ||
+ | | J3-4 | OUT2: Connection of the inductor load| | ||
+ | | J3-5 | GND: Ground connection | ||
+ | | J3-6 | GND: Ground connection | ||
- | | + | 7. **Connector J4**: Connects +12V power supply and Ground return |
- | - Jumper Link LK1: | + | 8. **Connector J2**: Connection of an external supply up to +20V if jumper link LK4 is not shorted \\ |
- | - Header J1: | + | 9. **Jumper |
- | - Jumper | + | |
- | - Jumper Link LK3: | + | |
- | - Connector J3: | + | |
- | - Connector J4 | + | |
- | - Connector J2: | + | |
===== Software and Driver Installation ===== | ===== Software and Driver Installation ===== | ||
Line 56: | Line 68: | ||
* Follow the on screen prompts to install the software | * Follow the on screen prompts to install the software | ||
- | {{: | + | {{: |
- | {{: | + | {{: |
- | {{: | + | {{: |
- | {{: | + | {{: |
+ | {{: | ||
===== Downloading Firmware to EVAL-ADuC7061-MKZ ===== | ===== Downloading Firmware to EVAL-ADuC7061-MKZ ===== | ||
- | * Connect the EVAL-ADuV7061-MKZ to the PC using USB cable, then find the port assigned to this board in the Device Manager. | + | * Connect the EVAL-ADuC7061-MKZ to the PC using USB cable, then find the COM port assigned to this board in the Device Manager. |
{{: | {{: | ||
* Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. | * Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. | ||
Line 74: | Line 87: | ||
===== Using Evaluation Software ===== | ===== Using Evaluation Software ===== | ||
- | == Software Front Panel == | + | ==== Software Front Panel ==== |
- | {{: | + | {{: |
- | {{: | + | {{: |
- | + | ==== Description | |
- | ==== Descriptions: | + | 1. Provides control to the following: |
+ | * **Connect**: | ||
+ | * **Disconnect**: | ||
+ | * **STOP APP**: Closing the CN0196 Evaluation Software | ||
+ | 2. Provides control to the following: | ||
+ | * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms | ||
+ | < | ||
+ | * **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width | ||
+ | * **Start/ | ||
+ | * **High Side Shot**: When this button is pressed, the PWM waveform will display the Voltage on the high side Mosfets Q1 and Q2 | ||
+ | * **Low Side Shot**: | ||
+ | * **Reset**: Resets all the configuration and hardware connection | ||
+ | 3. Displays the PWM waveform (V) vs Time(s) depending on the configuration set on the PWM controls | ||
+ | 4. Displays the current status/ | ||
+ | 5. Provides control to the following: | ||
+ | * **VDD**: Controls the supply voltage up to 20V | ||
+ | * **Inductor**: | ||
+ | 6. Displays the Inductor (A) vs Time(s) waveform | ||
- | - Connect: Provides connection between EVAL-CN0196-EB1Z and EVAL-ADuC7061-MKZ boards. | + | ===== Schematic, PCB Layout, Bill of Materials ===== |
- | - Disconnect: Provides disconnection between EVAL-CN0196-EB1Z and EVAL-ADuC7061-MKZ boards. | + | |
- | - Stop APP: Stop gathering data | + | |
- | - Load Configuration: | + | |
- | - VDD: | + | |
- | - Inductor: | + | |
- | - Enable: | + | |
- | - Maximum Current: | + | |
- | - PWM Waveform: | + | |
- | - PWM Configuration: | + | |
- | - PWM Pulse Width: | + | |
- | - PWM Interval: | + | |
- | - Stop: | + | |
- | - High Side Shot: | + | |
- | - Low Side Shot: | + | |
- | - Reset: | + | |
- | - Current Wave: | + | |
+ | <WRAP round 80% download> | ||
+ | [[adi> | ||
+ | * Schematics | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * PADS project | ||
+ | </ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | // End of Document // |