This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0196 [07 Dec 2017 08:07] – Glaizel Arinuelo | resources:eval:user-guides:circuits-from-the-lab:cn0196 [07 Dec 2017 08:11] – Glaizel Arinuelo | ||
---|---|---|---|
Line 36: | Line 36: | ||
===== Connectors and Jumper Configurations ===== | ===== Connectors and Jumper Configurations ===== | ||
- | {{: | + | {{: |
==== Description ==== | ==== Description ==== | ||
Line 95: | Line 95: | ||
* **STOP APP**: Closing the CN0196 Evaluation Software | * **STOP APP**: Closing the CN0196 Evaluation Software | ||
2. Provides control to the following: | 2. Provides control to the following: | ||
- | * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms < | + | * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms |
+ | < | ||
* **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width | * **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width | ||
* **Start/ | * **Start/ |