This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0196 [07 Dec 2017 08:04] – Glaizel Arinuelo | resources:eval:user-guides:circuits-from-the-lab:cn0196 [15 Dec 2017 22:57] – Brandon Bushey | ||
---|---|---|---|
Line 36: | Line 36: | ||
===== Connectors and Jumper Configurations ===== | ===== Connectors and Jumper Configurations ===== | ||
- | {{: | + | {{: |
==== Description ==== | ==== Description ==== | ||
- | 1. Switch S1: ON state provides an isolated side PWM pulses, OFF states makes the PWM disappears\\ | + | 1. **Switch S1**: ON state provides an isolated side PWM pulses, OFF states makes the PWM disappears\\ |
- | 2. Jumper Link LK1: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\ | + | 2. **Jumper Link LK1**: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\ |
- | 3. Header J1: Provides connection of the controlling signals between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ as seen in below table | + | 3. **Header J1**: Provides connection of the controlling signals between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ as seen in below table |
^EVAL-ADuC7061MKZ^EVAL-CN0196-EB1Z^ | ^EVAL-ADuC7061MKZ^EVAL-CN0196-EB1Z^ | ||
| PWRIN J1-1 | +5V_2 J1-1 | | | PWRIN J1-1 | +5V_2 J1-1 | | ||
Line 48: | Line 48: | ||
| PWM0 J2-26 | PWM0_I J1-5 | | | PWM0 J2-26 | PWM0_I J1-5 | | ||
| DVDD J2-28 | +2V5 J1-3 | | | DVDD J2-28 | +2V5 J1-3 | | ||
- | 4. Jumper Link LK2: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\ | + | 4. **Jumper Link LK2**: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\ |
- | 5. Jumper Link LK3: If pin 1 and 2 is shorted, disabling the ADUM7234 for under voltage condition is generated on board. Shorting pin 2 and 3 will provide externally disabling the isolator via J1-6 header. \\ | + | 5. **Jumper Link LK3**: If pin 1 and 2 is shorted, disabling the ADUM7234 for under voltage condition is generated on board. Shorting pin 2 and 3 will provide externally disabling the isolator via J1-6 header. \\ |
- | 6. Connector J3: See below table | + | 6.** Connector J3**: See below table |
^Pin Number^Description^ | ^Pin Number^Description^ | ||
| J3-1 | VDD: Power Supply of the load | | | J3-1 | VDD: Power Supply of the load | | ||
Line 59: | Line 59: | ||
| J3-6 | GND: Ground connection | | J3-6 | GND: Ground connection | ||
- | 7. Connector J4: Connects +12V power supply and Ground return | + | 7. **Connector J4**: Connects +12V power supply and Ground return |
- | 8. Connector J2: Connection of an external supply up to +20V if jumper link LK4 is not shorted \\ | + | 8. **Connector J2**: Connection of an external supply up to +20V if jumper link LK4 is not shorted \\ |
- | 9. Jumper link LK4: Shorting this pin sets the VDD voltage to +12V | + | 9. **Jumper link LK4**: Shorting this pin sets the VDD voltage to +12V |
===== Software and Driver Installation ===== | ===== Software and Driver Installation ===== | ||
Line 95: | Line 95: | ||
* **STOP APP**: Closing the CN0196 Evaluation Software | * **STOP APP**: Closing the CN0196 Evaluation Software | ||
2. Provides control to the following: | 2. Provides control to the following: | ||
- | * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms < | + | * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms |
+ | < | ||
* **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width | * **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width | ||
* **Start/ | * **Start/ | ||
Line 118: | Line 119: | ||
</ | </ | ||
+ | // End of Document // | ||
| | ||