This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0194 [24 May 2018 11:05] – Jesse Daniel Santos | resources:eval:user-guides:circuits-from-the-lab:cn0194 [03 Jan 2021 21:55] – fix links Robin Getz | ||
---|---|---|---|
Line 4: | Line 4: | ||
{{: | {{: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board (**SDP-B Board**) |
- | * [[http:// | + | * [[adi>EVAL-CN0194-SDPZ|EVAL-CN0194-SDPZ]] Evaluation Board (**CN-0194 Board**) |
* Power Supply | * Power Supply | ||
* Adjustable DC power supply, output should satisfy: from +6V to +12V over than 500mA. | * Adjustable DC power supply, output should satisfy: from +6V to +12V over than 500mA. | ||
Line 22: | Line 22: | ||
* CN0194 SDP Evaluation Software | * CN0194 SDP Evaluation Software | ||
* Supplied with CD | * Supplied with CD | ||
+ | * [[ftp:// | ||
===== Connecting the Hardware ===== | ===== Connecting the Hardware ===== | ||
==== General Setup ==== | ==== General Setup ==== | ||
- | * The [[http:// | + | * EVAL-CN0194-SDPZ connects to the SDP-B Board via the 120-Pin connector |
- | * Connect +6V DC power supplies on the J1 and J2 connectors to power the [[http:// | + | * Connect +6V DC power supplies on the **J1** and **J2** connectors to power the EVAL-CN0194-SDPZ |
- | * - EVAL-CN0194-SDPZ is ready to use if diodes | + | * - EVAL-CN0194-SDPZ is ready to use if diodes |
- | * The [[http:// | + | * The EVAL-SDP-CB1Z connects to the PC via the USB cable. |
- | * Apply the <fc #ff0000>input signals</ | + | * Apply the input signals on the provided points on the board labeled **AIN1** and **AIN2**. |
- | + | ||
- | | + | |
===== Installing the Software ===== | ===== Installing the Software ===== | ||
Line 44: | Line 43: | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
==== Software Control and Indicator Descriptions ==== | ==== Software Control and Indicator Descriptions ==== | ||
- | {{: | + | {{: |
-**Connect/ | -**Connect/ | ||
* When this button is clicked, the SDP-B Board USB connection to the CN-0194 Board status will be filliped. | * When this button is clicked, the SDP-B Board USB connection to the CN-0194 Board status will be filliped. | ||
Line 73: | Line 72: | ||
* This indicator displays a message regarding the status of the SDP-B Board. | * This indicator displays a message regarding the status of the SDP-B Board. | ||
-**Status LED** | -**Status LED** | ||
- | * This LED showing the ADC working status, when ADC is converting this LED will be light up, otherwise it will be turn off. \\ | + | * This LED showing the ADC working status, when ADC is converting this LED will be light up, otherwise it will be turn off. |
- | {{: | + | |
-**Frequency Analysis** | -**Frequency Analysis** | ||
* __THD__ : Total harmonic distortion | * __THD__ : Total harmonic distortion |