Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0194 [19 Apr 2018 09:40] Jesse Daniel Santosresources:eval:user-guides:circuits-from-the-lab:cn0194 [30 Jul 2021 07:17] (current) Victor Calinao, Jr
Line 4: Line 4:
 {{:resources:eval:user-guides:circuits-from-the-lab:cn0194:cn0194-00-1024_sch.png?600| }} {{:resources:eval:user-guides:circuits-from-the-lab:cn0194:cn0194-00-1024_sch.png?600| }}
 ===== Required Equipment =====  ===== Required Equipment ===== 
-  * [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board (**SDP-B Board**) +  * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board (**SDP-B Board**) 
-  * [[http://www.analog.com/EVAL-CN0194-SDPZ|EVAL-CN0194-SDPZ]] Evaluation Board (**CN-0194 Board**)+  * [[adi>EVAL-CN0194-SDPZ|EVAL-CN0194-SDPZ]] Evaluation Board (**CN-0194 Board**)
   * Power Supply   * Power Supply
     * Adjustable DC power supply, output should satisfy: from +6V to +12V over than 500mA.     * Adjustable DC power supply, output should satisfy: from +6V to +12V over than 500mA.
Line 22: Line 22:
     * CN0194 SDP Evaluation Software     * CN0194 SDP Evaluation Software
       * Supplied with CD       * Supplied with CD
-===== General Setup ===== +      * [[ftp://ftp.analog.com/pub/cftl/CN0194/2.1.0/CN0194_Evaluation_Software.zip|CN0194_Evaluation_Software.zip]]
- +
-  The [[http://www.analog.com/EVAL-CN0194-SDPZ|EVAL-CN0194-SDPZ]] **(CN-0194 Board)** connects to the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector CON A +
-  * Use the Adjustable DC power supplies to powers the [[http://www.analog.com/EVAL-CN0194-SDPZ|EVAL-CN0194-SDPZ]] **(CN-0194 Board)** via the **J4** connector +
-  * The [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.+
  
 ===== Connecting the Hardware ===== ===== Connecting the Hardware =====
 +==== General Setup ====
 +  * EVAL-CN0194-SDPZ connects to the SDP-B Board via the 120-Pin connector **CON A**
 +  * Connect +6V DC power supplies on the **J1** and **J2** connectors to power the EVAL-CN0194-SDPZ
 +  *   - EVAL-CN0194-SDPZ is ready to use if diodes **D3**, **D4**, and **D7** light up.
 +  * The EVAL-SDP-CB1Z connects to the PC via the USB cable.
 +  * Apply the input signals on the provided points on the board labeled **AIN1** and **AIN2**. 
  
 ===== Installing the Software ===== ===== Installing the Software =====
Line 41: Line 43:
 ===== Using the Evaluation Software ===== ===== Using the Evaluation Software =====
 ==== Software Control and Indicator Descriptions ==== ==== Software Control and Indicator Descriptions ====
 +{{:resources:eval:user-guides:circuits-from-the-lab:cn0194:software_use.jpg?1000| }}
   -**Connect/Disconnect Button**   -**Connect/Disconnect Button**
     * When this button is clicked, the SDP-B Board USB connection to the CN-0194 Board status will be filliped.  A connection to the SDP-B Board must be made to use the software.        * When this button is clicked, the SDP-B Board USB connection to the CN-0194 Board status will be filliped.  A connection to the SDP-B Board must be made to use the software.   
Line 54: Line 57:
     * Sets which channel is used and displayed.     * Sets which channel is used and displayed.
   -**Control Tabs**   -**Control Tabs**
-    * __Time Domain__ : This Tab showing the acquired data analyzed result in histogram+    * __Time Domain__ : This tab shows the signal received in the ADC plotted in amplitude vs time.  
-    * __Frequency Domain__ : This Tab include two indicators to showing the position and velocity output of RDC, update in real time when RDC is converting. +    * __Frequency Domain__ : This tab shows the signal received in the ADC plotted in amplitude vs frequency. This Tab include two indicators to showing the position and velocity output of RDC, update in real time when RDC is converting. 
-    * __Histogram__ : +    * __Histogram__ : This tab shows distribution of the captured signal amplitude displayed as the ADC code.
     * __S/W Version Info__ : Showing the SDP-B Board information when USB connection available.     * __S/W Version Info__ : Showing the SDP-B Board information when USB connection available.
   -**Navigation Tools**   -**Navigation Tools**
-    * __Cursor__ +    * __Cursor__ 
     * __Magnification__ : Contains magnification tools      * __Magnification__ : Contains magnification tools 
     * __Hand__ : Used for navigating through the graph     * __Hand__ : Used for navigating through the graph
Line 69: Line 72:
     * This indicator displays a message regarding the status of the SDP-B Board.     * This indicator displays a message regarding the status of the SDP-B Board.
   -**Status LED**   -**Status LED**
-    * This LED showing the ADC working status, when ADC is converting this LED will be light up, otherwise it will be turn off.+    * This LED showing the ADC working status, when ADC is converting this LED will be light up, otherwise it will be turn off. 
   -**Frequency Analysis**   -**Frequency Analysis**
     * __THD__ : Total harmonic distortion     * __THD__ : Total harmonic distortion
Line 81: Line 84:
   -** SDP Firmware Revision Details **   -** SDP Firmware Revision Details **
     * __Major Rev__:      * __Major Rev__: 
-    * _Minor Rev__: +    * __Minor Rev__: 
     * __Date__:      * __Date__: 
     * __Host Code Rev__:      * __Host Code Rev__: 
     * __BF Code Rev__:      * __BF Code Rev__: 
-    * __Time__: +    * __Time__:  
 \\  \\ 
 ---- ----
 +
 ==== Establishing a USB Connection Link ==== ==== Establishing a USB Connection Link ====
   - Follow the instructions to properly install the software and connect the hardware as described in the previous sections.   - Follow the instructions to properly install the software and connect the hardware as described in the previous sections.
Line 101: Line 105:
   - When the number of samples reached the samples setting the converting will stop.   - When the number of samples reached the samples setting the converting will stop.
   - Click the **Save Data Button** to save the conversion data.   - Click the **Save Data Button** to save the conversion data.
 +
 +=====Registration===== 
 +<WRAP round tip 80% >
 +Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware.  [[reg>EVAL-CN0194-SDPZ?&v=Rev B|Register]] to receive all these great benefits and more!</WRAP>
 +
resources/eval/user-guides/circuits-from-the-lab/cn0194.txt · Last modified: 30 Jul 2021 07:17 by Victor Calinao, Jr