Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0194 [24 May 2018 11:10] Jesse Daniel Santosresources:eval:user-guides:circuits-from-the-lab:cn0194 [30 Jul 2021 07:17] (current) Victor Calinao, Jr
Line 4: Line 4:
 {{:resources:eval:user-guides:circuits-from-the-lab:cn0194:cn0194-00-1024_sch.png?600| }} {{:resources:eval:user-guides:circuits-from-the-lab:cn0194:cn0194-00-1024_sch.png?600| }}
 ===== Required Equipment =====  ===== Required Equipment ===== 
-  * [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board (**SDP-B Board**) +  * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board (**SDP-B Board**) 
-  * [[http://www.analog.com/EVAL-CN0194-SDPZ|EVAL-CN0194-SDPZ]] Evaluation Board (**CN-0194 Board**)+  * [[adi>EVAL-CN0194-SDPZ|EVAL-CN0194-SDPZ]] Evaluation Board (**CN-0194 Board**)
   * Power Supply   * Power Supply
     * Adjustable DC power supply, output should satisfy: from +6V to +12V over than 500mA.     * Adjustable DC power supply, output should satisfy: from +6V to +12V over than 500mA.
Line 22: Line 22:
     * CN0194 SDP Evaluation Software     * CN0194 SDP Evaluation Software
       * Supplied with CD       * Supplied with CD
 +      * [[ftp://ftp.analog.com/pub/cftl/CN0194/2.1.0/CN0194_Evaluation_Software.zip|CN0194_Evaluation_Software.zip]]
  
 ===== Connecting the Hardware ===== ===== Connecting the Hardware =====
 ==== General Setup ==== ==== General Setup ====
-  * The [[http://www.analog.com/EVAL-CN0194-SDPZ|EVAL-CN0194-SDPZ]] **(CN-0194 Board)** connects to the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector CON A +  * EVAL-CN0194-SDPZ connects to the SDP-B Board via the 120-Pin connector **CON A** 
-  * Connect +6V DC power supplies on the J1 and J2 connectors to power the [[http://www.analog.com/EVAL-CN0194-SDPZ|EVAL-CN0194-SDPZ]] **(CN-0194 Board)**  +  * Connect +6V DC power supplies on the **J1** and **J2** connectors to power the EVAL-CN0194-SDPZ 
-  *   - EVAL-CN0194-SDPZ is ready to use if diodes <fc #6495ed>D3</fc><fc #6495ed>D4</fc>, and <fc #6495ed>D7</fc> light up. +  *   - EVAL-CN0194-SDPZ is ready to use if diodes **D3****D4**, and **D7** light up. 
-  * The [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. +  * The EVAL-SDP-CB1Z connects to the PC via the USB cable. 
-  * Apply the <fc #ff0000>input signals</fc> on the provided points on the board.  +  * Apply the input signals on the provided points on the board labeled **AIN1** and **AIN2**
- +
- (Insert pic of evaluation system)+
  
 ===== Installing the Software ===== ===== Installing the Software =====
Line 44: Line 43:
 ===== Using the Evaluation Software ===== ===== Using the Evaluation Software =====
 ==== Software Control and Indicator Descriptions ==== ==== Software Control and Indicator Descriptions ====
-{{:resources:eval:user-guides:circuits-from-the-lab:cn0194:software_use.jpg?800| }} +{{:resources:eval:user-guides:circuits-from-the-lab:cn0194:software_use.jpg?1000| }}
-{{:resources:eval:user-guides:circuits-from-the-lab:cn0194:software_use_1.jpg?500| }} +
-{{:resources:eval:user-guides:circuits-from-the-lab:cn0194:software_use_2.jpg?500| }} +
-{{:resources:eval:user-guides:circuits-from-the-lab:cn0194:software_use_3.jpg?500| }} +
-{{:resources:eval:user-guides:circuits-from-the-lab:cn0194:software_use_4.jpg?500| }}+
   -**Connect/Disconnect Button**   -**Connect/Disconnect Button**
     * When this button is clicked, the SDP-B Board USB connection to the CN-0194 Board status will be filliped.  A connection to the SDP-B Board must be made to use the software.        * When this button is clicked, the SDP-B Board USB connection to the CN-0194 Board status will be filliped.  A connection to the SDP-B Board must be made to use the software.   
Line 110: Line 105:
   - When the number of samples reached the samples setting the converting will stop.   - When the number of samples reached the samples setting the converting will stop.
   - Click the **Save Data Button** to save the conversion data.   - Click the **Save Data Button** to save the conversion data.
 +
 +=====Registration===== 
 +<WRAP round tip 80% >
 +Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware.  [[reg>EVAL-CN0194-SDPZ?&v=Rev B|Register]] to receive all these great benefits and more!</WRAP>
 +
resources/eval/user-guides/circuits-from-the-lab/cn0194.txt · Last modified: 30 Jul 2021 07:17 by Victor Calinao, Jr