This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0190 [20 Sep 2017 05:41] – Glaizel Arinuelo | resources:eval:user-guides:circuits-from-the-lab:cn0190 [30 Jul 2021 07:17] – Victor Calinao, Jr | ||
---|---|---|---|
Line 5: | Line 5: | ||
The circuit supplies most of the typical power rails required for digital and analog circuits and also demonstrates an easy way to realize overvoltage, | The circuit supplies most of the typical power rails required for digital and analog circuits and also demonstrates an easy way to realize overvoltage, | ||
- | The circuit is flexible and can accept a wide input voltage range from 6 V to 14 V. This is possible because the highly efficient switching controllers and regulators used in the first stage of each power rail have correspondingly wide input ranges. The [[http:// | + | The circuit is flexible and can accept a wide input voltage range from 6 V to 14 V. This is possible because the highly efficient switching controllers and regulators used in the first stage of each power rail have correspondingly wide input ranges. The [[adi>ADM1178|ADM1178]] block provides overvoltage and overcurrent detection and protection for the input supply, as well as hotswap control for the whole system. The [[adi>ADM1066|ADM1066]] offers a single-chip solution for power supply monitoring and sequencing control for all of the 12 power rails and also margining control for the 3.3V(2A) rail. |
\\ | \\ | ||
Line 84: | Line 84: | ||
===== Software and Driver Installation ===== | ===== Software and Driver Installation ===== | ||
- | You can design your own control strategy and download it into the ADM1066 through this I2C bus connector(JP1) to make the power monitoring and sequencing control for your own custom application using the [[http:// | + | You can design your own control strategy and download it into the ADM1066 through this I2C bus connector(JP1) to make the power monitoring and sequencing control for your own custom application using the [[adi>en/ |
To create a customer sequencing solution, and programming the ADM1066 you need to do the following: | To create a customer sequencing solution, and programming the ADM1066 you need to do the following: | ||
Line 103: | Line 103: | ||
<WRAP center round download 80%> | <WRAP center round download 80%> | ||
- | Download the [[http:// | + | Download the [[adi>media/ |
</ | </ | ||
Line 116: | Line 116: | ||
<WRAP center round download 80%> | <WRAP center round download 80%> | ||
- | Download and Install the [[http:// | + | Download and Install the [[adi>media/ |
</ | </ | ||
Line 123: | Line 123: | ||
- Install Graphviz. \\ {{ : | - Install Graphviz. \\ {{ : | ||
- Upon completion, follow the on-screen promps to install the prog106x Setup Application Software \\ {{ : | - Upon completion, follow the on-screen promps to install the prog106x Setup Application Software \\ {{ : | ||
- | < | + | < |
===== Using Super Sequencer Software ===== | ===== Using Super Sequencer Software ===== | ||
- | Super Sequencer Evaluation Software enables the user to create new control strategy and generates new intel hex file for ADM1066. For detailed information about Super Sequencer features, visit [[http:// | + | Super Sequencer Evaluation Software enables the user to create new control strategy and generates new intel hex file for ADM1066. For detailed information about Super Sequencer features, visit [[adi>media/ |
Generating new hex file using Super Sequencer Software | Generating new hex file using Super Sequencer Software | ||
Line 149: | Line 149: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>media/ |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
Line 156: | Line 156: | ||
</ | </ | ||
+ | " | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | // End of document // |