This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0189 [03 Jan 2021 21:56] – fix links Robin Getz | resources:eval:user-guides:circuits-from-the-lab:cn0189 [30 Jul 2021 07:15] (current) – Victor Calinao, Jr | ||
---|---|---|---|
Line 6: | Line 6: | ||
* [[adi> | * [[adi> | ||
* One SDP Controller board: | * One SDP Controller board: | ||
- | * [[adi>EVAL-SDP-CS1Z| EVAL-SDP-CS1Z]] SDP Evaluation board | + | * [[adi> |
* [[adi> | * [[adi> | ||
* [[ftp:// | * [[ftp:// | ||
Line 28: | Line 28: | ||
- Press **“Next”** to install the Drivers and complete the installation of all software necessary to evaluate the **EVAL-CN0189-SDPZ** | - Press **“Next”** to install the Drivers and complete the installation of all software necessary to evaluate the **EVAL-CN0189-SDPZ** | ||
===== Step by Step Instruction for Connecting the Hardware ===== | ===== Step by Step Instruction for Connecting the Hardware ===== | ||
- | - Connect the [[adi>EVAL-SDP-CS1Z|EVAL-SDP-CS1Z]] and the [[adi> | + | - Connect the [[adi> |
{{: | {{: | ||
- | - Plug in the DC barrel jack to connector J3 of the [[adi> | + | - Plug in the DC barrel jack to connector J3 of the [[adi> |
{{: | {{: | ||
{{: | {{: | ||
Line 40: | Line 40: | ||
- **System Controls** | - **System Controls** | ||
- **Connect** – This button configures the [[adi> | - **Connect** – This button configures the [[adi> | ||
- | - **Disconnect** – This button will disconnect the [[http:// | + | - **Disconnect** – This button will disconnect the [[adi>eval-cn0189-sdpz|EVAL-CN0189-SDPZ]] board. |
- **Connector A** - This menu allows the user to select which connector of the SDP board is being utilized. | - **Connector A** - This menu allows the user to select which connector of the SDP board is being utilized. | ||
- **Conversion Mode Controls** - | - **Conversion Mode Controls** - | ||
Line 72: | Line 72: | ||
- Press **Calibrate** to calculate the offset and sensitivity values for each axis. | - Press **Calibrate** to calculate the offset and sensitivity values for each axis. | ||
- Now any further calculations or conversions performed anywhere in the software (**Demonstration** tab or **Sampled Data** tab) will utilize the offset and sensitivity values calculated here. | - Now any further calculations or conversions performed anywhere in the software (**Demonstration** tab or **Sampled Data** tab) will utilize the offset and sensitivity values calculated here. | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | |||
+ | // End of document // |