This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0188 [28 Nov 2017 06:37] – update Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0188 [04 Dec 2017 10:50] – update Trisha Cabildo | ||
---|---|---|---|
Line 90: | Line 90: | ||
\\ | \\ | ||
+ | ==== Running the System ==== | ||
+ | -Open the CN0188.exe application from the default installation location | ||
+ | -Set the correct connector and click the Connect Button | ||
+ | -Upon successful connection, set the desired input signal parameters such as shunt voltage and temperature | ||
+ | -Start and control data acquisition through the data acquisition control buttons | ||
+ | -Output data will be shown in the graph. Edit graph through plot options and check boxes provided | ||
+ | -Click Disconnect if finished | ||
+ | -Click Quit to exit the program | ||
+ | |||
+ | \\ | ||
---- | ---- | ||