Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0179 [02 Jan 2014 09:37] – January2 Rev1 Glaizel Arinueloresources:eval:user-guides:circuits-from-the-lab:cn0179 [30 Jul 2021 07:13] (current) Victor Calinao, Jr
Line 1: Line 1:
- ======CN-0179 Software User Guide======+====== CN-0179 Software User Guide ======
  
-<fs medium>**OVERVIEW**</fs>+===== OVERVIEW =====
  
- +The circuit is a 4 mA-to-20 mA current loop transmitter for communication between a process control system and its actuator. Besides being cost effective, this circuit offers the industry’s low power solution. The 4 mA-to-20 mA current loop has been used extensively in programmable logic controllers (PLCs) and distributed control systems (DCS’s), with digital or analog inputs and outputs. Current loop interfaces are usually preferred because they offer the most cost effective approach to long distance noise immune data transmission. The combination of low power  [[adi>AD8657|AD8657]]  dual op amp,   [[adi>AD5641|AD5641]] DAC, and [[adi>ADR02|ADR02]] reference allows more power budget for higher power devices, such as microcontrollers and digital isolators. The circuit output is 0 mA to 20 mA of current. The 4 mA to 20 mA range is usually mapped to represent the input control range from the DAC or micro-controller, while the output current range of 0 mA to 4 mA is often used to diagnose fault conditions.
-The circuit is a 4 mA-to-20 mA current loop transmitter for communication between a process control system and its actuator. Besides being cost effective, this circuit offers the industry’s low power solution. The 4 mA-to-20 mA current loop has been used extensively in programmable logic controllers (PLCs) and distributed control systems (DCS’s), with digital or analog inputs and outputs. Current loop interfaces are usually preferred because they offer the most cost effective approach to long distance noise immune data transmission. The combination of low power  [[http://www.analog.com/AD8657|AD8657]]  dual op amp,   [[http://www.analog.com/AD5641|AD5641]] DAC, and [[http://www.analog.com/ADR02|ADR02]] reference allows more power budget for higher power devices, such as microcontrollers and digital isolators. The circuit output is 0 mA to 20 mA of current. The 4 mA to 20 mA range is usually mapped to represent the input control range from the DAC or micro-controller, while the output current range of 0 mA to 4 mA is often used to diagnose fault conditions.+
  
 ---- ----
  
-<fs medium>**GENERAL SETUP**</fs> +===== GENERAL SETUP ===== 
-  * [[http://www.analog.com/EVAL-CN0179-PMDZ|EVAL-CN0179-PMDZ]] Evaluation Board +  * [[adi>EVAL-CN0179-PMDZ|EVAL-CN0179-PMDZ]] Evaluation Board 
-  * [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board +  * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board 
-  * [[http://www.analog.com/SDP-PMD-IB1Z|SDP-PMD-IB1Z]] Evaluation Board+  * [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]] Evaluation Board
   * [[ftp://ftp.analog.com/pub/cftl/CN0179|CN0179 Evaluation Software]]   * [[ftp://ftp.analog.com/pub/cftl/CN0179|CN0179 Evaluation Software]]
     * (supplied with provided CD in kit)     * (supplied with provided CD in kit)
Line 18: Line 17:
   * Agilent 3458A multimeter or equivalent   * Agilent 3458A multimeter or equivalent
   * +6V “Wall Wart”    * +6V “Wall Wart” 
 +
 ---- ----
  
-<fs medium>**MINIMUM PC/SYSTEM REQUIREMENTS**</fs>+===== MINIMUM PC/SYSTEM REQUIREMENTS =====
   * One PC with the following   * One PC with the following
      * Windows XP SP2, Windows Vista or Windows 7 Business/Enterprise/Ultimate editions      * Windows XP SP2, Windows Vista or Windows 7 Business/Enterprise/Ultimate editions
Line 29: Line 29:
 ---- ----
  
-<fs medium>**HOW TO INSTALL THE EVALUATION SOFTWARE**</fs>+===== HOW TO INSTALL THE EVALUATION SOFTWARE =====
   - Extract the file **CN0179 Eval Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you install the [[ftp://ftp.analog.com/pub/cftl/CN0179/|CN0179 Evaluation Software]] to the default directory path **C:\Program Files\Analog Devices\CN0179\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP>{{:resources:eval:user-guides:circuits-from-the-lab:cn0179:cn0179-software-1.png|}}   - Extract the file **CN0179 Eval Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you install the [[ftp://ftp.analog.com/pub/cftl/CN0179/|CN0179 Evaluation Software]] to the default directory path **C:\Program Files\Analog Devices\CN0179\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP>{{:resources:eval:user-guides:circuits-from-the-lab:cn0179:cn0179-software-1.png|}}
   - Click **Next** to view the installation review page\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0179:cn0179-software-2.png|}}\\ \\   - Click **Next** to view the installation review page\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0179:cn0179-software-2.png|}}\\ \\
Line 39: Line 39:
 ---- ----
  
-<fs medium>**PROCEDURES FOR CONNECTING THE HARDWARE**</fs>+===== PROCEDURES FOR CONNECTING THE HARDWARE =====
 {{:resources:eval:user-guides:circuits-from-the-lab:cn0179-hardware.png|}} {{:resources:eval:user-guides:circuits-from-the-lab:cn0179-hardware.png|}}
  
-  - Connect the 120-pin connector of the [[http://www.analog.com/SDP-PMD-IB1Z|SDP-PMD-IB1Z]] circuit board to the connector marked “CON A” on the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board.  Nylon hardware should be used to firmly secure the two boards, using the holes provided at the ends of the 120-pin connectors. +  - Connect the 120-pin connector of the [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]] circuit board to the connector marked “CON A” on the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board.  Nylon hardware should be used to firmly secure the two boards, using the holes provided at the ends of the 120-pin connectors. 
-  - Place shunt to header JP1 to give +3.3V voltage out as seen in the label found in  [[http://www.analog.com/SDP-PMD-IB1Z|SDP-PMD-IB1Z]]. +  - Place shunt to header JP1 to give +3.3V voltage out as seen in the label found in  [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]]. 
-  - Connect the 12-pin right angle male pin header of [[http://www.analog.com/EVAL-CN0179-PMDZ|EVAL-CN0179-PMDZ]] to the 12-pin right angle female pin header of [[http://www.analog.com/SDP-PMD-IB1Z|SDP-PMD-IB1Z]]. +  - Connect the 12-pin right angle male pin header of [[adi>EVAL-CN0179-PMDZ|EVAL-CN0179-PMDZ]] to the 12-pin right angle female pin header of [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]]. 
-  - Connect the current meter in series with the Iout terminal block of the [[http://www.analog.com/EVAL-CN0179-PMDZ|EVAL-CN0179-PMDZ]] +  - Connect the current meter in series with the Iout terminal block of the [[adi>EVAL-CN0179-PMDZ|EVAL-CN0179-PMDZ]] 
   - Connect DC Power Supply (+18V/GND) to the Power connector P1.   - Connect DC Power Supply (+18V/GND) to the Power connector P1.
-  - Plug the mini end of the USB cable into connector J1 of the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and connect the other end of the USB cable into the Laptop or PC.  +  - Plug the mini end of the USB cable into connector J1 of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and connect the other end of the USB cable into the Laptop or PC.  
-  - Plug in the wall wart and connect it to connector J1 of the [[http://www.analog.com/SDP-PMD-IB1Z|SDP-PMD-IB1Z]].+  - Plug in the wall wart and connect it to connector J1 of the [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]].
   - Place shunt to Header J1 to measure the voltage across the load on the Iout terminal block. No shunt means current measurement.   - Place shunt to Header J1 to measure the voltage across the load on the Iout terminal block. No shunt means current measurement.
  
 ---- ----
  
-<fs medium>**OPENING AND ENABLING THE EVALUATION SOFTWARE**</fs>+===== OPENING AND ENABLING THE EVALUATION SOFTWARE =====
  
   - Launch the executable found at C:\Program Files\Analog Devices\CN0179 and press the “Connect” button.   - Launch the executable found at C:\Program Files\Analog Devices\CN0179 and press the “Connect” button.
Line 63: Line 63:
 ---- ----
  
-<fs medium>**USING THE EVALUATION SOFTWARE**</fs>+===== USING THE EVALUATION SOFTWARE =====
  
 There are two ways to select the input control on the DAC; one is for setting the Output Current while the other is for setting the DAC CODE. There are two ways to select the input control on the DAC; one is for setting the Output Current while the other is for setting the DAC CODE.
Line 72: Line 72:
 ---- ----
  
-<fs medium>**DESCRIPTIONS:**</fs>+===== Descriptions=====
  
   - **Enter Hex Code** – This control allows to Enter a value from 0x000 to 0x3FF.   - **Enter Hex Code** – This control allows to Enter a value from 0x000 to 0x3FF.
   - **Iout** – This indicator shows the calculated Output Current depending on the input Code.   - **Iout** – This indicator shows the calculated Output Current depending on the input Code.
-  - **Data Bits** – Binary equivalent of the Code loaded to the [[http://www.analog.com/AD5641|AD5641]] DAC.+  - **Data Bits** – Binary equivalent of the Code loaded to the [[adi>AD5641|AD5641]] DAC.
   - **VDAC** – This indicator shows the calculated DAC output Voltage depending on the input code.   - **VDAC** – This indicator shows the calculated DAC output Voltage depending on the input code.
   - **Enter Output Current** – This control allows to Enter a value from 0 to 20.   - **Enter Output Current** – This control allows to Enter a value from 0 to 20.
-  - **Data Code** – This indicator shows the Hex Code equivalent of the value loaded to the [[http://www.analog.com/AD5641|AD5641]] DAC. +  - **Data Code** – This indicator shows the Hex Code equivalent of the value loaded to the [[adi>AD5641|AD5641]] DAC. 
-  - **Write DAC** – When this button is pressed, the values/codes entered will send to the [[http://www.analog.com/AD5641|AD5641]] DAC via SPI. +  - **Write DAC** – When this button is pressed, the values/codes entered will send to the [[adi>AD5641|AD5641]] DAC via SPI. 
   - **System Status String Indicator** - This indicator displays a message to the user detailing the current state of the software.   - **System Status String Indicator** - This indicator displays a message to the user detailing the current state of the software.
   - **System Status LED Indicator** - This indicator displays the current state of the software in the form of an LED.\\  There are three status LED colors:\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0179:cn0179-software-busy.png|}} - Busy\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0179:cn0179-software-inactive.png|}} - Inactive\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0179:cn0179-software-error.png|}} - Error\\   - **System Status LED Indicator** - This indicator displays the current state of the software in the form of an LED.\\  There are three status LED colors:\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0179:cn0179-software-busy.png|}} - Busy\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0179:cn0179-software-inactive.png|}} - Inactive\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0179:cn0179-software-error.png|}} - Error\\
   - **SDP Board Information** - provides details on the firmware version of the Blackfin used by the SDP board.   - **SDP Board Information** - provides details on the firmware version of the Blackfin used by the SDP board.
  
 +=====Registration===== 
 +<WRAP round tip 80% >
 +Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware.  [[reg>EVAL-CN0179-PMDZ?&v=Rev B|Register]] to receive all these great benefits and more!</WRAP>
  
 +// End of document //
    
resources/eval/user-guides/circuits-from-the-lab/cn0179.1388651850.txt.gz · Last modified: 02 Jan 2014 09:37 by Glaizel Arinuelo