This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0179 [02 Jan 2014 09:37] – January2 Rev1 Glaizel Arinuelo | resources:eval:user-guides:circuits-from-the-lab:cn0179 [05 May 2015 19:49] – formatting Brandon Bushey | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======CN-0179 Software User Guide====== | + | ====== CN-0179 Software User Guide ====== |
- | + | ||
- | <fs medium> | + | |
+ | ===== OVERVIEW ===== | ||
The circuit is a 4 mA-to-20 mA current loop transmitter for communication between a process control system and its actuator. Besides being cost effective, this circuit offers the industry’s low power solution. The 4 mA-to-20 mA current loop has been used extensively in programmable logic controllers (PLCs) and distributed control systems (DCS’s), with digital or analog inputs and outputs. Current loop interfaces are usually preferred because they offer the most cost effective approach to long distance noise immune data transmission. The combination of low power [[http:// | The circuit is a 4 mA-to-20 mA current loop transmitter for communication between a process control system and its actuator. Besides being cost effective, this circuit offers the industry’s low power solution. The 4 mA-to-20 mA current loop has been used extensively in programmable logic controllers (PLCs) and distributed control systems (DCS’s), with digital or analog inputs and outputs. Current loop interfaces are usually preferred because they offer the most cost effective approach to long distance noise immune data transmission. The combination of low power [[http:// | ||
Line 8: | Line 7: | ||
---- | ---- | ||
- | <fs medium> | + | ===== GENERAL SETUP ===== |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 18: | Line 17: | ||
* Agilent 3458A multimeter or equivalent | * Agilent 3458A multimeter or equivalent | ||
* +6V “Wall Wart” | * +6V “Wall Wart” | ||
+ | |||
---- | ---- | ||
- | <fs medium> | + | ===== MINIMUM PC/SYSTEM REQUIREMENTS |
* One PC with the following | * One PC with the following | ||
* Windows XP SP2, Windows Vista or Windows 7 Business/ | * Windows XP SP2, Windows Vista or Windows 7 Business/ | ||
Line 29: | Line 29: | ||
---- | ---- | ||
- | <fs medium> | + | ===== HOW TO INSTALL THE EVALUATION SOFTWARE |
- Extract the file **CN0179 Eval Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> | - Extract the file **CN0179 Eval Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> | ||
- Click **Next** to view the installation review page\\ \\ {{: | - Click **Next** to view the installation review page\\ \\ {{: | ||
Line 39: | Line 39: | ||
---- | ---- | ||
- | <fs medium> | + | ===== PROCEDURES FOR CONNECTING THE HARDWARE |
{{: | {{: | ||
Line 53: | Line 53: | ||
---- | ---- | ||
- | <fs medium> | + | ===== OPENING AND ENABLING THE EVALUATION SOFTWARE |
- Launch the executable found at C:\Program Files\Analog Devices\CN0179 and press the “Connect” button. | - Launch the executable found at C:\Program Files\Analog Devices\CN0179 and press the “Connect” button. | ||
Line 63: | Line 63: | ||
---- | ---- | ||
- | <fs medium> | + | ===== USING THE EVALUATION SOFTWARE |
There are two ways to select the input control on the DAC; one is for setting the Output Current while the other is for setting the DAC CODE. | There are two ways to select the input control on the DAC; one is for setting the Output Current while the other is for setting the DAC CODE. | ||
Line 72: | Line 72: | ||
---- | ---- | ||
- | <fs medium> | + | ===== Descriptions: ===== |
- **Enter Hex Code** – This control allows to Enter a value from 0x000 to 0x3FF. | - **Enter Hex Code** – This control allows to Enter a value from 0x000 to 0x3FF. |