Both sides previous revisionPrevious revision | |
resources:eval:user-guides:circuits-from-the-lab:cn0178 [30 Jul 2021 07:12] – Victor Calinao, Jr | resources:eval:user-guides:circuits-from-the-lab:cn0178 [23 Mar 2022 05:53] (current) – updated sw link Trisha Cabildo |
---|
* [[adi>EVAL-CN0178-SDPZ|EVAL-CN0178-SDPZ Evaluation Board]] | * [[adi>EVAL-CN0178-SDPZ|EVAL-CN0178-SDPZ Evaluation Board]] |
* [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp://ftp.analog.com/pub/cftl/CN0178/|CN0178 Evaluation Software]] | * [[http://swdownloads.analog.com/cse/cftl/CN0178/CN0178_SDP_Eval_Software.zip|CN0178 Evaluation Software]] |
* 6 V or 6 V Wall wart | * 6 V or 6 V Wall wart |
* //Agilent E3631A power supply// | * //Agilent E3631A power supply// |
---- | ---- |
===== Installing the Evaluation Software ===== | ===== Installing the Evaluation Software ===== |
- Extract the file **CN0178_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you install the [[ftp://ftp.analog.com/pub/cftl/CN0178/|CN0178 Evaluation Software]] to the default directory path **C:\Program Files (x86)\Analog Devices\CN0178\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP> {{:resources:eval:user-guides:circuits-from-the-lab:cn0178:1.png?nolink&500|}} | - Extract the file **CN0178_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you install the [[http://swdownloads.analog.com/cse/cftl/CN0178/CN0178_SDP_Eval_Software.zip|CN0178 Evaluation Software]] to the default directory path **C:\Program Files (x86)\Analog Devices\CN0178\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP> {{:resources:eval:user-guides:circuits-from-the-lab:cn0178:1.png?nolink&500|}} |
- Click **Next** to view the installation review page\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0178:2.png?nolink&500|}}\\ \\ | - Click **Next** to view the installation review page\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0178:2.png?nolink&500|}}\\ \\ |
- Click **Next** to start the installation\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0178:3.png?nolink&500|}}\\ \\ | - Click **Next** to start the installation\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0178:3.png?nolink&500|}}\\ \\ |
| |
===== More Information and Useful Links ===== | ===== More Information and Useful Links ===== |
* [[ftp://ftp.analog.com/pub/cftl/CN0178/|CN0178 Evaluation Software]] | * [[http://swdownloads.analog.com/cse/cftl/CN0178/CN0178_SDP_Eval_Software.zip|CN0178 Evaluation Software]] |
* [[ADI>CN0178|CN0178 Circuit Note Page]] | * [[ADI>CN0178|CN0178 Circuit Note Page]] |
* [[adi>media/en/reference-design-documentation/design-integration-files/CN0178-DesignSupport.zip|CN0178 Design Support Package]] | * [[adi>media/en/reference-design-documentation/design-integration-files/CN0178-DesignSupport.zip|CN0178 Design Support Package]] |