This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0178 [25 Oct 2017 05:48] – created Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0178 [23 Mar 2022 05:53] (current) – updated sw link Trisha Cabildo | ||
---|---|---|---|
Line 13: | Line 13: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
- | * [[ftp://ftp.analog.com/ | + | * [[http://swdownloads.analog.com/ |
- | | + | * 6 V or 6 V Wall wart |
- | | + | * //Agilent E3631A power supply// |
* PC with the following //Minimum Requirements// | * PC with the following //Minimum Requirements// | ||
* Windows 7 (32-bit), Windows Vista (32-bit) or Windows XP | * Windows 7 (32-bit), Windows Vista (32-bit) or Windows XP | ||
* USB interface | * USB interface | ||
- | * RF signal source | + | * RF signal source |
* //Rohde & Schwarz SMT-03 RF signal source// | * //Rohde & Schwarz SMT-03 RF signal source// | ||
* Coaxial RF cable with SMA connectors | * Coaxial RF cable with SMA connectors | ||
Line 27: | Line 27: | ||
===== General Setup ===== | ===== General Setup ===== | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
- | {{ : | + | {{ : |
- | * The [[http:// | + | * The [[adi>EVAL-CN0178-SDPZ|EVAL-CN0178-SDPZ]] **(CN-0178 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
- | * Terminal block **J2** is the +6 V power supply input | + | * Terminal block **J1** is the +6 V power supply |
+ | * Terminal block **J2** is the +6 V barrel connector for wall wart supply input | ||
* Terminal block **J3** is the SMA connector for RF input | * Terminal block **J3** is the SMA connector for RF input | ||
\\ | \\ | ||
+ | ==== Test setup ==== | ||
+ | {{ : | ||
+ | - Connect the 120-pin connector on the [[adi> | ||
+ | - Connect the RF signal source to the [[adi> | ||
+ | - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | ||
+ | *//If available, a +6 V "wall wart" can be connected to the barrel connector on the board and used in place of the +6 V power supply// | ||
+ | - Connect the USB cable supplied with the SDP board to the USB port on the PC | ||
+ | - Apply power to the +6 V supply (or “wall wart”) connected to [[adi> | ||
+ | - Launch the evaluation software | ||
+ | - Connect the USB cable from the PC to the USB mini connector on the SDP board | ||
+ | \\ | ||
<WRAP center round important 60%> | <WRAP center round important 60%> | ||
- | Do **not** connect the USB cable to the Mini-USB connector on the SDP board before turning on the dc power supply for the **EVAL-CN0150-SDPZ**. | + | Do **not** connect the USB cable to the Mini-USB connector on the SDP board before turning on the dc power supply for the **EVAL-CN0178-SDPZ**. |
</ | </ | ||
+ | \\ | ||
+ | |||
+ | ==== Calibration ==== | ||
+ | Because the slope and intercept of the system vary from device to device, a system level calibration is **required**. For this board, a 4-point calibration is used to correct for some non-linearity in the RF detector' | ||
+ | - Apply four known signal levels to ADL5902. Note that it should be well within the linear operating range of the device {{ : | ||
+ | - Measure the corresponding output codes from the ADC | ||
+ | - Calculate SLOPE_ADC and INTERCEPT calibration coefficients using the following equations: | ||
+ | * **SLOPE_1** = (CODE_1 - CODE_2)/ | ||
+ | * **INTERCEPT1** = CODE_1/ | ||
+ | - This calculation is repeated using CODE2/CODE3 and CODE3/CODE4 to calculate SLOPE2/ | ||
+ | - These will be used to calculate the unknown input power level, PIN, when operation in the field using the equation | ||
+ | * **PIN** = (CODE/ | ||
+ | - The observed code from the ADC will be compared to the calibration coefficient codes in order to retrieve the appropriate SLOPE and INTERCEPT calibration coefficients. | ||
+ | * Example: If CODE from ADC is between CODE1 and CODE2, then SLOPE1/ | ||
+ | \\ | ||
---- | ---- | ||
===== Installing the Evaluation Software ===== | ===== Installing the Evaluation Software ===== | ||
- | - Extract the file **CN0150_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> | + | - Extract the file **CN0178_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> |
- | - **Accept** the license agreement to proceed to the installation review page\\ \\ {{: | + | - Click **Next** to view the installation review page\\ \\ {{: |
- | - Click **Next** to view the installation review page\\ \\ {{: | + | - Click **Next** to start the installation\\ \\ {{: |
- | - Click **Next** to start the installation\\ \\ {{: | + | - Upon completion of the installation of the **CN-0178 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%> |
- | - Upon completion of the installation of the **CN-0150 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%> | + | - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: |
- | - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: | + | - Press **“Install”** to install the **SDP Drivers** and complete the installation of all software. |
- | - Press **“Install”** to install the **SDP Drivers** and complete the installation of all software. | + | |
---- | ---- | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
- | ====Test Setup Tab==== | + | ==== Main Window |
- | {{ : | + | {{ : |
- | | + | - **Connect** Button - Starts the connection between the [[ADI> |
+ | - **Disconnect** Button - Ends the connection between the [[ADI> | ||
+ | - **SDP Connector** - Selects which 120-pin connection of the SDP-B Board to use | ||
+ | - **Input Power** - Indicate input signal power level | ||
+ | - **Frequency** - Indicate input signal frequency | ||
+ | - **Data Acquisition** Controls \\ {{ : | ||
+ | * **Sample Data** - Start acquisition of measurement data | ||
+ | * **Remove Data Point** - Remove a data point from samples | ||
+ | * **Clear Data** - Clear the current measurement data | ||
+ | * **Save Data** - Save measurement data to file | ||
+ | - **Sample Data Graph** Tab - Shows the XY plot of ADC code and output error (%) with respect to the shunt voltage\\ {{ : | ||
+ | * **Plot Options** - Edit plot display and options like interpolation and color of output waveform | ||
+ | - **Calibration** Tab | ||
+ | * **Calibration Inputs** - Four point input power levels used for calibration purposes | ||
+ | * **Calibration Data** - Enable calibration of the device | ||
+ | * **Calibration Coefficients** - Read only. Calculated calibration coefficients based on four point input power levels | ||
+ | - **Administration** Tab \\ {{ : | ||
+ | * **Read Firmware** - Reads the firmware of CN0150 Evaluation Board | ||
+ | * **Flash LED** - Flashes the LED on the SDP controller board | ||
+ | | ||
\\ | \\ | ||
+ | ==== Running the System ==== | ||
+ | -Open the CN0178.exe application from the default installation location | ||
+ | -Set the correct connector and click the Connect Button | ||
+ | -Upon successful connection, calibrate the device through the calibration tab | ||
+ | -After proper calibration, | ||
+ | -Click Disconnect if finished | ||
+ | -Click Quit to exit the program | ||
+ | |||
+ | \\ | ||
---- | ---- | ||
===== More Information and Useful Links ===== | ===== More Information and Useful Links ===== | ||
- | * [[ftp://ftp.analog.com/ | + | * [[http://swdownloads.analog.com/ |
- | * [[ADI>CN0150|CN0150 | + | * [[ADI>CN0178|CN0178 |
- | * [[http:// | + | * [[adi>media/ |
- | * [[ADI>AD8318|AD8318 | + | |
- | * [[ADI>ADR421|ADR421 | + | * [[ADI>ADL5902|ADL5902 |
- | * [[ADI>AD7887|AD7887 | + | * [[ADI>AD7466|AD7466 |
+ | * [[ADI>ADG3231|ADG3231 | ||
===== Schematic, PCB Layout, Bill of Materials ===== | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>media/ |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
Line 75: | Line 129: | ||
* PADS project | * PADS project | ||
</ | </ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
//End of Document// | //End of Document// | ||