This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0178 [04 Dec 2017 09:32] – update Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0178 [30 Jul 2021 07:12] – Victor Calinao, Jr | ||
---|---|---|---|
Line 13: | Line 13: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp:// | * [[ftp:// | ||
* 6 V or 6 V Wall wart | * 6 V or 6 V Wall wart | ||
Line 28: | Line 28: | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
{{ : | {{ : | ||
- | * The [[http:// | + | * The [[adi>EVAL-CN0178-SDPZ|EVAL-CN0178-SDPZ]] **(CN-0178 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* Terminal block **J1** is the +6 V power supply | * Terminal block **J1** is the +6 V power supply | ||
* Terminal block **J2** is the +6 V barrel connector for wall wart supply input | * Terminal block **J2** is the +6 V barrel connector for wall wart supply input | ||
Line 37: | Line 37: | ||
==== Test setup ==== | ==== Test setup ==== | ||
{{ : | {{ : | ||
- | - Connect the 120-pin connector on the [[adi> | + | - Connect the 120-pin connector on the [[adi> |
- Connect the RF signal source to the [[adi> | - Connect the RF signal source to the [[adi> | ||
- With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | ||
Line 76: | Line 76: | ||
---- | ---- | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
- | ====Test Setup Tab==== | + | ==== Main Window |
- | {{ : | + | {{ : |
- | | + | - **Connect** Button - Starts the connection between the [[ADI> |
+ | - **Disconnect** Button - Ends the connection between the [[ADI> | ||
+ | - **SDP Connector** - Selects which 120-pin connection of the SDP-B Board to use | ||
+ | - **Input Power** - Indicate input signal power level | ||
+ | - **Frequency** - Indicate input signal frequency | ||
+ | - **Data Acquisition** Controls \\ {{ : | ||
+ | * **Sample Data** - Start acquisition of measurement data | ||
+ | * **Remove Data Point** - Remove a data point from samples | ||
+ | * **Clear Data** - Clear the current measurement data | ||
+ | * **Save Data** - Save measurement data to file | ||
+ | - **Sample Data Graph** Tab - Shows the XY plot of ADC code and output error (%) with respect to the shunt voltage\\ {{ : | ||
+ | * **Plot Options** - Edit plot display and options like interpolation and color of output waveform | ||
+ | - **Calibration** Tab | ||
+ | * **Calibration Inputs** - Four point input power levels used for calibration purposes | ||
+ | * **Calibration Data** - Enable calibration of the device | ||
+ | * **Calibration Coefficients** - Read only. Calculated calibration coefficients based on four point input power levels | ||
+ | - **Administration** Tab \\ {{ : | ||
+ | * **Read Firmware** - Reads the firmware of CN0150 Evaluation Board | ||
+ | * **Flash LED** - Flashes the LED on the SDP controller board | ||
+ | | ||
\\ | \\ | ||
+ | ==== Running the System ==== | ||
+ | -Open the CN0178.exe application from the default installation location | ||
+ | -Set the correct connector and click the Connect Button | ||
+ | -Upon successful connection, calibrate the device through the calibration tab | ||
+ | -After proper calibration, | ||
+ | -Click Disconnect if finished | ||
+ | -Click Quit to exit the program | ||
+ | |||
+ | \\ | ||
---- | ---- | ||
Line 86: | Line 114: | ||
* [[ftp:// | * [[ftp:// | ||
* [[ADI> | * [[ADI> | ||
- | * [[http:// | + | * [[adi>media/ |
* [[ADI> | * [[ADI> | ||
Line 95: | Line 123: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>media/ |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
Line 101: | Line 129: | ||
* PADS project | * PADS project | ||
</ | </ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
//End of Document// | //End of Document// | ||