This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0172 [13 Dec 2012 16:39] – [CIRCUIT NOTE TITLE (CN0172)] Brandon Bushey | resources:eval:user-guides:circuits-from-the-lab:cn0172 [30 Jul 2021 07:11] (current) – Victor Calinao, Jr | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== Overview ===== | ===== Overview ===== | ||
- | The function of the [[http:// | + | The function of the [[adi>CN0172|CN0172]] is to provide a high accuracy multi-channel thermocouple measurement solution. Achieving a precision thermocouple measurement requires a signal chain of precision components that will amplify the small thermocouple voltage, remove noise, correct non-linearity, |
===== General Setup ===== | ===== General Setup ===== | ||
- | * 1x [[http:// | + | * 1x [[adi>EVAL-CN0172-SDPZ|EVAL-CN0172-SDPZ]] Circuit Evaluation board |
- | * 1x [[http:// | + | * 1x [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller board |
* 1x SDP Breakout Board | * 1x SDP Breakout Board | ||
* 3x K-type thermocouples | * 3x K-type thermocouples | ||
Line 52: | Line 52: | ||
- **Save Data in Folder** – Directory for data storage | - **Save Data in Folder** – Directory for data storage | ||
- Once the Board Setup is complete the user can obtain data by clicking the **“Start Data Acquisition”** button.{{ : | - Once the Board Setup is complete the user can obtain data by clicking the **“Start Data Acquisition”** button.{{ : | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | |||
+ | // End of document // |