This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0172 [11 Oct 2012 16:50] – removing block diagram Brandon Bushey | resources:eval:user-guides:circuits-from-the-lab:cn0172 [13 Dec 2012 16:39] – [CIRCUIT NOTE TITLE (CN0172)] Brandon Bushey | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== | + | ====== CN0172 |
===== Overview ===== | ===== Overview ===== | ||
Line 26: | Line 26: | ||
- Download [[ftp:// | - Download [[ftp:// | ||
- | - Extract the files within the file **CN0172 SDP Eval Software.zip** and open the file **setup.exe**. | + | - Extract the files within the file **CN0172 SDP Eval Software.zip** and open the file **setup.exe**. |
- | - Press **“Next”**.{{ : | + | - Press **“Next”**.{{ : |
- | - Press **“Next”**.{{ : | + | - Press **“Next”**.{{ : |
- | - Upon completion of the installation of the **CN0172 SDP Eval Software**, the installer for the **ADI SDP Drivers** will execute. | + | - Upon completion of the installation of the **CN0172 SDP Eval Software**, the installer for the **ADI SDP Drivers** will execute. |
- | - Press **“Next”**{{ : | + | - Press **“Next”**{{ : |
- Press **“Finish”** to install the Drivers and complete the installation of all software necessary to evaluate the **EVAL-CN0172-SDPZ** | - Press **“Finish”** to install the Drivers and complete the installation of all software necessary to evaluate the **EVAL-CN0172-SDPZ** | ||
- | |||
===== Step by Step Instruction for Connecting the Hardware ===== | ===== Step by Step Instruction for Connecting the Hardware ===== | ||
- | - Ensure that the Breakout board and the EVAL-CN0172-SDPZ are wired up correctly. Connect the **EVAL-SDP-CB1Z** and the Multi-Channel **breakout board** using both 120 pin male and female connectors found on the respective boards.{{ : | + | - Ensure that the Breakout board and the EVAL-CN0172-SDPZ are wired up correctly. Connect the **EVAL-SDP-CB1Z** and the Multi-Channel **breakout board** using both 120 pin male and female connectors found on the respective boards.{{ : |
- | - Mount the SDP Board onto the breakout board.{{ : | + | - Mount the SDP Board onto the breakout board.{{ : |
- | - Plug 3 K-type thermocouple wires into the thermocouple connector as shown.{{ : | + | - Plug 3 K-type thermocouple wires into the thermocouple connector as shown.{{ : |
- Plug the mini end of the USB cable into connector J1 of the **EVAL-SDP-CB1Z** and connect the other end of the USB cable into the Laptop or PC. | - Plug the mini end of the USB cable into connector J1 of the **EVAL-SDP-CB1Z** and connect the other end of the USB cable into the Laptop or PC. | ||
- Wait for found new hardware wizard to appear and finish installation of SPD driver before opening the software. | - Wait for found new hardware wizard to appear and finish installation of SPD driver before opening the software. | ||
- | |||
===== Opening and Enabling the Evaluation Software ===== | ===== Opening and Enabling the Evaluation Software ===== | ||
- | - Launch the software which will be located in the analog devices folder in all programs.{{ : | + | - Launch the software which will be located in the analog devices folder in all programs.{{ : |
- After starting the application the user must click the **“Board Setup”** button. The user has the option to edit one or more of the following options: | - After starting the application the user must click the **“Board Setup”** button. The user has the option to edit one or more of the following options: | ||
- **Thermocouple type** – User selects the correct thermocouple being used | - **Thermocouple type** – User selects the correct thermocouple being used | ||
Line 53: | Line 51: | ||
- **Data logging status** – Enable to record temperature in location specified in save data to folder directory | - **Data logging status** – Enable to record temperature in location specified in save data to folder directory | ||
- **Save Data in Folder** – Directory for data storage | - **Save Data in Folder** – Directory for data storage | ||
- | - Once the Board Setup is complete the user can obtain data by clicking the **“Start Data Acquisition”** button.{{ : | + | - Once the Board Setup is complete the user can obtain data by clicking the **“Start Data Acquisition”** button.{{ : |