Wiki

This version (07 Dec 2023 07:30) was approved by Allan Uy.The Previously approved version (22 Nov 2023 09:16) is available.Diff

CN0583 Smoke Detector Module User Guide

The hardware used for evaluation of the CN0583 smoke detector module is composed of two parts — the EVAL-CN0583-SOM smoke detector system-on-module (SOM), and the EVAL-CN0583-CRR1 carrier board.



The EVAL-CN0583-SOM is a standalone module designed for development of smoke detection applications. The CN0583 SOM integrates an ADPD188BI smoke sensor, a MAX32660 microcontroller, and regulated DC power supplies needed for proper operation. The SOM only requires DC power and ground connections from a host system to run a smoke detection application, and will output an alarm signal via a GPIO pin.

The EVAL-CN0583-CRR1 is an easy to use carrier board developed for evaluation of the SOM and enable rapid prototyping. The CN0583 carrier board has an onboard debugger based on the MAX32625PICO that allows drag-and-drop programming of the SOM and USB-UART communication. An indicator LED and buzzer are also included on the board to allow users to implement a basic alarm function in their smoke detector application.



System-on-Module

Board Castellation

The SOM has 28 castellated “pins” divided into two 14-pin rows, and arranged in a dual in-line pattern. These pins are used to supply power and interface external circuitry with the SOM hardware, allowing access to the GPIO pins of the MAX32660 and ADPD188BI. The table below shows the default pinout of the SOM when programmed with the CN0583 demo application.


Pin Number Pin Name Function
1 VBATT Supply Voltage Input (2.2 V to 5.5 V)
2
3 GND Ground.
4
5 NC No connection.
6 GPIO0 GPIO pin used for optional timing signals. Connected to GPIO0 of the ADPD188BI.
7 GPIO1 GPIO pin used for optional timing signals. Connected to GPIO1 of the ADPD188BI.
8 LED_OUT GPIO pin used to trigger an external visual indicator (e.g., LED). Connected to P0.4 of the MAX32660.
9 BUTTON_IN GPIO pin used for reading user inputs from an external button. Connected to P0.2 of the MAX32660.
10 ALARM_OUT GPIO pin used to trigger an external audio device (e.g., buzzer). Connected to P0.5 of the MAX32660.
11 GND Ground.
12
13 VBATT 2.2 V to 5.5 V Supply.
14
15 SWDIO Serial Wire Debug Data. Connected to P0.0 of the MAX32660.
16 SWDCLK Serial Wire Debug Clock. Connected to P0.1 of the MAX32660.
17 GND Ground.
18 RESET Hardware Power Reset. Active-Low Input.
19 UART_TX UART Tx Data. Connected to P0.6 of the MAX32660.
20 UART_RX UART Rx Data. Connected to P0.7 of the MAX32660.
21 GND Ground.
22 SCLK SPI Clock. Connected to P0.12 of the MAX32660.
23 CS SPI Chip Select. Connected to P0.13 of the MAX32660.
24 MISO SPI Master Input, Slave Output. Connected to P0.10 of the MAX32660.
25 MOSI SPI Master Output, Slave Input. Connected to P0.11 of the MAX32660.
26 GND Ground.
27 VBATT 2.2 V to 5.5 V Supply.
28


Refer to the ADPD188BI and MAX32660 data sheets for details on the available functions of their respective GPIO pins.

The actual functions of the digital pins are user-configurable, and are determined by how the MAX32660 GPIO pins are configured in the SOM firmware. When changing the pin assignments, check if the new pinout will conflict with the onboard circuity of the the carrier board.

Do not set P0.0 and P0.1 to any other function besides SWDIO and SWDCLK to avoid issues with reprogramming the SOM using the carrier board.

If this was accidentally done and there is a need to upload a new firmware, the flash memory of the MAX32660 must first be erased prior to reprogramming. To do this, install Maxim Microcontrollers SDK and Visual Studio Code, then perform the following steps:

  1. Create a new project from MaximSDK’s examples for MAX32660 in Visual Studio Code.
  2. Build this project with the ‘build’ task in Visual Studio Code.
  3. Connect the RESET pin of the SOM to any GND pin.
  4. Run the ‘erase flash’ task in Visual Studio Code. (You may see a 'target not halted' message on the terminal, but this is expected).
  5. Disconnect the RESET pin of the SOM from GND.
  6. Power cycle the SOM by disconnecting the power source, and then immediately reconnecting it afterward.


UART Cable Connection

There are 4 test points on the SOM that can be used to access the UART port of the MAX32660 with an external cable. This can be used to configure the smoke detector module during run time, or stream the measured data back to a serial terminal program.


Pin Number Pin Name Function
1 1V8 Optional 1.8 V Supply. Alternative to VBATT.
2 GND Ground.
3 UART_RX UART Tx Data. Connected to P0.7 of the MAX32660.
4 UART_TX UART Rx Data. Connected to P0.6 of the MAX32660.


Input power to the SOM can be supplied either through the VBATT pins on the board castellation, or via pin 1 of JP1.
Refer to the table below on setting the JP1 and JP4 jumpers to select the power source.

Jumper Configuration Function
JP1 JP4
1:2 A/B Input power is sourced from the carrier board via the VBATT pins. Default.
2:3 B Input power is sourced from a UART cable via the P1 test points.


LED Supply Voltage Configuration

Depending on your specific power and application requirements, it may be desirable to only supply power to one of the internal LEDs of the ADPD188BI. Refer to the table below on setting the JP2 and JP3 jumpers to enable the LED supply voltages.

Jumper Configuration Function
JP2 A 5V supply for the ADPD188BI blue LED is enabled. Default.
B 5V supply for the ADPD188BI blue LED is disabled.
JP3 A 3.3V supply for the ADPD188BI infrared LED. Default.
B 3.3V supply for the ADPD188BI infrared LED.





Carrier Board

The EVAL-CN0583-CRR1 is a carier board designed to directly mount the EVAL-CN0583-SOM and emulate a traditional smoke detector application.



SOM Mounting

The two rows of pogo pins (P1, P2) are spring-loaded connectors used to mount the SOM. The SOM is inserted between these connectors “one side at a time” by aligning one castellated edge with a row of carrier board pogo pins, and then pressing into them. Once one row of pins has been pushed in, the other side of the SOM can be lowered and similarly inserted. Once released, the SOM will be mechanically secured with each of the castellated pin electrically connected with the pogo pins.



Power Source Options

Depending on the application requirements, input power to the SOM can be supplied in one of three ways. To select the power source, adjust the setting of JP1 as listed in the table below.

Jumper Configuration Input Power
JP1 BATTERY CR123A battery.
EXT. SUPPLY External 2.2V to 5.5V power via the P3 header.
USB POWER USB bus power via the P6 connector. Default.



Only the input power source of the SOM can be switched using jumper JP1. The onboard programmer/debugger on the carrier board will always draw power from the USB connector.


Push Buttons

There are two buttons on the CN0583 carrier board.

  1. The TEST button can be used as a user input in the smoke detector application loaded on the SOM (e.g. implementing a manual alarm test function). Connected to P0.2 of the MAX32660 on the SOM via pin 6 of P1.
  2. The UPDATE button is used when updating the firmware of the debugger. The debugger is normally programmed with a DAPLINK image that provides USB Mass Storage Device (MSD) drag-and-drop programming, USB Communications Device Class (CDC) virtual serial port, and UART communication with the MAX32660 on the SOM.



LED Indicators

There are two LEDs on the CN0583 carrier board.

  1. The ALARM LED can be used as a visual indicator in the smoke detection application loaded on the SOM (e.g. showing when an alarm condition is reached). This LED is connected to P0.4 of the MAX32660 on the SOM via pin 7 of P1.
  2. RGB LED is used in the debugger interface of the carrier board, and will blink when there is activity (e.g. sending commands to the SOM, updating the debugger firmware).


Buzzer

The buzzer on the carrier board can be used as an audible alarm for the smoke detector application loaded on the SOM. This is connected to P0.5 of the MAX32660 on the SOM via pin 5 of P1.


Data Storage

The carrier board includes a micro-SD card slot to enable storage of smoke data. To enable/disable this function, adjust the setting of jumper JP2 as listed in the table below.

Jumper Configuration Function
JP2 ON Enable micro-SD card functionality. Default.
OFF Disable micro-SD card functionality.


Programming the Debugger

The debugger circuit used in the carrier board is based on the MAX32625PICO application platform. By default, the included MAX32625 is already programmed with a bootloader and DAPLINK application firmware so that it can be used immediately out of the box. The included bootloader can be enabled by holding the UPDATE button while powering on the board. If necessary however, the MAX32625 can be reprogrammed via the SWD signals available on a keyed 10-pin connector (P7).

Pin Number Pin Name Function
1 VTREF Logic-Level Reference Voltage for the SWD interface. Connected to VDDIO (1.8V) of the MAX32625.
2 SWDIO SWD Data I/O . Connected to TMS/SWDIO of the MAX32625.
3 GND Ground.
4 SWCLK SWD Clock. Connected to TCK/SWDCLK of the MAX32625.
5 GND Ground.
6 DBG_TX UART Tx. Connected to P2.1 of the MAX32625.
7 NC No connection.
8 DBG_RX UART Rx. Connected to P2.0 of the MAX32625.
9 NC No connection.
10 RST Software Reset. Connected to SRSTN of the MAX32625.




CN0583 Example Demo


Demo Requirements

The following are required to implement the example CN0583 demo application:

  • ADPD188BI Smoke Chamber (Included with the SOM)
  • Micro-SD Card (Optional)
  • USB Micro-B Cable
  • Computer (Must have a serial terminal installed)


Hardware Setup

  1. Install the ADPD188BI smoke chamber on the primary side of the SOM.
  2. Carefully insert the SOM between P1 and P2 of the carrier board, following the cutout on the center. The proper orientation of the module will have pin 1 closest to the buzzer, and pin 28 on the side with the test button.
  3. Connect the P6 on the carrier board to the computer using the micro-USB cable.
  4. On the computer, check if the CN0583 hardware setup is recognized as a DAPLINK drive. This will indicate that the necessary drivers are complete and correct.


Serial Terminal Setup

A serial terminal is an application that runs on a PC or laptop that is used to display data and interact with a connected device (including many of the Circuits from the Lab reference designs). The device's UART peripheral is most often connected to a UART to USB interface IC, which appears as a traditional COM port on the host PC/ laptop. (Traditionally, the device's UART port would have been connected to an RS-232 line driver / receiver and connected to the PC via a 9-pin or 25-pin serial port.) There are many open-source applications, and while there are many choices, typically we use one of the following:

Before continuing, please make sure you download and install one of the above programs.

There are several parameters on all serial terminal programs that must be setup properly in order for the PC and the connected device to communicate. Below are the common settings that must match on both the PC side and the connected UART device.

  1. COM Port - This is the physical connection made to your PC or laptop, typically made through a USB cable but can be any serial communications cable. You can determine the COM port assigned to your device by visiting the device manager on your computer. Another method for identifying which COM port is associated with a USB-based device is to look at which COM ports are present before plugging in your device, then plug in your device, and look for a new COM port.
  2. Baud Rate - This is the speed at which data is being transferred from the connected device to your PC. These parameters must be the same on both devices or data will be corrupted. The default setting for most of the reference designs in 115200.
  3. Data Bits - The number of data bits per transfer. Typically, UART transmits ASCII codes back to the serial port so by default this is almost always set to 8-Bits.
  4. Stop Bits - The number of “stop” conditions per transmission. For the CN0583 demo, this should be set to 2 for redundancy.
  5. Parity - Is a way to check for errors during the UART transmission. Unless otherwise specified, set parity to “none”.
  6. Flow Control - Is a way to ensure that data lose between fast and slow devices on the same UART bus are not lost during transmission. This is typically not implemented in a simple system, and unless otherwise specified, set to “none”.


In many instances there are other options that each of the different serial terminal applications provide, such as local line echo or local line editing, and features like this can be turned on or off depending on your preferences. This setup guide will not go over all the options of each tool, but just the minor features that will make it easier to read back data from the connected devices.

Example setup using PuTTY

  1. Plug in your connected device using a USB cable or other serial cable.
  2. Wait for the device driver of the connected device to install on your PC or Laptop.
  3. Open your device manager, and find out which COM port was assigned to your device.


  4. Open up your serial terminal program (e.g., PuTTY)
  5. Click on the serial configuration tab or window, and input the settings to match the requirements of your connected device. The default baud rate for most of the reference designs is 115200. Make sure that you use the correct baud rate for your application.


  6. Ensure you click on the checkboxes for Implicit CR in every LF and Implicit LF in every CF.
  7. Ensure that local echo and line editing are enabled, so that you can see what you type and are able to correct mistakes. (Some devices may echo typed characters - if so, you will see each typed character twice. If this happens, turn off local echo.)


  8. Click on the open button, and as long as your connected device and serial terminal program are setup the same, than you should be able to start entering commands.


Available Commands

Typing help (or simply h) after the initial calibration sequence will display the list of commands and their shortened versions.

Function Short Command Verbose Command Description Example
Application Control h help Display the help tooltip.
s <no> stream <no> Put the device in GO mode and stream data from the device to the terminal.
<no> = number of samples to stream to the terminal. If left unspecified, this is automatically assumed infinite when s is executed.
To stream data indefinitely:
s

To stream only 5 samples:
s 5
i idle Stop the stream and put the device in program mode.
ms <opt> mode_set <opt> Set the output mode of the data.
<opt> = 'code' to stream data in codes; 'ptr' to stream data in PTR.
To set the output mode to PTR:
ms ptr
os <odr> odr_set <odr> Set the output data rate.
<odr> = new data rate.
To set the output data rate to 2.45 samples per second:
os 2.45
og odr_get Display the current output data rate.
n <string> note <string> Print user note on the console.
<string> = text to be printed.
To print 'Note 1' on the console:
n Note 1
SD Card Control fo <name> file_open <name> Open a text file (*.txt) on the micro-SD card to store data. If the specified text file does not exist, it will be created and saved on the card automatically.
<name> = name of the file to be opened.
To open 'file1.txt' on the micro-SD card:
fo file1
fc file_close Save changes to the currently open text file and close it.
ADPD188BI Control rr <addr> reg_read <addr> Read a specified ADPD188BI register and display its current value on the terminal.
«addr» = register address in hexadecimal.
To read register 0x0A:
rr a
rw <addr> <val> reg_write <addr> <val> Write a specified value to a ADPD188BI register.
«addr» = register address in hexadecimal.
«val» = value to be written to the register in hexadecimal.
To write '0x12C' to register '0x0A':
rw a 12c
rd reg_dump Reads and displays the values of all ADPD188BI registers.


By default, the output mode and data rate are set to PTR and 0.163 (1/6) samples per second, respectively.



Example Output Data

Below are examples of the CN0583 boards outputting data in PTR and raw codes and then exiting after several samples:




Device Driver Support

There are no-OS drivers provided for controlling the digital devices on the CN0583 boards.


Schematic, PCB Layout, Bill of Materials

CN0583 Design & Integration Files

  • Schematics
  • PCB Layout
  • Bill of Materials
  • Allegro Project
  • Assembly Drawing


Hardware Registration

Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. Register to receive all these great benefits and more!

End of Document

resources/eval/user-guides/circuits-from-the-lab/cn-0583/start.txt · Last modified: 07 Dec 2023 07:30 by Allan Uy