This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:aducm355_arduino_interposer [02 May 2019 04:03] – [Product Overview] erbe reyta | resources:eval:user-guides:circuits-from-the-lab:aducm355_arduino_interposer [03 Mar 2023 08:22] (current) – updated the design files download link Joyce Velasco | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== Description===== | ===== Description===== | ||
- | The Arduino interface can be found on many microprocessor development platforms and are a great way to begin prototyping a design. The EVAL-M355-ARDZ-INT was developed to enable quick and easy connection of the ADuCM355 based sensor boards to the EVAL-ADICUP3029 development board or any equivalent Arduino MCU controller boards. This allows for testing the functionality as well as the performance of the circuit using a controlled evaluation environment. | + | The Arduino interface can be found on many microprocessor development platforms and are a great way to begin prototyping a design. The [[adi>EVAL-M355-ARDZ-INT]] was developed to enable quick and easy connection of the ADuCM355 based sensor boards to the [[adi>EVAL-ADICUP3029]] development board or any equivalent Arduino MCU controller boards. This allows for testing the functionality as well as the performance of the circuit using a controlled evaluation environment. |
===== Product Overview ===== | ===== Product Overview ===== | ||
- | ADuCM355 base Sensor Shield Board Interface Connectors: | + | [[adi>ADuCM355]] base Sensor Shield Board Interface Connectors: |
- | {{: | + | {{: |
- | <note important> | + | <note important> |
Arduino Shield Board Interface Connectors: | Arduino Shield Board Interface Connectors: | ||
Line 22: | Line 22: | ||
{{ : | {{ : | ||
+ | \\ | ||
===== EVAL-M355-ARDZ-INT Power Rails ===== | ===== EVAL-M355-ARDZ-INT Power Rails ===== | ||
Line 82: | Line 82: | ||
- Set the UART switch(S2) on the EVAL-ADICUP3029 to the " | - Set the UART switch(S2) on the EVAL-ADICUP3029 to the " | ||
- Place EVAL-M355-ARDZ-INT on top of the EVAL-ADICUP3029{{ : | - Place EVAL-M355-ARDZ-INT on top of the EVAL-ADICUP3029{{ : | ||
- | - Placed on the desired number of ADuCM355 sensor daughter board on top of the interposer board.(up to 4){{ : | + | - Placed on the desired number of ADuCM355 sensor daughter board on top of the interposer board(up to 4). {{ : |
- Plug in EVAL-ADICUP3029 into USB port of computer using the micro USB cable. (You may need to wait for the ADICUP3029 device drivers to install if this is the first time the device was plugged in.) | - Plug in EVAL-ADICUP3029 into USB port of computer using the micro USB cable. (You may need to wait for the ADICUP3029 device drivers to install if this is the first time the device was plugged in.) | ||
Line 90: | Line 90: | ||
^ Webpage | ^ Webpage | ||
- | | [[http:// | + | | [[adi>cn0428|CN0428]] |
- | | [[http:// | + | | [[adi>cn0429|CN0429]] |
===== Software Available ===== | ===== Software Available ===== | ||
- | [[https:// | + | [[https:// |
===== Schematic, PCB Layout, Bill of Materials ===== | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
Line 101: | Line 101: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | EVAL-M355-ARDZ-INT | + | [[adi> |
- | * {{ : | + | * Schematic |
- | * {{ : | + | * PCB Layout |
- | * {{ : | + | * Bill of Materials |
- | * {{ : | + | * Allegro Project |
</ | </ | ||
+ | |||
+ | ===== Registration ===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
//End of Document// | //End of Document// |