Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:circuits-from-the-lab:aducm355_arduino_interposer [08 Nov 2018 09:33] – [SWD/JTAG Connector] erbe reyta | resources:eval:user-guides:circuits-from-the-lab:aducm355_arduino_interposer [03 Mar 2023 08:22] (current) – updated the design files download link Joyce Velasco |
---|
===== Description===== | ===== Description===== |
| |
The Arduino interface can be found on many microprocessor development platforms and are a great way to begin prototyping a design. The EVAL-M355-ARDZ-INT was developed to enable quick and easy connection of the ADuCM355 based sensor boards to the ADICuP3029 development board or any equivalent Arduino MCU controller boards. This allows for testing the functionality as well as the performance of the circuit using a controlled evaluation environment. | The Arduino interface can be found on many microprocessor development platforms and are a great way to begin prototyping a design. The [[adi>EVAL-M355-ARDZ-INT]] was developed to enable quick and easy connection of the ADuCM355 based sensor boards to the [[adi>EVAL-ADICUP3029]] development board or any equivalent Arduino MCU controller boards. This allows for testing the functionality as well as the performance of the circuit using a controlled evaluation environment. |
| |
===== Product Overview ===== | ===== Product Overview ===== |
| |
ADuCM355 base Sensor Shield Board Interface Connectors: | [[adi>ADuCM355]] base Sensor Shield Board Interface Connectors: |
{{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:aducm355_base_sensor_shield_actual.png?600 |}} | {{:resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:pin_header.jpg?600|}} |
| |
| <note important>Check if connectors P1, P2, P3 and P4 were correctly installed. The notch found for all headers should be at the bottom left near the header number 14 of the silk screen. </note> |
| |
Arduino Shield Board Interface Connectors: | Arduino Shield Board Interface Connectors: |
| |
{{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:sensor_board_connector_header.png?600 |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:sensor_board_connector_header.png?600 |}} |
| \\ |
===== EVAL-M355-ARDZ-INT Power Rails ===== | ===== EVAL-M355-ARDZ-INT Power Rails ===== |
| |
| |
| |
===== Switch Matrix =====-from-the-lab:eval-aducm355-ardz-int:swithch_matrix_actual.png?600 |}} | ===== Switch Matrix ===== |
| |
| {{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:swithch_matrix_actual.png?600 |}} |
===== Digital Communication Interfaces Supported ===== | ===== Digital Communication Interfaces Supported ===== |
| |
The debugger from the ADICuP3029 can be used and can be linked to the interposer board through the SWD_DEBUG (P10). The user can use a standard 10-pin ARM JTAG/SWD ribbon cable to connect to the ADICuP3029 debugger to the interposer board. | The debugger from the ADICuP3029 can be used and can be linked to the interposer board through the SWD_DEBUG (P10). The user can use a standard 10-pin ARM JTAG/SWD ribbon cable to connect to the ADICuP3029 debugger to the interposer board. |
| |
{{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:aducm3029_to_daughter_board_swd.png?600 |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:aducm3029_to_daughter_board_swd.png?400 |}} |
{{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:swd_debugger_connectors_actual.png?600 |}} | |
| |
There is a way to cut the SWD traces on the ADICUP3029 board right at the break away section of the board. By cutting the trace for the SWD_DIO and SWD_CLK located near P12 found from the ADICUP3029, this allows customers to program both the ADICUP3029 and M355-INT boards without losing the ability to stream serial data back to the USB port. | {{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:jtag_swd_10_connector.png?300 |}} |
{{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:swd_debugger_cut_trace.png?600 |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:swd_debugger_connectors_actual_1.png?600 |}} |
| |
| There is a way to cut the SWD traces on the ADICUP3029 board right at the break away section of the board. By cutting the trace for the SWD_DIO, SWD_CLK and SWD_RST located near P12. There are two(2) traces on the top of the board that must be cut using a knife, and one(1) trace found at the bottom of ADICUP3029 (the outter most trace), This allows customers to program both the ADICUP3029 and M355-INT boards without losing the ability to stream serial data back to the USB port. |
| {{:resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:adicup3029_primary_cut.png?400 |}}{{:resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:adicup3029_secondary_cut.png?400 |}}\\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ |
===== Debug/Programming Channel Selector for ADuCM355 Sensor Surf Boards ===== | ===== Debug/Programming Channel Selector for ADuCM355 Sensor Surf Boards ===== |
| |
- Set the UART switch(S2) on the EVAL-ADICUP3029 to the "USB" position in order to stream data back to the serial terminal. | - Set the UART switch(S2) on the EVAL-ADICUP3029 to the "USB" position in order to stream data back to the serial terminal. |
- Place EVAL-M355-ARDZ-INT on top of the EVAL-ADICUP3029{{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:shield_board_to_adicup_connections_actual.png?600 |}} | - Place EVAL-M355-ARDZ-INT on top of the EVAL-ADICUP3029{{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:shield_board_to_adicup_connections_actual.png?600 |}} |
- Placed on the desired number of ADuCM355 sensor daughter board on top of the interposer board.(up to 4){{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:sensor_shield_connections_actual.png?600 |}} | - Placed on the desired number of ADuCM355 sensor daughter board on top of the interposer board(up to 4). {{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:sensor_shield_connections_actual.png?600 |}} |
- Plug in EVAL-ADICUP3029 into USB port of computer using the micro USB cable. (You may need to wait for the ADICUP3029 device drivers to install if this is the first time the device was plugged in.) | - Plug in EVAL-ADICUP3029 into USB port of computer using the micro USB cable. (You may need to wait for the ADICUP3029 device drivers to install if this is the first time the device was plugged in.) |
| |
| |
^ Webpage ^ Application ^ EVAL-ADICUP3029 Software Available ^ | ^ Webpage ^ Application ^ EVAL-ADICUP3029 Software Available ^ |
| [[http://www.analog.com/cn0428|CN0428]] | Water Quality | Yes | | | [[adi>cn0428|CN0428]] | Water Quality | Yes | |
| [[http://www.analog.com/cn0429|CN0429]] | Gas Sensor | Yes | | | [[adi>cn0429|CN0429]] | Gas Sensor | Yes | |
| |
===== Software Available ===== | ===== Software Available ===== |
| |
[[https://github.com/analogdevicesinc/EVAL-ADICUP3029/tree/master/projects|EVAL-ADICUP3029 Source Code for CN0428 and CN0429]] | [[https://github.com/analogdevicesinc/EVAL-ADICUP3029/tree/master/projects/ADuCM3029_demo_cn0428_cn0429|EVAL-ADICUP3029 Source Code for CN0428 and CN0429]] |
| |
===== Schematic, PCB Layout, Bill of Materials ===== | ===== Schematic, PCB Layout, Bill of Materials ===== |
<WRAP round 80% download> | <WRAP round 80% download> |
| |
EVAL-M355-ARDZ-INT Design & Integration Files | [[adi>media/en/evaluation-documentation/evaluation-design-files/eval-m355-ardz-int-designsupport.zip|EVAL-M355-ARDZ-INT Design & Integration Files]] |
* {{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:02-051325-01-a.pdf |Schematics}} | * Schematic |
* {{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:05-051325-01-a.xlsx |Bill of Materials }} | * PCB Layout |
* {{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:051325a_fab.zip |Gerber Files}} | * Bill of Materials |
* {{ :resources:eval:user-guides:circuits-from-the-lab:eval-aducm355-ardz-int:051325a_assy.zip | Assembly Files }} | * Allegro Project |
</WRAP> | </WRAP> |
| |
| ===== Registration ===== |
| <WRAP round tip 80% > |
| Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. [[reg>EVAL-M355-ARDZ-INT?&v=Rev A|Register]] to receive all these great benefits and more!</WRAP> |
| |
//End of Document// | //End of Document// |