This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:arduino-uno:reference_designs:demo_cn0357 [18 Jan 2018 14:51] – [General Description/Overview] Mircea Caprioru | resources:eval:user-guides:arduino-uno:reference_designs:demo_cn0357 [03 Jan 2021 22:04] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Toxic Gas Detector using the Arduino Uno ====== | ====== Toxic Gas Detector using the Arduino Uno ====== | ||
- | The **CN0357_example** is a toxic gas(CO) detector demo project for the Arduino Uno base board with additional [[http:// | + | The **CN0357_example** is a toxic gas(CO) detector demo project for the Arduino Uno base board with additional [[adi>en/ |
\\ | \\ | ||
===== General Description/ | ===== General Description/ | ||
- | This user guide gives a detailed explanation about **CN0357_example** toxic gas (CO) detection project for Arduino base board and [[http:// | + | This user guide gives a detailed explanation about **CN0357_example** toxic gas (CO) detection project for Arduino base board and [[adi>en/ |
\\ | \\ | ||
{{ : | {{ : | ||
\\ | \\ | ||
- | The [[http:// | + | The [[adi>en/ |
\\ | \\ | ||
Line 35: | Line 35: | ||
- Plug the **EVAL-CN0357-ARDZ** shield on top of the **Arduino Uno** development board by matching up the **POWER, ANALOG, DIGI0, DIGI1** connectors. | - Plug the **EVAL-CN0357-ARDZ** shield on top of the **Arduino Uno** development board by matching up the **POWER, ANALOG, DIGI0, DIGI1** connectors. | ||
* Note, the boards should only plug together one way, preventing reverse connections. | * Note, the boards should only plug together one way, preventing reverse connections. | ||
- | - Connect your carbon monoxide(CO) sensor to the EVAL-CN0357-ARDZ via (**P1**). | + | - Connect your carbon monoxide(CO) sensor to the EVAL-CN0357-ARDZ via (**P1**).{{ : |
- | - Ensure the jumper **AD5720_CS** has a shunt across Pin 3 and Pin 4 of the **EVAL-CN0357-ARDZ** | + | |
- | - Ensure the jumper **AD7790_CS** has a shunt across Pin 1 and Pin 2 of the **EVAL-CN0357-ARDZ**{{ : | + | |
- Plug in the Type B USB cable into the USB port on the Arduino Uno, and the other end into the PC or laptop. | - Plug in the Type B USB cable into the USB port on the Arduino Uno, and the other end into the PC or laptop. | ||