This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:arduino-uno:reference_designs:demo_adxl372 [18 Jan 2018 09:46] – [Impact Measurement Demo using the Arduino Uno] Mircea Caprioru | resources:eval:user-guides:arduino-uno:reference_designs:demo_adxl372 [22 Jan 2018 08:47] (current) – [Project Structure] Mircea Caprioru | ||
---|---|---|---|
Line 2: | Line 2: | ||
This demo will use **EVAL-ADXL372-ARDZ** shield along with **Arduino Uno** base board to create a impact measurement application, | This demo will use **EVAL-ADXL372-ARDZ** shield along with **Arduino Uno** base board to create a impact measurement application, | ||
- | {{ : | + | {{ : |
===== General Description/ | ===== General Description/ | ||
Line 9: | Line 9: | ||
The **ADXL372** is an ultralow power, 3-axis, **±200 g** MEMS accelerometer. | The **ADXL372** is an ultralow power, 3-axis, **±200 g** MEMS accelerometer. | ||
+ | <note important> | ||
===== Demo Requirements ===== | ===== Demo Requirements ===== | ||
Line 22: | Line 23: | ||
===== Setting up the Hardware ===== | ===== Setting up the Hardware ===== | ||
- | FIXME | ||
- Plug the **EVAL-ADXL372-ARDZ** shield on top of the **Arduino Uno** development board by matching up the **POWER, ANALOG, DIGI0, DIGI1** connectors. | - Plug the **EVAL-ADXL372-ARDZ** shield on top of the **Arduino Uno** development board by matching up the **POWER, ANALOG, DIGI0, DIGI1** connectors. | ||
* Note, the boards should only plug together one way, preventing reverse connections. | * Note, the boards should only plug together one way, preventing reverse connections. | ||
- | - Make sure the jumpers **P8, P9, P6** are configured exactly as the picture below. | + | - Make sure the jumpers **P10, P11, P12** are configured exactly as the picture below. |
- | * P9 -> Pin 1-2 | + | * P10 -> Pin 1-2 |
- | * P8 -> Pin 2-3 | + | * P11 -> Pin 1-2 |
- | * P6 -> Pin 1-2 {{ : | + | * P12 -> Pin 1-2 |
+ | {{ : | ||
- Plug in the Type B USB cable into the USB port on the Arduino Uno, and the other end into the PC or laptop. | - Plug in the Type B USB cable into the USB port on the Arduino Uno, and the other end into the PC or laptop. | ||
Line 43: | Line 44: | ||
===== Project Structure===== | ===== Project Structure===== | ||
- | {{ : | + | {{ : |
The Arduino Sketch is used to load the example into Arduino IDE. The project is composed of three main parts: | The Arduino Sketch is used to load the example into Arduino IDE. The project is composed of three main parts: | ||
Line 49: | Line 50: | ||
* the main program (arduino sketch) | * the main program (arduino sketch) | ||
* application layer (IC drivers and sensor data) | * application layer (IC drivers and sensor data) | ||
+ | * communication layer | ||
===== Configuring the Software Parameters ===== | ===== Configuring the Software Parameters ===== | ||