Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:arduino-uno:reference_designs:demo_adxl362 [22 Jan 2018 08:47] – [Project Structure] Mircea Caprioruresources:eval:user-guides:arduino-uno:reference_designs:demo_adxl362 [23 Jan 2018 16:25] (current) – [General Description/Overview] Mircea Caprioru
Line 8: Line 8:
 The **ADXL362_example** uses the [[resources:eval:user-guides:eval-adicup360:hardware:adxl362|EVAL-ADXL362-ARDZ shield]] which has an **ADXL362 3-axis MEMS accelerometer** and a incorporated **NHD-C12832A1Z-NSW-BBW display** (128x32). The **ADXL362_example** uses the [[resources:eval:user-guides:eval-adicup360:hardware:adxl362|EVAL-ADXL362-ARDZ shield]] which has an **ADXL362 3-axis MEMS accelerometer** and a incorporated **NHD-C12832A1Z-NSW-BBW display** (128x32).
  
-{{:resources:eval:user-guides:eval-adicup360:reference_designs:adlx362_adicup360.jpg?450 |}}+{{:resources:eval:user-guides:arduino-uno:reference_designs:img_20180123_170819.jpg?400 |}}
  
 The application reads the ** X ** , ** Y **, and ** Z ** acceleration registers each **500 [ms]**. The acceleration in the 3 axes is displayed in **[mG]** on the LCD. Also this application demonstrates the usage of the motion switch. Movement zones - **UP**, **DOWN**, **RIGHT**, **LEFT**, **CENTER** - are displayed in the right side of the LCD.  The application reads the ** X ** , ** Y **, and ** Z ** acceleration registers each **500 [ms]**. The acceleration in the 3 axes is displayed in **[mG]** on the LCD. Also this application demonstrates the usage of the motion switch. Movement zones - **UP**, **DOWN**, **RIGHT**, **LEFT**, **CENTER** - are displayed in the right side of the LCD. 
resources/eval/user-guides/arduino-uno/reference_designs/demo_adxl362.txt · Last modified: 23 Jan 2018 16:25 by Mircea Caprioru