Wiki

This version is outdated by a newer approved version.DiffThis version (09 Nov 2018 11:58) is a draft.
Approvals: 0/1

This is an old revision of the document!


AgileNet 6T (AN6T) Wireless Networking Protocol Solutions

AgileNet 6T is a long range Sub-GHz wireless networking solution used in the applications ​such as Emergency Lighting, ​Commercial Agriculture,​Commercial Environment monitoring ​which are highly reflective and have multi-path environments.

AgileNet 6T is based on 6TiSCH. 6TiSCH is combining the performance of IEEE802.15.4e TSCH with an IPv6-enabled upper stack. TSCH aims at reducing the impact of the wireless medium unpredictability to enable the use of reliable low-power wireless networks. It is very good at saving the nodes' energy because each node shares a schedule, allowing it to know in advance when to turn on or off its radio. The IEEE 802.15.4 standard uses different frequency band, and each frequency band is separated in channels. In TSCH, communications are done using those different channels and at different times.

AN6T Solution Architecture

resources/eval/user-guides/agilenet6t.1541761114.txt.gz · Last modified: 09 Nov 2018 11:58 by Mahendravarman rajarao