This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:agilenet6t [04 Sep 2019 15:21] – Aditya S | resources:eval:user-guides:agilenet6t [18 Sep 2019 11:24] – Added steps to download ANet SW package and links to other wiki pages Aditya S | ||
---|---|---|---|
Line 4: | Line 4: | ||
AgileNet 6T is based on 6TiSCH. 6TiSCH is combining the performance of IEEE802.15.4e TSCH with an IPv6-enabled upper stack. The IEEE 802.15.4 standard uses different frequency band, and each frequency band is separated in channels. In TSCH, communications are done using those different channels and at different times. However, IEEE 802.15.4 standard does not define how to build and maintain the communication schedule. AN6T Wireless networking solution defines to organize the communication schedule in a distributed way. | AgileNet 6T is based on 6TiSCH. 6TiSCH is combining the performance of IEEE802.15.4e TSCH with an IPv6-enabled upper stack. The IEEE 802.15.4 standard uses different frequency band, and each frequency band is separated in channels. In TSCH, communications are done using those different channels and at different times. However, IEEE 802.15.4 standard does not define how to build and maintain the communication schedule. AN6T Wireless networking solution defines to organize the communication schedule in a distributed way. | ||
- | ====== AN6T Wireless Solution Architecture | + | ===== AN6T Wireless Solution Architecture ===== |
Line 17: | Line 17: | ||
* Secured Communication | * Secured Communication | ||
+ | ===== AN6T Stack Architecture ===== | ||
+ | {{: | ||
- | ====== AN6T Stack Architecture ====== | ||
- | {{: | + | ===== AGILENET-6T SOFTWARE PACKAGE ===== |
+ | ==== INSTALLING THE AGILENET-6T SOFTWARE PACKAGE ==== | ||
+ | Download the AgileNet-6T software by filling in the request form at https:// | ||
+ | - Fill in the requested information under the Software Recipient Information and Commercial information sections. | ||
+ | - Under the Software requested section, set Target hardware to Ultra Low Power Microcontrollers, | ||
+ | - After the request is approved, a link to download the software is sent to the provided email address. | ||
+ | - Use the link to install the AgileNet-6T software package. | ||
+ | ===== Additional resources ===== | ||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | * [[resources: |