This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:adrv936x_rfsom:hardware [30 May 2019 17:24] – [Revision F] Travis Collins | resources:eval:user-guides:adrv936x_rfsom:hardware [06 Oct 2021 14:54] – [Dimensions] Robin Getz | ||
---|---|---|---|
Line 2: | Line 2: | ||
Whether you want to understand the changes between revisions, or just understand how to probe the PCB, this is where all the information should be. | Whether you want to understand the changes between revisions, or just understand how to probe the PCB, this is where all the information should be. | ||
+ | |||
+ | ===== ADRV936x - Mechanical ===== | ||
+ | |||
+ | The ADRV9361-Z7035 SDR 2X2 SOM uses a 20 layer PCB that measures 2.440” x 3.937” (62 mm x 100 mm). The 62mm x 100mm form factor is compatible with the DP10062 “Sick of Beige v1.0” specification from dangerousprototypes.com. | ||
+ | |||
+ | ==== Connectors ==== | ||
+ | |||
+ | The MicroHeaders used on ADRV9361-Z7035 are FCI 0.8mm BergStak®100-position Dual Row, BTB Vertical Receptacles (61082-101400LF). These receptacles mate with any of the FCI 0.8mm BergStak® 100-position Dual Row BTB Vertical Plugs (61083-10x400LF) to provide variable stack heights of 5mm, 6mm, 7mm or 8mm. The SOM uses the FCI “receptacle” while carrier cards use the “plug”. Both receptacle and plug include a PCB locator peg that can be used to design precisely mated SOM and carrier layouts. | ||
+ | |||
+ | {{ : | ||
+ | | ||
+ | More information about these connectors can be found [[http:// | ||
+ | |||
+ | ==== Dimensions ===== | ||
The physical dimensions of the connectors, mounting holes and PCB is common between the ADRV9361-Z7035 and the ADRV9364-Z7020. | The physical dimensions of the connectors, mounting holes and PCB is common between the ADRV9361-Z7035 and the ADRV9364-Z7020. | ||
Line 7: | Line 21: | ||
<WRAP round download> | <WRAP round download> | ||
The Footprint is common between the two parts: | The Footprint is common between the two parts: | ||
- | | + | |
+ | * Carrier Card Connector Dimensions: | ||
+ | * {{: | ||
+ | * ADRV9361-Z7035 Step file: {{ : | ||
+ | </ | ||
+ | ==== Pinout ===== | ||
+ | |||
+ | <WRAP round download> | ||
The connector pinouts are a superset: | The connector pinouts are a superset: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
- | |||
- | Carrier Card Connector Dimensions: | ||
- | * {{: | ||
</ | </ | ||
Line 20: | Line 38: | ||
==== Revision F ==== | ==== Revision F ==== | ||
- | Still under review. | + | This is the current shipping version. |
<WRAP round download> | <WRAP round download> | ||
- | * {{: | + | * {{: |
+ | * {{ : | ||
+ | * {{ : | ||
</ | </ | ||
+ | * Changes from Rev E to Rev F: | ||
+ | * The schematic did not change. We only made an adjustment to the layout. | ||
+ | * The RF traces were modified to improve the insertion loss and the return loss as well as the EVM. | ||
+ | * This resulted in some layout changes for discrete capacitors | ||
+ | * On the SOM the revision is shown as " | ||
+ | * The reset button moved position | ||
+ | |||
==== Revision E ==== | ==== Revision E ==== | ||
+ | |||
<WRAP round download> | <WRAP round download> | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
- | * {{: | + | * {{: |
</ | </ | ||
- | === Why do a Rev F? === | ||
- | * The schematic did not change. We only made an adjustment to the layout. | ||
- | * The RF traces were modified to improve the insertion loss and the return loss as well as the EVM. | ||
==== Revision C (First publicly available revision) ==== | ==== Revision C (First publicly available revision) ==== | ||
Line 66: | Line 91: | ||
* This has the notation error described above. | * This has the notation error described above. | ||
* {{: | * {{: | ||
- | * {{ : | + | * {{ : |
</ | </ | ||
Line 82: | Line 107: | ||
* Added a [[wp> | * Added a [[wp> | ||
* Improved the RF traces to have better insertion loss and return loss. | * Improved the RF traces to have better insertion loss and return loss. | ||
+ | |||
+ | ===== Carrier Support ===== | ||
+ | |||
+ | The ADRV9361-Z7035 supports all features on the [[adi> | ||
===== Support ===== | ===== Support ===== |