The Quick Start Guides provide a simple step by step instruction on how to do an initial system setup for the EVAL-ADRV9026/ADRV9029 boards on various FPGA development boards. They will discuss how to program the bitstream, run a no-OS program, or boot a Linux distribution.
The EVAL-ADRV9026/ADRV9029 is, by definition a “FPGA mezzanine card” (FMC), that means it needs a carrier to plug into. The carriers we support are:
Board | EVAL-ADRV9026/ADRV9029 |
---|---|
ZCU102 | √ |
Arria 10 SoC | WIP |
The supported OS are:
Board | HDL | Linux Software | No-OS Software |
---|---|---|---|
ZCU102 | √ | √ | √ |
Arria 10 SoC | WIP | WIP | WIP |
The EVAL-ADRV9026/ADRV9029 boards connects to the HPC1 connector (unless otherwise noted). The carrier setup requires power (12VDC 3A MAX), UART (115200), ethernet (Linux), HDMI (if available) and/or JTAG (no-OS) connections. A few typical setups are shown below.
Detailed description of the setup procedure for ADRV9009 (similar procedure for ADRV9026/9029):