Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:adrv9009:quickstart:zynqmp [05 Jun 2018 14:33] – add picture Michael Hennerichresources:eval:user-guides:adrv9009:quickstart:zynqmp [03 Sep 2020 20:17] (current) – Explicitly stated the position of the SW6 switch for booting from the SD Card Adrian Costina
Line 34: Line 34:
   * Connect USB UART J83 (Micro USB) to your host PC.   * Connect USB UART J83 (Micro USB) to your host PC.
   * Insert SD card into socket.   * Insert SD card into socket.
-  * Configure ZCU102 for SD BOOT. +  * Configure ZCU102 for SD BOOT (mode SW6[4:1] switch in the position **OFF,OFF,OFF,ON** as seen in the below picture)
   * Turn on the power switch on the FPGA board.   * Turn on the power switch on the FPGA board.
   * Observe kernel and serial console messages on your terminal. (use the first ttyUSB or COM port registed)    * Observe kernel and serial console messages on your terminal. (use the first ttyUSB or COM port registed) 
resources/eval/user-guides/adrv9009/quickstart/zynqmp.1528202037.txt.gz · Last modified: 05 Jun 2018 14:33 by Michael Hennerich