This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:adrv9009:quickstart:zynqmp [05 Jun 2018 14:33] – add picture Michael Hennerich | resources:eval:user-guides:adrv9009:quickstart:zynqmp [03 Sep 2020 20:17] (current) – Explicitly stated the position of the SW6 switch for booting from the SD Card Adrian Costina | ||
---|---|---|---|
Line 34: | Line 34: | ||
* Connect USB UART J83 (Micro USB) to your host PC. | * Connect USB UART J83 (Micro USB) to your host PC. | ||
* Insert SD card into socket. | * Insert SD card into socket. | ||
- | * Configure ZCU102 for SD BOOT. | + | * Configure ZCU102 for SD BOOT (mode SW6[4:1] switch in the position **OFF, |
* Turn on the power switch on the FPGA board. | * Turn on the power switch on the FPGA board. | ||
* Observe kernel and serial console messages on your terminal. (use the first ttyUSB or COM port registed) | * Observe kernel and serial console messages on your terminal. (use the first ttyUSB or COM port registed) |