This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:adrv9009-zu11eg [22 Dec 2020 17:06] – Brian OLoughlin | resources:eval:user-guides:adrv9009-zu11eg [23 Dec 2020 12:29] – Brian OLoughlin | ||
---|---|---|---|
Line 5: | Line 5: | ||
The RF-SOM can be used as a sub-part in a larger customer system or as an evaluation and prototyping platform. | The RF-SOM can be used as a sub-part in a larger customer system or as an evaluation and prototyping platform. | ||
To use the RF-SOM for evaluation and prototyping a carrier board is required. The Analog Devices ADRV2CRR-FMC Carrier board is designed for this purpose, or a customer can develop their own custom carrier or system board. | To use the RF-SOM for evaluation and prototyping a carrier board is required. The Analog Devices ADRV2CRR-FMC Carrier board is designed for this purpose, or a customer can develop their own custom carrier or system board. | ||
- | An additional RF board can also be fitted to the carrier to further expand the system up to 8 Tx and Rx radio channels. | + | An additional RF Transceiver |
**The RF-SOM box includes:** | **The RF-SOM box includes:** |