This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:adrv9009-zu11eg:syncronization [13 Oct 2021 11:09] – [Clock distribution] Claudia Goga | resources:eval:user-guides:adrv9009-zu11eg:syncronization [21 Feb 2024 09:06] (current) – [Reference distribution] Michael Hennerich | ||
---|---|---|---|
Line 30: | Line 30: | ||
| dts | [[linux.github> | | dts | [[linux.github> | ||
| dts | [[linux.github> | | dts | [[linux.github> | ||
+ | |||
+ | <note warning> | ||
+ | Depending on the Linux/ | ||
+ | [[repo> | ||
+ | |||
+ | < | ||
+ | arch: arm64: adrv9009-zu11eg: | ||
+ | To match default AD-SYNCHRONA14-EBZ configuration: | ||
+ | |||
+ | CH8 - HMC7044 CLKOUT4 - CMOS | ||
+ | CH10 - HMC7044 CLKOUT5 - LVPECL AC-COUPLED | ||
+ | CH6 - HMC7044 CLKOUT6 - CMOS | ||
+ | CH9 - HMC7044 CLKOUT12 - LVPECL AC-COUPLED | ||
+ | </ | ||
+ | </ | ||
==== Clock distribution ==== | ==== Clock distribution ==== | ||
Line 45: | Line 60: | ||
* Replace C18, C19, C236, C240 with 0 Ohm resistors | * Replace C18, C19, C236, C240 with 0 Ohm resistors | ||
* Replace C289, C290 with 0 Ohm resistors | * Replace C289, C290 with 0 Ohm resistors | ||
- | * Unload 0 Ohm resistors from location R77, R112 and load to R110, R112 | + | * Unload 0 Ohm resistors from location R77, R112 and insert |
+ | Rev C.1: | ||
+ | * Replace C289, C290 with 0 Ohm resistors | ||
+ | * Unload 0 Ohm resistors from location R77, R112 and insert to R110, R111 | ||
</ | </ | ||
- | | C289 | bypass/ | ||
- | | C290 | bypass/ | ||
- | | R110 | insert/ | ||
- | | R111 | insert/ | ||
^ Function ^ File ^ | ^ Function ^ File ^ | ||
Line 89: | Line 103: | ||
===== Software ===== | ===== Software ===== | ||
- | * 11/ | + | * [[:resources:tools-software:linux-software:kuiper-linux |Analog Devices Kuiper Linux]] |
- | * {{ :resources:eval:user-guides:adrv9009-zu11eg:adrv9009_zu11eg_fmcomms8_nov9_2020.zip |ADRV9009-ZU11EG+FMCOMMMS8 Boot Files}} | + | |
- | * 02/ | + | |
- | * {{ : | + | |
- | * {{ : | + | |
<note tip>The board which connects the external HMC7044 clockchip is refered as **primary** and requires the devicetree (system.dtb) from the primary folder in the archive. Likewise the board without the external clockchip connected is called **secondary**, | <note tip>The board which connects the external HMC7044 clockchip is refered as **primary** and requires the devicetree (system.dtb) from the primary folder in the archive. Likewise the board without the external clockchip connected is called **secondary**, |