This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:adrv9009-zu11eg:syncronization [27 May 2021 15:52] – [Theory of Operation] Laszlo Nagy | resources:eval:user-guides:adrv9009-zu11eg:syncronization [15 Jun 2021 14:32] – [Clock distribution] Michael Hennerich | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== ADRV9009-ZU11EG Multi-SOM Synchronization ====== | ====== ADRV9009-ZU11EG Multi-SOM Synchronization ====== | ||
- | .... | + | |
+ | ===== Clock tree synchronization considerations ===== | ||
+ | |||
+ | The HMC7044 used throughout the entire clock-tree in this design supports two alternative synchronizations modes and methods. Both modes may have their own benefits and tradeoffs, such as Jitter, Correlated Close in Phase Noise, Timing Requirements, | ||
+ | We recommend planning for and evaluating both options. | ||
+ | |||
+ | We provide device-trees for both methods. | ||
+ | |||
+ | ==== Reference distribution ==== | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | A lower frequency reference is used between different levels in the clock tree (Inter-stage Frequency). All clock-chips in the hierarchy require its own local VCXO and this reference is used to lock the VCXO using PLL1 to the external reference. Any of the four available reference inputs '' | ||
+ | |||
+ | A additional '' | ||
+ | |||
+ | ==== Clock distribution ==== | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | The maximum frequency used in the system is generated by the topmost HMC7044 and then distributed throughout the entire clock tree (Inter-stage Frequency). | ||
+ | This method bypasses the PLL1 and PLL2 of all clock chips below the TOP chip. All lower level clock-chips act as clock fanout buffers, where only the clock distribution network output dividers can be used. | ||
+ | This method is referred as **clock distribution**. All lower level clock-chips receive their input clock via '' | ||
+ | |||
+ | Depending on your [[resources: | ||
+ | |||
+ | | C289 | bypass/ | ||
+ | | C290 | bypass/ | ||
+ | | R110 | insert/ | ||
+ | | R111 | insert/ | ||
===== Hardware setup ===== | ===== Hardware setup ===== |