This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:adrv9009-zu11eg:syncronization [17 Jun 2021 09:17] – [Clock distribution] Michael Hennerich | resources:eval:user-guides:adrv9009-zu11eg:syncronization [17 Jun 2021 09:22] – [Clock distribution] Michael Hennerich | ||
---|---|---|---|
Line 38: | Line 38: | ||
This method is referred as **clock distribution**. All lower level clock-chips receive their input clock via '' | This method is referred as **clock distribution**. All lower level clock-chips receive their input clock via '' | ||
+ | <note tip>This mode also allows for TRX baseband rates that would be otherwise not possible with the default installed VCXO of 122.880MHz. Let's say someone needs exactly 250.000MSPS. This becomes possible by providing a 500.000MHz or 1000.000MHz external clock.</ | ||
+ | |||
Depending on your [[resources: | Depending on your [[resources: | ||