This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:admx:eval-admx2001ebz [22 Apr 2024 22:33] – Updated to cover 1.2.2 new features, firmware updates, enhanced images and added full pinout Slater Campbell | resources:eval:user-guides:admx:eval-admx2001ebz [26 Apr 2024 20:00] (current) – updated ToC and added FW update image Slater Campbell | ||
---|---|---|---|
Line 423: | Line 423: | ||
</ | </ | ||
- | === Calibration Steps === | + | ==== Calibration Steps ==== |
To calibrate the module in a specific gain combination, | To calibrate the module in a specific gain combination, | ||
- Select the desired measurement configuration (gain, frequency, magnitude and offset) | - Select the desired measurement configuration (gain, frequency, magnitude and offset) | ||
Line 455: | Line 455: | ||
</ | </ | ||
- | === Example === | + | ==== Calibration |
Calibrate the gain setting (0, 1) at 100kHz with a resistor of value 1k Ohms. The true resistance Rt from the E4980A at 100kHz was measured as 1000.019 Ohms, and the true reactance Xt was 0.822 Ohms. | Calibrate the gain setting (0, 1) at 100kHz with a resistor of value 1k Ohms. The true resistance Rt from the E4980A at 100kHz was measured as 1000.019 Ohms, and the true reactance Xt was 0.822 Ohms. | ||
< | < | ||
Line 510: | Line 510: | ||
</ | </ | ||
- | === Reading and Writing Calibration Coefficients === | + | ==== Reading and Writing Calibration Coefficients |
Calibration coefficients for each gain can be read to the terminal, and written back to the device. This allows the user to save coefficients for multiple different test setups, conditions, or frequencies. | Calibration coefficients for each gain can be read to the terminal, and written back to the device. This allows the user to save coefficients for multiple different test setups, conditions, or frequencies. | ||
To read the currently loaded coefficients for a certain gain setting, run the command '' | To read the currently loaded coefficients for a certain gain setting, run the command '' | ||
Line 536: | Line 536: | ||
This process should be repeated for all coefficients for a given gain to be valid. If using other gains, the coefficients will need to be stored for them too. Then, they must be saved using '' | This process should be repeated for all coefficients for a given gain to be valid. If using other gains, the coefficients will need to be stored for them too. Then, they must be saved using '' | ||
- | === Calibration Over Frequency === | + | ---- |
+ | ==== Calibration Over Frequency | ||
Starting in firmware version 1.2.2, calibration over frequency support is implemented. This means that all 16 gain settings can be fully calibrated at multiple frequency points. The process for calibrating over frequency is the same as single point calibration, | Starting in firmware version 1.2.2, calibration over frequency support is implemented. This means that all 16 gain settings can be fully calibrated at multiple frequency points. The process for calibrating over frequency is the same as single point calibration, | ||
Line 552: | Line 553: | ||
The commands for reading and writing calibration coefficients detailed in [[eval-admx2001ebz# | The commands for reading and writing calibration coefficients detailed in [[eval-admx2001ebz# | ||
- | === Preloaded Calibration Sets === | + | ==== Preloaded Calibration Sets ==== |
Version 1.2.2 also adds support for ADMX2001B modules to ship with a set of calibration coefficients intended to help with evaluating the board. Although the firmware supports it, boards that are currently shipping will not have calibration coefficients preloaded. This will be a future development. | Version 1.2.2 also adds support for ADMX2001B modules to ship with a set of calibration coefficients intended to help with evaluating the board. Although the firmware supports it, boards that are currently shipping will not have calibration coefficients preloaded. This will be a future development. | ||