This shows you the differences between two versions of the page.
— | resources:eval:user-guides:admx:admx100x [06 Apr 2021 04:33] – Added typical performance specs Gustavo Castro | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== ADMX1002, Ultra-low Distortion and Low Noise Signal Generator ====== | ||
+ | ==== Features ==== | ||
+ | - SPI and ATE Communication | ||
+ | - On-board supply | ||
+ | - External common mode voltage option | ||
+ | - Sync In & Sync Out for Coherent Sampling | ||
+ | - External output clamp voltage option | ||
+ | - Differential to Single Ended Conversion | ||
+ | ==== Package Contents ==== | ||
+ | - EVAL-ADMX100X-FMCZ evaluation board | ||
+ | - 12V wall adapter Power Supply | ||
+ | - 6-pin PMOD cable kit | ||
+ | ==== Additional Equipment Needed ==== | ||
+ | - ADMX1002 Module | ||
+ | - [[adi> | ||
+ | - [[adi> | ||
+ | - SMA cables for output connection | ||
+ | ==== Software Needed ==== | ||
+ | * ADMX1002 sourcing GUI | ||
+ | * The user needs to request the GUI download package through the Software Request Form. Bellow is the link to the " | ||
+ | * [[https:// | ||
+ | ===== General Description ===== | ||
+ | The ADMX1002 module is an ultra-low distortion and low noise signal generator. It offers a frequency range up to 40 kHz. ADMX1002 can be used with digital pre distortion (DPD) algorithm of up to 20 kHz and has distortion performance up to 130dB typical at 1 kHz. A flexible digital interface allows for easy integration into any system. | ||
+ | The EVAL-ADMX100X-FMCZ evaluation kit demonstrates the best in class signal source performance of the ADMX1002 module. The module can be shown to achieve better that -125dB THD, with SNR figures typically greater that 117dB. The evaluation board kit includes an intuitive GUI for sourcing. This interface communicates to the module via a USB to SPI through the [[adi> | ||
+ | ===== EVAL-ADMX100X-FMCZ Evaluation Board ===== | ||
+ | Figure 1 shows the EVAL-ADMX100X-FMCZ evaluation board. Followings are the connectors, inputs and outputs related to this evaluation board: | ||
+ | * ADMX1002 Module connector: The ADMX1002 module is connected to the EVAL-ADMX100X-FMCZ evaluation board via (P5) module connector. | ||
+ | * Source PMOD header: | ||
+ | * Power Supply: The EVAL-ADMX100X-FMCZ evaluation board is powered from a 12V wall adaptor via P14. The evaluation board provides on-board supply regulators to generate the +3.3V and ±9V required to power the module. | ||
+ | * SMA connectors description are summarized is Table 1. | ||
+ | * Jumpers and Switch Setup are summarized is Table 2. | ||
+ | **Table 1. SMA Connector**\\ | ||
+ | |||
+ | ^Connector | ||
+ | |OUTP | ||
+ | |OUTN | ||
+ | |SINGLE ENDED OUTPUT |Source single ended output| | ||
+ | |INN |Reserved| | ||
+ | |INP |Reserved| | ||
+ | |ACQ_SYNC_IN | ||
+ | |SYNC_IN | ||
+ | |||
+ | **Table 2. Jumper and Switch Setup**\\ | ||
+ | |||
+ | ^Name ^Function | ||
+ | |P4 |VCM from DAC or EXT |1-2 (VCM_DAC)| | ||
+ | |P6 |EN | ||
+ | |P8 |Sense Input Clamp to +5V |Inserted| | ||
+ | |P9 |Sense Input Clamp to -5V |Inserted| | ||
+ | |P11 |Reserved | ||
+ | |P12 |Reserved | ||
+ | |P13 |Reserved | ||
+ | |S1 |Reserved | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 1. EVAL-ADMX100X-FMCZ Evaluation Board// | ||
+ | </ | ||
+ | |||
+ | ==== QUICK START GUIDE ==== | ||
+ | Figure 2 illustrates the required setup to evaluate the ADMX1002 module. The following equipment are required to perform a full evaluation: | ||
+ | - ADMX1002 module | ||
+ | - EVAL-ADMX100X-FMCZ kit that contains: | ||
+ | - EVAL-ADMX100X-FMCZ evaluation board | ||
+ | - Power adaptor | ||
+ | - 6-pin PMOD cable | ||
+ | - [[adi> | ||
+ | - [[adi> | ||
+ | - Windows 10 | ||
+ | - SMA cables for connection from EVAL-ADMX100X-FMCZ evaluation board to analyzer or oscilloscope | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 2. Evaluation Board Connection// | ||
+ | </ | ||
+ | |||
+ | ==== SETUP ==== | ||
+ | Figure 4 depicts the full evaluation setup. Follow the steps below to set up the full evaluation board. | ||
+ | - Check Jumper & Switch settings (see Table 2.) | ||
+ | - Connect ADMX1002 module to the module connector (P5) on EVAL-ADMX100X-FMCZ evaluation board | ||
+ | - Connect the SDP_S or SDP_B controller board to the SDP-I-PMD interposer board | ||
+ | - Put jumper JP1 into SPI position (see Figure 3.). | ||
+ | - <fc # | ||
+ | - Connect the SDP-I-PMD interposer board to the “SOURCE/ | ||
+ | - Connect the gender changer to one end of the 6-pin PMOD cable | ||
+ | - <fc # | ||
+ | - <fc # | ||
+ | - Connect USB Cable from PC to SDP-S or SDP-B | ||
+ | - Apply the SDP-I-PMD interposer board power and wait for 10 seconds | ||
+ | - Apply the EVAL-ADMX100X-FMCZ evaluation board power | ||
+ | * After the power is applied, the " | ||
+ | * <fc # | ||
+ | - Start ADI ADMX1002 GUI and press Connect (see " | ||
+ | - You should see the firmware number "FW: 3.1.0.0" | ||
+ | - <fc # | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | Figure 3. SDP-I-PMD Interposer Board Jumper Connection | ||
+ | </ | ||
+ | |||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 4. Complete Evaluation Setup// | ||
+ | </ | ||
+ | |||
+ | ===== SOFTWARE INSTALLATION ===== | ||
+ | ==== INSTALLING THE SYSTEM DEMONSTRATION PLATFORM DRIVERS ==== | ||
+ | If you have not installed the System Demonstration Platform (SDP) drivers already, you need to download and install it first before installing the ADMX1002 GUI. Bellow you can find the SDP USB driver installer and the installation instruction. | ||
+ | * [[http:// | ||
+ | * {{ : | ||
+ | |||
+ | ==== INSTALLING THE ADMX1002 GUI ==== | ||
+ | To install the ADMX1002 sourcing GUI, take the following steps: | ||
+ | * To download the ADMX1002 software GUIs, sign in to your “myAnalog” account and click on “Resources” and then click on “Special” tab to find the " | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 5. ADMX1002 zip file to be downloaded from myAnalog account// | ||
+ | </ | ||
+ | |||
+ | * Download and unzip the " | ||
+ | * ADMX1002_SDP_Scripting_Tool: | ||
+ | * ADMX1002AWG_Generator: | ||
+ | * GUI-Installer: | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 6. ADMX1002 folder to Download ADMX1001 GUI// | ||
+ | </ | ||
+ | |||
+ | * After Unzipping the " | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 7. Beginning of ADMX1002 Sourcing GUI Setup// | ||
+ | </ | ||
+ | |||
+ | * Accept the license agreement (see Figure 8). | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 8. ADMX1002 Sourcing GUI License Agreement// | ||
+ | </ | ||
+ | |||
+ | * Select the location to install the software, and then click Next. Figure 9 shows the default locations, which are displayed when the window opens; select another location by clicking Browse. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 9. Selecting the Location for Software Installation// | ||
+ | </ | ||
+ | |||
+ | * The installer is now ready to install. Click Next to continue (see Figure 10). | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 10. Confirm Installation// | ||
+ | </ | ||
+ | |||
+ | * 7. Close after installation has completed (see Figure 11). | ||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 11. Indicating When the Installation is Complete// | ||
+ | </ | ||
+ | |||
+ | ===== SOFTWARE OPERATION ===== | ||
+ | ==== ADMX1002 SOURCING GUI TOOLBAR AND STATUSBAR OVERVIEW ==== | ||
+ | * (A) Connect/ | ||
+ | * (B) Run – This button runs the signal. | ||
+ | * (C) Stop – This button stops any running signal. | ||
+ | * (D) Calibrate – This button runs the digital pre distortion (DPD) algorithm. | ||
+ | * (E) Trigger Mode – Use this to change selection to either “Continuous” or “Single-shot”. | ||
+ | * (F) Signal Type – Use this to change selection to either “Alternating”, | ||
+ | * (G) Write – This button writes the “set” values and reads the “generated” parameters to the ADMX1002 module. The generated parameters will then be displayed at the Generated Parameters Panel. | ||
+ | * (H) Set Parameters Configuration – Amplitude and Frequency levels can be changed here. | ||
+ | * (I) Profile Save | ||
+ | * (J) Profile Load | ||
+ | * (K) Use Profile checkbox – Check when loading profiles; otherwise, uncheck. | ||
+ | * (L) Set the maximum number of profiles. | ||
+ | * (M) Profile Id – Change id accordingly. | ||
+ | * (N) Signal Plot – Shows the signal preview. | ||
+ | * (O) Generated Parameters Panel – Displays parameters read from the module. | ||
+ | * (P) Status Message – The status of the software will be displayed here. | ||
+ | * (Q) Timer – Shows the timer on some status. During running, DPD algorithm, and writing of AWG data, a timer will be shown. | ||
+ | * (R) POST/BIST | ||
+ | * (S) Opens the Log Window | ||
+ | * (T) Opens the Registers Read/Write Window | ||
+ | * (U) Versioning – Firmware Version, Verilog Version and PCB Version | ||
+ | * (V) Module ID | ||
+ | * (W) SPI Data Rate | ||
+ | * (X) Controller Board Type – Defaulted to SDP | ||
+ | * (Y) Help | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 12. ADMX1002 Sourcing GUI overview// | ||
+ | </ | ||
+ | |||
+ | ==== RUN WITHOUT DIGITAL PRE-DISTORTION (DPD) ==== | ||
+ | The following sequence shall produce a signal without (DPD) algorithm (see Figure 5 for the label): | ||
+ | - Set desired parameters (H). | ||
+ | - WRITE parameters (G). Panel in (O) will display the generated configuration of the signal. | ||
+ | - RUN parameters (B). The Status Bar (P) should display “Ready” and the timer beside it should start. This means that the ADMX1002 module is now processing the configuration. It should change to " | ||
+ | - STOP (C) will immediately terminate the signal generation. The Status Bar in (P) will then display “Stop / Ready.” | ||
+ | ==== RUN WIT DIGITAL PRE-DISTORTION (DPD) ==== | ||
+ | The following sequence shall produce a signal with DPD algorithm: | ||
+ | - Set desired parameters (amplitude and frequency) (H). | ||
+ | - WRITE parameters (G). Panel in (O) will display the generated configuration of the signal. | ||
+ | - Click Calibrate (D). A “Calibrating…” status will be seen in the Status Bar (P) and the timer (Q) will start. Wait until the Status Bar (P) will change to “Calibrated” and display the time elapsed. This process may take up to 2 minutes. | ||
+ | - RUN (B). The Status Bar (P) should display “Ready” and the timer beside it should start. It should change to " | ||
+ | - STOP (C) will immediately terminate the signal generation. The Status Bar (P) will then display “Stop / Ready.” | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 13. Setting Parameters for Generating a Single-tone Signal With and Without DPD (Continuous mode)// | ||
+ | </ | ||
+ | |||
+ | ==== GENERATE TWO-TONE SIGNAL ==== | ||
+ | The following sequence shall produce a two-tone signal assuming the GUI is already connected (see Figure 6 for the label): | ||
+ | - Change the Signal Type (F) to “IMD”. The CALIBRATE button is disabled since it is only allowed in sinewave. | ||
+ | - Set desired parameters (H). A signal preview will be plotted (N). | ||
+ | - WRITE parameters (G). Panel in (O) will display the generated configuration of the signal. | ||
+ | - RUN parameters (B). The Status Bar (P) should display “Ready” and the timer beside it should start. This means that the ADMX1002 module is now processing the configuration. It should change to " | ||
+ | - STOP (C) will immediately terminate the signal generation. The Status Bar in (P) will then display “Stop / Ready”. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 14. Setting Parameters for a Two-tone Signal// | ||
+ | </ | ||
+ | |||
+ | ==== GENERATE DC SIGNAL ==== | ||
+ | The following sequence shall produce a DC signal assuming the GUI is already connected (see Figure 7 for the label): | ||
+ | - Change the Signal Type (F) to “Direct”. The CALIBRATE button is disabled since it is only allowed in sinewave. The only allowed Trigger Mode is “Continuous”. | ||
+ | - Set desired parameters (H). A signal preview will be plotted (N). | ||
+ | - WRITE parameters (G). Panel in (O) will display the generated configuration of the signal. | ||
+ | - RUN parameters (B). The Status Bar (P) should display “Ready” and the timer beside it should start. This means that the ADMX1002 module is now processing the configuration. It should change to " | ||
+ | - STOP (C) will immediately terminate the signal generation. The Status Bar in (P) will then display “Stop / Ready” | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 15. Setting Parameters for a DC Signal// | ||
+ | </ | ||
+ | |||
+ | ==== GENERATE SINEWAVE SIGNAL (SINGLE-SHOT) ==== | ||
+ | All the previous software operation examples have the trigger mode set to “Continuous”. Now let us try the other option which is “Single-shot”. The signal duration of this mode is based on the number of samples defined. | ||
+ | The following sequence shall produce a sinewave signal with trigger mode set to single shot, assuming the GUI is already connected (see Figure 8 for the label): | ||
+ | - Change the Signal Type (F) to “Alternating”. | ||
+ | - Change the Trigger Mode (E) to “Single-shot”. | ||
+ | - Set desired parameters (H). The default number of cycles is 100. A signal preview will be plotted (N).WRITE parameters (G). Panel in (O) will display the generated configuration of the signal. | ||
+ | - RUN parameters (B). The Status Bar (P) should display “Ready” and the timer beside it should start. This means that the ADMX1001 module is now processing the configuration. It should change to " | ||
+ | - STOP (C) will immediately terminate the signal generation. The Status Bar in (P) will then display “Stop / Ready”. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 16. Setting Parameters for a Sinewave Signal (Single-shot Mode)// | ||
+ | </ | ||
+ | |||
+ | ==== STORING PROFILES ==== | ||
+ | The following sequence shall save a profile (see Figure 9 for the label): | ||
+ | - (Optional) Change the “Number of Profiles” (L) stored from default. A dialog box " | ||
+ | - Make sure to UNCHECK the “Use Profile” checkbox (K). | ||
+ | - For each profile to save: | ||
+ | - STOP (C) any running signal. | ||
+ | - Select the Profile ID (M) to associate with the profile to store. | ||
+ | - Set (H) desired parameters (Amplitude and Frequency). The plot will automatically display the waveform that corresponds to the parameters entered. | ||
+ | - Write parameters (G). Panel (O) will display the Amplitude and Frequency settings of the signal. | ||
+ | - (Optional) Calibrate (D). The Status Bar in (P) will change from “Ready” to “Calibrating…” status and the timer (L) beside it will start. After calibrating the signal, (P) will say it is “Calibrated” and display the time elapsed (L). | ||
+ | - RUN (B) and STOP (C). | ||
+ | - Click the SAVE profile button (I). Status Bar (P) will display “Saving Profile…” first and then “Profile Saved” indicating it has already saved the settings with the associated Profile ID. | ||
+ | - Repeat (3) for additional profiles to save. | ||
+ | - Note: Make sure to select a different Profile ID number for each profile, otherwise, the previous will get overwritten. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 17. Saving Profile at profile id 1// | ||
+ | </ | ||
+ | |||
+ | ==== LOADING PROFILES ==== | ||
+ | The following sequence shall load previously saved profile (see Figure 10 for the label): | ||
+ | - STOP (C) any running signal. The Status Bar (P) will display “Stop / Ready”. | ||
+ | - CHECK the “Use Profile” checkbox (K) | ||
+ | - Select the saved Profile ID. (M) | ||
+ | - Click the LOAD profile button (J). The Status Bar (P) will be displaying “Loading Profile…” first, then “Profile Loaded (Not Calibrated)” (for signals without DOD) or “Profile Loaded (Calibrated)” (for signals with DPD). | ||
+ | - Loaded profile parameters (amplitude and frequency) from the selected Profile ID will be visible in (O). | ||
+ | - Run (B) the loaded profile. Status Bar (P) should display “Ready” and the timer (L) beside it should start. This means that the ADMX1001 module is now processing the configuration. It should change to " | ||
+ | |||
+ | ==== USING A DIFFERENT SAVED PROFILE ==== | ||
+ | - STOP (C) any running signal. The Status Bar (P) will display “Stop / Ready”. | ||
+ | - With the “Use Profile” checkbox (K) still checked, select another Profile ID (M) with previously stored profile. | ||
+ | - Click the LOAD profile button (J). The Status Bar (P) will display “Loading Profile” first, then “Profile Loaded (Not Calibrated)” (for signals without DPD) or “Profile Loaded (Calibrated)” (for signals with DPD). | ||
+ | - Loaded profile parameters (amplitude and frequency) from the selected Profile ID will be visible in (O) | ||
+ | - Run (B) the loaded profile. Status Bar (P) should display “Ready” and the timer (L) beside it should start. This means that the ADMX1001 module is now processing the configuration. It should change to " | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 18. Loading Profile with profile id 1// | ||
+ | </ | ||
+ | |||
+ | ==== RUNNING AWG ==== | ||
+ | Refer to "AWG FILE GENERATOR" | ||
+ | - Change the Signal Type (F) to “AWG File”. The other control buttons are now disabled since no file is loaded yet. | ||
+ | - Click the "Load file" button (LF) and select the desired CSV file. A preview signal will be plotted (N) representing the file. The Write (G) button will now be enabled. | ||
+ | - Click Write (G) to send the AWG data to the ADMX1002 module. The status message (P) will display “Writing AWG data”. Once completed, it will now display “AWG write complete” and the timer (Q) stops. The Run (B) and Stop (C) button are now enabled. | ||
+ | - Click Run (B) to run the signal and Stop (C) to stop it. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 19. ADMX1002 AWG File plotted and ready to send to module// | ||
+ | </ | ||
+ | |||
+ | ==== AWG FILE GENERATOR ==== | ||
+ | An excel file (see Figure 20) will be used to create an AWG data (CSV) file. In order to save the output files, you need to create a folder called ADMX1002AWG in your " | ||
+ | - Set the desired frequency. | ||
+ | - Set the desired amplitude. | ||
+ | - Set the desired Wave Type. The available options are: | ||
+ | - Square wave | ||
+ | - Triangular wave | ||
+ | - Sawtooth wave | ||
+ | - Click " | ||
+ | - Click Save button to save the data in CSV format. Access the data at C:/ | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 20. AWG Generator// | ||
+ | </ | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 21. AWG Data with Plot// | ||
+ | </ | ||
+ | |||
+ | ===== ADMX1002 SCRIPTING INSTRUCTION ===== | ||
+ | To write your own script, take the following steps: | ||
+ | - Find the " | ||
+ | - ADMX1002_SDP_script.exe: | ||
+ | - sdpApi1.dll: | ||
+ | - ADMX1002_start.scr: | ||
+ | - ADMX1002_stop.scr: | ||
+ | - Follow the steps in "QUICK START GUIDE" to set up the ADMX1002. | ||
+ | * <fc # | ||
+ | - Open the Windows Command Prompt and change the directory to the folder " | ||
+ | * <fc # | ||
+ | * You will get the message "if you get here without error ADMX1002 should be generating waves" if you did the steps correctly and the signal should be generated at the outputs (see Figure 26). | ||
+ | * The ADMX1002 register map can be found in the following file: {{ : | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 22. Scripting Tool Folder// | ||
+ | </ | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 23. Disconnect the ADMX1002 Sourcing GUI// | ||
+ | </ | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 24. Windows Command Prompt to Generate a Signal// | ||
+ | </ | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 25. Error Message After Running the Command// | ||
+ | </ | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 26. Script Successfully Generated the Signal// | ||
+ | </ | ||
+ | |||
+ | ===== ADMX1002 Typical Performance ===== | ||
+ | |||
+ | === DC OUTPUT CHARACTERISTICS === | ||
+ | ^Parameter | ||
+ | |Output Voltage Range | ±4 |V | | ||
+ | |VCM Output Range | ±2.5 |V | | ||
+ | |DC Output Current | ||
+ | |Differential Offset | ||
+ | |Common-Mode Offset | ||
+ | |||
+ | === AC OUTPUT CHARACTERISTICS === | ||
+ | ^Parameter | ||
+ | |Differential Voltage Range | 3.5 | ||
+ | |Min. Output Frequency | ||
+ | |Max. Output Frequency | ||
+ | |Max. Output Frequency, DPD | 20 |kHz | | ||
+ | |Frequency Resolution |