This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:adm2587e [25 Jan 2018 14:04] – Richard Anslow | resources:eval:user-guides:adm2587e [25 Jan 2018 14:07] – Richard Anslow | ||
---|---|---|---|
Line 6: | Line 6: | ||
The EVAL-ADM2587EARDZ Arduino Shield & EVAL-ADM2587ERPIZ Raspberry Pi Shield use an identical basic design, J1 Raspberry Pi connector populated for EVAL-ADM2587ERPIZ, | The EVAL-ADM2587EARDZ Arduino Shield & EVAL-ADM2587ERPIZ Raspberry Pi Shield use an identical basic design, J1 Raspberry Pi connector populated for EVAL-ADM2587ERPIZ, | ||
- | This Wiki guide provides hardware references and Arduino software for full integration of the EVAL-ADM2587EARDZ in a demonstration platform. This wiki guide also provides hardware references and Raspberry pi sample code. | + | This Wiki guide provides hardware references and Arduino software for full integration of the EVAL-ADM2587EARDZ in a demonstration platform. This wiki guide also provides hardware references and Raspberry pi sample code for the EVAL-ADM2587ERPIZ. |
{{: | {{: | ||
Line 27: | Line 27: | ||
\\ | \\ | ||
----- | ----- | ||
- | ===== EVAL-ADM2587EARDZ Arduino Shield Example Code ===== | + | ===== EVAL-ADM2587EARDZ Arduino |
\\ Arduino UNO code is provided so that that user can perform a loopback test mode for the ADM2587E RS-485 transceiver. Load the ' | \\ Arduino UNO code is provided so that that user can perform a loopback test mode for the ADM2587E RS-485 transceiver. Load the ' |