This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:adin1300-and-adin1200:dp83867_to_adin1300_phy_exchange_guide [07 Jan 2022 15:23] – Formatting changed for even pages Mark Bolger | resources:eval:user-guides:adin1300-and-adin1200:dp83867_to_adin1300_phy_exchange_guide [19 Jun 2023 17:30] – Mark Bolger | ||
---|---|---|---|
Line 104: | Line 104: | ||
The ADIN1300 supports RGMII, MII and RMII MAC interface modes. The following sections describe the RGMII, MII and RMII interfaces for both devices. | The ADIN1300 supports RGMII, MII and RMII MAC interface modes. The following sections describe the RGMII, MII and RMII interfaces for both devices. | ||
+ | |||
=== RGMII Interface === | === RGMII Interface === | ||
Line 109: | Line 110: | ||
Both devices support the internal delay on the clocks. By default, the ADIN1300 is configured in RGMII mode with a 2 ns delay on RXC and TXC. | Both devices support the internal delay on the clocks. By default, the ADIN1300 is configured in RGMII mode with a 2 ns delay on RXC and TXC. | ||
- | {{: | + | {{: |
=== MII Interface === | === MII Interface === | ||
Line 249: | Line 250: | ||
https:// | https:// | ||
+ | ==== Non Operating System Driver ==== | ||
+ | The ADIN1200 has a C Non Operating System Driver available from the devices product page here: | ||
+ | [[adi> | ||
</ | </ |