This is an old revision of the document!
The purpose of this application note is to describe the configuration of the ADIN1300 for the various Ethernet PHY compliance test modes as set out by IEEE802.3. The ADIN1300 supports the IEEE test modes, Test Mode 1, Test Mode 2, Test Mode 3 and Test Mode 4 used for 1000BASE-T IEEE compliance testing. The ADIN1300 has some additional test modes that are useful for 10BASE-T and 100BASE-TX compliance testing. Details of the registers, sequences of writes are captured in this document. Use this application note in conjunction with the product datasheet.
When performing this testing, user will need Ethernet compliance test fixture and associated Ethernet physical layer compliance software. There are a number of vendors provide Ethernet Compliance test equipment. For ADI in-house validation, we used Tektronix TDSET3 compliance software in addition to having UNH (University of New Hampshire perform compliance testing). Once equipment is in place and hardware powered and connected to the test fixture, configure the PHY through the MDIO interface to set the required test mode and use the compliance software to record and report the results.
To ensure the device is in a known state, either start from a power cycle or alternatively, issue the following writes to reset the device with fresh read of the hardware configuration.
The ADIN1300 supports a range of extended management interface registers which can be accessed using Clause 45 access or alternatively using Clause 22 access through the EXT_REG_PTR (address 0x0010) and EXT_REG_DATA (address 0x0011), these registers provide user ability to read/write to the extended register space (any register greater than 0x001F) indirectly. If using Clause 22 access, write the 16-bit register address into the EXT_REG_PTR register and then read or write the EXT_REG_DATA register.
The ADIN1300 supports the IEEE test modes, Test Mode 1, Test Mode 2, Test Mode 3 and Test Mode 4 used for 1000BASE-T IEEE compliance testing. An IEEE test mode can be selected by writing to register address 9, bits 15:13. The TST_MODE bit field can be used to select the transmit test waveforms required for Gigabit IEEE compliance testing.
Address: 0x09: Reset, 0x0200, Name: MSTR_SLV_CONTROL This address corresponds to the MASTER-SLAVE Control register specified in clause 40.5.1.1 of IEEE Std 802.3. Only Test mode bits are show in table below, refer to datasheet register map for further detail.
ADD TABLE
This test mode is used for a number of tests as follows:
To configure the device in Test Mode 1, issue the following writes over MDIO MII_CONTROL.SFT_PD. Write(0b1) Register 0x0000, bit 11: Place the device into Software Power Down MSTR_SLV_CONTROL.TST_MODE.Write(1) Register 0x0009, bit 15:13: Enable Test Mode 1 MII_CONTROL.SFT_PD.Write(0b0) Register 0x0000, bit 11: Bring PHY out of Software Power Down ==== TEST MODE 2 & 3 ==== This test mode is used to ensure the TX_TCLK jitter with respect to an un-jittered reference is within range. Note the ADIN1300 does not expose TX_TCLK directly. To configure the device in Test Mode 2, issue the following writes over MDIO MII_CONTROL.SFT_PD. Write(0b1) Register 0x0000, bit 11: Place the device into Software Power Down MSTR_SLV_CONTROL.TST_MODE.Write(2) Register 0x0009, bits 15:13: Enable Test Mode 2 MII_CONTROL.SFT_PD.Write(0b0) Register 0x0000, bit 11: Bring PHY out of Software Power Down To configure the device in Test Mode 3, issue the following writes over MDIO MII_CONTROL.SFT_PD. Write(0b1) Register 0x0000, bit 11: Place the device into Software Power Down MSTR_SLV_CONTROL.TST_MODE.Write(3) Register 0x0009, bits 15:13: Enable Test Mode 3 MII_CONTROL.SFT_PD.Write(0b0) Register 0x0000, bit 11: Bring PHY out of Software Power Down ==== TEST MODE 4 ==== This test mode is used To ensure the peak distortion is within the specified range. To verify the return loss is above the specified attenuation. To verify the PHYs common-mode rejection ratio is in range To configure the device in Test Mode 4, issue the following writes over MDIO MII_CONTROL.SFT_PD. Write(0b1) Register 0x0000, bit 11: Place the device into Software Power Down MSTR_SLV_CONTROL.TST_MODE.Write(4) Register 0x0009, bits 15:13. Enable Test Mode 4 MII_CONTROL.SFT_PD.Write(0b0) Register 0x0000 bit 11: Bring PHY out of Software Power Down
For 100BASE-TX operation there are a variety of tests. There are two main test modes main register involved here is the B_100_TX_TST_MODE register at address 0xB413 (available via Clause 45 access)
Address: 0xB413, Reset: 0x0000, Name: B_100_TX_TST_MODE This register provides the ability to transmit a 100BASE-TX test signal.
To configure the device for 100BASE-TX VOD measurements, issue the following writes over MDIO MII_CONTROL.Write(0x2900) Register 0x0000 to place the device into Software PD, configure 100BASE-TX full duplex, autoneg disabled PHY_CTRL_1.AUTO_MDI_EN.Write(0b) Register 0x0012, bit 10: Disable Auto MDI/MDIX PHY_CTRL_1.MAN_MDIX.Write(0b0) Register 0x0012, bit 9: Operate in MDI configuration B_100_TX_TST_MODE.Write(1/2/3/4) Register 0xB413 bits 2:0: Configure required test mode on Dim 0 or 1 PHY_CTRL_3. LINK_EN.Write(0b1) Register 0x0017, bit 13: Enable linking MII_CONTROL.SFT_PD.Write(0b0) Register 0x0000 bit 11: Bring PHY out of Software Power Down
When operating in 10 Mbps speeds, the PHY is configured for 10BASE-Te transmit levels by default. 10BASE-T provides larger transmit levels and can be configured by clearing the B_10_E_EN register. The 10BASE-Te/T compliance tests are: • Link Pulse Testing • Medium Attachment Unit (MAU) • TP_IDL • Jitter • Differential Voltage • Harmonics • Transmitter Return Loss • Receiver Return Loss • Common-Mode Voltage The B_10_TX_TST_MODE register is used to select transmit test signals useful for 10BASE-T compliance testing.
Address: 0xB412, Reset: 0x0000, Name: B_10_TX_TST_MODE This register provides the ability to transmit a 10BASE-T test signal.
To configure the device for 10BASE-T transmit test mode, consisting of 5MHz square wave on desired dimension, issue the following writes over MDIO GE_SFT_RST_CFG_EN.Write(0b1) Register 0xFF0D to ensure the hardware configuration is refreshed. GE_SFT_RST. Write(0b1) Register 0xFF0C subsystem reset MII_CONTROL.SFT_RST. Write(0b1) Register 0x0000 Issue a software reset, this bit is self clearing MII_CONTROL.Write(0x0900) Register 0x0000 Enter Software Power Down and configure 10M FD, disable AutoNegotiation B_10_TX_TST_MODE.Write(0b100) Register 0xB412 Choice of 100: Enable Transmit 5MHz square wave on Dim 1; 011: 5MHz on Dim0; 010 10MHz on Dim1; 001: 10MHz on Dim0. MII_CONTROL.SFT_PD.Write(0b0) Register 0x0000 Bring PHY out of Software PD
An alternative configuration, where the device is configured in 10BASE-T forced mode in loopback with Tx suppression disabled, with transmission of frames with random payloads using the frame generator as follows: GE_SFT_RST_CFG_EN.Write(0b1) Register 0xFF0D to ensure the hardware configuration is refreshed. GE_SFT_RST. Write(0b1) Register 0xFF0C subsystem reset MII_CONTROL.SFT_RST. Write(0b1) Register 0x0000 bit 15, Issue a software reset, this bit is self clearing MII_CONTROL.SFT_PD.Write(0b0) Register 0x0000 bit 11, Bring PHY out of Software PD PHY_CTRL_1.DIAG_CLK_EN.Write(0b1) Register 0x0012 bit 2, Enable the Diagnostic Clock MII_CONTROL.LOOPBACK.Write(0b1) Register 0x0000 bit 14, Enable Loopback PHY_CTRL_1.MAN_MDIX.Write(0b0) Register 0x0012 bit 9, Operate in MDI configuration PHY_CTRL_STATUS_1.LB_TX_SUP.Write(0b0) Register 0x0013 bit 6, Stop suppressing the transmit signal at the MDI pins in all digital loopback PHY_CTRL_STATUS_1.LB_ALL_DIG_SEL.Write(0b1) Register 0x0013 bit12 Enable all digital loopback PHY_CTRL_3. LINK_EN.Write(0b1) Register 0x0017 bit 13, Enable linking MII_CONTROL.SFT_PD.Write(0b0) Register 0x0000 bit 11, Bring PHY out of Software PD Wait for Link up FG_CONT_MODE_EN.Write(0b1) Register 0x9417 Enable the frame generator into continuous mode FG_CNTRL_RSTRT.FG_CNTRL.Write(1) Register 0x9416, bits 2:0: Enable random number in the MAC client data frame field, options of decrementing, alternative 0x55, all ones, all zeroes, random number FG_EN.FG_EN.Write(1) Enable Frame Generator Setup for 10BASE-T forced mode in loopback with Tx suppression disabled, with transmission of frames with random payloads using the frame generator, configure as follows in sequence above FG_CNTRL_RSTRT.FG_CNTRL.Write(0b011) 0xFF repeating payloads FG_CNTRL_RSTRT.FG_CNTRL.Write(0b010) 0x00 repeating payloads FG_CNTRL_RSTRT.FG_CNTRL.Write(0b100) alternative 0x55 payloads FG_CNTRL_RSTRT.FG_CNTRL.Write(0b101) data field decrementing from 255 to 0(decimal)
10BASE-T is configured by writing the following register – include it in the sequence above if 10BASE-T operation is required. B_10_E_EN.Write(0x0) 10BASE-Te is enabled by default, write 0 to configure 10BASE-T. </WRAP> </WRAP> —-
The ADI evaluation board uses small MDIO dongle board for USB to MDIO communications and the accompanying GUI provides access to the various Test modes from the “Test Mode” tab. Select the relevant test mode to configure and “Execute Test”. In the “Activity log” the register writes can be observed.
—-