This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:adin1100_userguide [07 Sep 2021 17:39] – [Hardware Configuration Setup] Shane Flanagan | resources:eval:user-guides:adin1100_userguide [09 Sep 2021 16:47] (current) – [User Guide for EVAL-ADIN1100EBZ] Catherine Redmond | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== ADIN1100 10BASE-T1L Ethernet PHY Evaluation Kit Media Converter to 10BASE-T with ADIN1200 Ethernet PHY ====== | + | ====== User Guide for EVAL-ADIN1100EBZ |
+ | |||
+ | === ADIN1100 10BASE-T1L Ethernet PHY Evaluation Kit Media Converter to 10BASE-T with ADIN1200 Ethernet PHY === | ||
+ | |||
===== General Description ===== | ===== General Description ===== | ||
Line 60: | Line 64: | ||
The power supply source can be selected by link on J1 “BOARD PWR SELECTION”. Inserting link in position “USB” enables the board to receive power from USB connector. Inserting link in position “PWR+EXT+” enables the board to receive power from connectors P1 and P2. | The power supply source can be selected by link on J1 “BOARD PWR SELECTION”. Inserting link in position “USB” enables the board to receive power from USB connector. Inserting link in position “PWR+EXT+” enables the board to receive power from connectors P1 and P2. | ||
If both J1 “BOARD PWR SELECTION” “USB and “PWR+EXT+” links are inserted, there is a “diode or” implemented on the input of J1, and the supply with a higher voltage will supply the board. | If both J1 “BOARD PWR SELECTION” “USB and “PWR+EXT+” links are inserted, there is a “diode or” implemented on the input of J1, and the supply with a higher voltage will supply the board. | ||
- | The power from the source is converted by a step-down converter U501 LT8619EDD# | + | The power from the source is converted by a step-down converter U501 LT8619EDD# |
The board power consumption depends on the mode of operation, with the maximum of approximately 0.5W. | The board power consumption depends on the mode of operation, with the maximum of approximately 0.5W. | ||
Line 132: | Line 136: | ||
^(RJ45) | ^(RJ45) | ||
^POWER | ^POWER | ||
+ | |||
+ | ==== µC Modes Of Operation ==== | ||
+ | The EVAL-ADIN1100EBZ can be used in various modes of | ||
+ | operations implemented in the uC firmware. Up to 16 modes of | ||
+ | operations can be selected by setting the 4 positions of the slide | ||
+ | switch S402. The status of the switch is accepted (latched) after | ||
+ | the board is powered up or reset. | ||
+ | Therefore, to change the mode of operation, the board must be | ||
+ | reset by pressing “RESET” button S400 or by applying power | ||
+ | cycle after changing the position of the slide switch S501. The | ||
+ | detailed description is in the relevant sections of this document. | ||
+ | |||
+ | **Table 5. Firmware Modes of Operation, set by S403, uC CFG** | ||
+ | ^ CFG3< | ||
+ | |ON | ON | ON | ||
+ | |ON | ON | ON | ||
+ | |ON | ON | OFF |ON | 2 | Reserved | ||
+ | |ON | ON | OFF | ||
+ | |ON | OFF | ON | ||
+ | |ON | OFF | ON | ||
+ | |ON | OFF | OFF | ||
+ | |ON | OFF | OFF | ||
+ | |OFF | ON | ON | ||
+ | |OFF | ON | ON | ||
+ | |OFF | ON | OFF | ||
+ | |OFF | ON | OFF | ||
+ | |OFF | OFF | ON | ||
+ | |OFF | OFF | ON | ||
+ | |OFF | OFF | OFF | ||
+ | |OFF | OFF | OFF | ||
+ | < | ||
+ | |||
+ | ===== Software===== | ||
+ | The EVAL-ADIN1100EBZ can be used as stand-alone board, with | ||
+ | the firmware already programmed in the uC flash memory, the | ||
+ | mode of operation set by mode switch, and status indicated by | ||
+ | LEDs. There is no software needed for this stand-alone use case.\\ | ||
+ | The demo can also be connected to a PC via USB port, the full set | ||
+ | of ADIN1100 register settings and features such as link quality | ||
+ | monitoring and diagnostics can be accessed with the ADIN1100 | ||
+ | Graphical User Interface software, available from Analog Devices.\\ | ||
+ | Alternatively, | ||
+ | 10BASE-T1L link status monitoring and some diagnostics can be | ||
+ | accessed using a simple set of ASCII text commands and messages | ||
+ | exchanged over the USB Com Port and a serial port terminal | ||
+ | software. | ||
+ | ==== Driver For USB COM Port ==== | ||
+ | The EVAL-ADIN1100EBZ uses FTDI FT232 for the USB Com | ||
+ | Port connectivity.\\ | ||
+ | Please make sure that appropriate Virtual Com Port driver is | ||
+ | included or installed on the host platform before connecting the | ||
+ | EVAL-ADIN1100EBZ to that host via USB cable.\\ | ||
+ | |||
+ | The drivers are available from FTDI, at the time of writing this | ||
+ | document at https:// | ||
+ | ==== COM Port And Terminal Settings ==== | ||
+ | When the EVAL-ADIN1100EBZ is connected to the host, it will | ||
+ | become available in the host system as a USB Com Port, and will be | ||
+ | assigned a com port number. The number will depend on the | ||
+ | system settings, on com port devices previously connected and | ||
+ | assigned in the system, and on the FTDI driver settings.\\ | ||
+ | |||
+ | The EVAL-ADIN1100EBZ uC firmware communicates over a | ||
+ | standard UART interface, with settings:\\ | ||
+ | |||
+ | Speed 115200 Bd., 1 Start Bit – 8 Data Bits – No Parity – 1 Stop Bit.\\ | ||
+ | |||
+ | The protocol is based on ASCII text commands and messages. | ||
+ | Each message and command are finished by < | ||
+ | message sent from the firmware to the host is finished by both | ||
+ | <CR> and <LF> characters. For the commands received from | ||
+ | host the firmware expects the < | ||
+ | <LF> or both <CR> and < | ||
+ | |||
+ | (//To be sure and clear: | ||
+ | <CR> .. “carriage return”, ASCII code 0x0D, 13dec, | ||
+ | <LF> .. “line feed”, ASCII code 0x0A, 10dec.//)\\ | ||
+ | ==== Terminal Software ==== | ||
+ | The EVAL-ADIN1100EBZ firmware works with the common | ||
+ | serial terminals. It has been tested on Windows platform with | ||
+ | PuTTY, RealTerm, Termite and the old Hyperterminal. | ||
+ | ==== Terminal Commands And Messages ==== | ||
+ | (//The examples here were captured using Compuphase Termite//). | ||
+ | ==== Initial Welcome Message ==== | ||
+ | When the EVAL-ADIN1100EBZ is correctly connected, from | ||
+ | the uC firmware and UART, via the USB Com Port, to the | ||
+ | terminal software, the firmware sends after power or after | ||
+ | pressing the board RESET button S501 an initial welcome | ||
+ | message:\\ | ||
+ | |||
+ | |||
+ | <fc # | ||
+ | ANALOG DEVICES 10BASE-T1L PHY Demo\\ | ||
+ | ================================================\\ | ||
+ | (c) 2021 Analog Devices Inc. All rights reserved\\ | ||
+ | ================================================\\ | ||
+ | Firmware ver.: 12 . 1 . 4784b935\\ | ||
+ | Hardware type: EVAL-ADIN1100EBZ\\ | ||
+ | Hardware ver.: A\\ | ||
+ | Hardware UID : AVAS142049\\ | ||
+ | uCCFG3-2-1-0 : OFF-OFF-OFF-ON (Mode 14)\\ | ||
+ | Firmware Mode: GUI / Interactive mode\\ | ||
+ | ================================================\\ | ||
+ | Type '<?>< | ||
+ | ================================================</ | ||
+ | |||
+ | ==== Terminal Commands ==== | ||
+ | The most important command is “<?>< | ||
+ | On the host keyboard, press key “?” followed by key “Enter”, | ||
+ | and the firmware will send a list of all commands implemented | ||
+ | in this version:\\ | ||
+ | <fc # | ||
+ | <fc # | ||
+ | List of Commands\\ | ||
+ | * MDIO (Clause 22) write to Phy, all numbers in hex.\\ | ||
+ | ' | ||
+ | * MDIO (Clause 22) read from Phy, all numbers in hex.\\ | ||
+ | ' | ||
+ | * MDIO (Clause 45) write to Phy, all numbers in hex.\\ | ||
+ | ' | ||
+ | * MDIO (Clause 45) read from Phy, all numbers in hex.\\ | ||
+ | ' | ||
+ | * Phy (hardware) reset\\ | ||
+ | <fc # | ||
+ | * Phy status and link properties.\\ | ||
+ | ' | ||
+ | * Start reporting status.\\ | ||
+ | ' | ||
+ | * Stop reporting status.\\ | ||
+ | ' | ||
+ | * Clear / reset status counters.\\ | ||
+ | ' | ||
+ | * uC Software Reset.\\ | ||
+ | ' | ||
+ | * Mode change, overrides uC CFG until next Reset.\\ | ||
+ | 'mode < | ||
+ | * List implemented modes.\\ | ||
+ | ' | ||
+ | * Comment – string of up to 98 characters\\ | ||
+ | ' | ||
+ | * Show list of commands.\\ | ||
+ | '?'< | ||
+ | ==============================================</ | ||
+ | ==== Status And Diagnostics ==== | ||
+ | To see the status of the demo, use command “phystatus”, | ||
+ | will read and show the latest status of the ADIN1200 10BASE-T | ||
+ | PHY and ADIN1100 10BASE-T1L PHY:\\ | ||
+ | |||
+ | <fc # | ||
+ | <fc # | ||
+ | ADIN1100 Link is Up, Master, 2.4 V\\ | ||
+ | MSE -37.2 dB Rx 0, Err 0</ | ||
+ | |||
+ | To see a continuous update, use commands “start”: | ||
+ | <fc # | ||
+ | <fc # | ||
+ | MSE -38.4 dB Rx 255, Err 0\\ | ||
+ | MSE -38.6 dB Rx 256, Err 0\\ | ||
+ | MSE -38.7 dB Rx 257, Err 0\\ | ||
+ | MSE -38.4 dB Rx 257, Err 0\\ | ||
+ | MSE -38.7 dB Rx 257, Err 0</ | ||
+ | <fc # | ||
+ | <fc # | ||
+ | |||
+ | The firmware will periodically, | ||
+ | send an update. The update in the present firmware version | ||
+ | includes:\\ | ||
+ | *“MSE” – 10BASE-T1L Mean Square Error, which indicates link quality. | ||
+ | * “Rx” – number of Ethernet frames received by PHY from 10BASE-T1L cable since the last board / firmware reset, or after use of command “clear” | ||
+ | * “Err” – number of frames with error received since the last board / firmware reset, or after use of command “clear” | ||
+ | |||
+ | To stop the continuous update, use command “stop”. | ||
+ | (Or reset the board.) | ||
+ | |||
+ | ===== µC Firmware Update===== | ||
+ | The uC (U401 ADuCM4050) is programmed before shipping | ||
+ | the demo board, and therefore there is no need to program it, | ||
+ | unless a new version of firmware is available, and you want to | ||
+ | update it on your board.\\ | ||
+ | The present firmware version can be checked via USB Com Port | ||
+ | and terminal software, it is displayed in the welcome message | ||
+ | after board reset or in response to “info” command.\\ | ||
+ | Firmware update is distributed as a compiled binary (.hex) file. | ||
+ | The easiest way to program it to the uC is using the USB Com | ||
+ | Port and CrossCore Serial Flash Programmer, available for free | ||
+ | download from analog.com, presently: | ||
+ | |||
+ | https:// | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign>// | ||
+ | |||
+ | USB Com Port driver (same as for using the terminal software) | ||
+ | needs to be installed on the PC before connecting the board and | ||
+ | using the CrossCore Serial Flash Programmer - see chapter | ||
+ | “Driver for USB Com Port”.\\ | ||
+ | When you have the driver and programmer software installed, | ||
+ | and firmware update hex file ready, use the following steps:\\ | ||
+ | - Connect the board (P401) via micro-USB cable to your PC. | ||
+ | - Start the CrossCore serial flash programmer software. | ||
+ | - Set the programmer (also see Figure 4): | ||
+ | *Target: ADuCM302x | ||
+ | *Serial Port: COMx (USB Serial Port) – (the “x” port number is depending on your PC) | ||
+ | *Baudrate: 115200 | ||
+ | *Action: Program | ||
+ | *(Second stage kernel is not applicable) | ||
+ | - File to download - browse for the firmware file on your PC | ||
+ | - On the demo board, simultaneously press and hold buttons S501 “RESET” and S401 “BOOT”. Release the RESET button first, followed by releasing the BOOT button. The on board microcontroller is in the programming state now, and the yellow / orange heart beat LED402 will stop blinking. | ||
+ | - Click Start and the code should start to download with messages provided in the Status window and progress bar across the bottom of the window.NOTE: | ||
+ | - After programing, press & release RESET button. | ||
+ | ===== Notes===== | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | **Legal Terms and Conditions** | ||
+ | By using the evaluation board discussed herein (together with any tools, components documentation or support materials, the “Evaluation Board”), you are agreeing to be bound by the terms and | ||
+ | conditions set forth below (“Agreement”) unless you have purchased the Evaluation Board, in which case the Analog Devices Standard Terms and Conditions of Sale shall govern. Do not use the Evaluation | ||
+ | Board until you have read and agreed to the Agreement. Your use of the Evaluation Board shall signify your acceptance of the Agreement. This Agreement is made by and between you (“Customer”) and | ||
+ | Analog Devices, Inc. (“ADI”), | ||
+ | free, limited, personal, temporary, non-exclusive, | ||
+ | Evaluation Board is provided for the sole and exclusive purpose referenced above, and agrees not to use the Evaluation Board for any other purpose. Furthermore, | ||
+ | subject to the following additional limitations: | ||
+ | Evaluation Board. As used herein, the term “Third Party” includes any entity other than ADI, Customer, their employees, affiliates and in-house consultants. The Evaluation Board is NOT sold to Customer; | ||
+ | all rights not expressly granted herein, including ownership of the Evaluation Board, arereserved by ADI. CONFIDENTIALITY. This Agreement and the Evaluation Board shall all be considered the confidential | ||
+ | and proprietary information of ADI. Customer may not disclose or transfer any portion of the Evaluation Board to any other party for any reason. Upon discontinuation of use of the Evaluation Board or | ||
+ | termination of this Agreement, Customer agrees to promptly return the Evaluation Board to ADI. ADDITIONAL RESTRICTIONS. Customer may not disassemble, | ||
+ | Evaluation Board. Customer shall inform ADI of any occurred damages or any modifications or alterations it makes to the Evaluation Board, including but not limited to soldering or any other activity that | ||
+ | affects the material content of the Evaluation Board. Modifications to the Evaluation Board must comply with applicable law, including but not limited to the RoHS Directive. TERMINATION. ADI may | ||
+ | terminate this Agreement at any time upon giving written notice to Customer. Customer agrees to return to ADI the Evaluation Board at that time. LIMITATION OF LIABILITY. THE EVALUATION BOARD | ||
+ | PROVIDED HEREUNDER IS PROVIDED “AS IS” AND ADI MAKES NO WARRANTIES OR REPRESENTATIONS OF ANY KIND WITH RESPECT TO IT. ADI SPECIFICALLY DISCLAIMS ANY REPRESENTATIONS, | ||
+ | ENDORSEMENTS, | ||
+ | FITNESS FOR A PARTICULAR PURPOSE OR NONINFRINGEMENT OF INTELLECTUAL PROPERTY RIGHTS. IN NO EVENT WILL ADI AND ITS LICENSORS BE LIABLE FOR ANY INCIDENTAL, SPECIAL, INDIRECT, OR | ||
+ | CONSEQUENTIAL DAMAGES RESULTING FROM CUSTOMER’S POSSESSION OR USE OF THE EVALUATION BOARD, INCLUDING BUT NOT LIMITED TO LOST PROFITS, DELAY COSTS, LABOR COSTS OR LOSS OF | ||
+ | GOODWILL. ADI’S TOTAL LIABILITY FROM ANY AND ALL CAUSES SHALL BE LIMITED TO THE AMOUNT OF ONE HUNDRED US DOLLARS ($100.00). EXPORT. Customer agrees that it will not directly or | ||
+ | indirectly export the Evaluation Board to another country, and that it will comply with all applicable United States federal laws and regulations relating to exports. GOVERNING LAW. This Agreement shall | ||
+ | be governed by and construed in accordance with the substantive laws of the Commonwealth of Massachusetts (excluding conflict of law rules). Any legal action regarding this Agreement will be heard | ||
+ | in the state or federal courts having jurisdiction in Suffolk County, Massachusetts, | ||
+ | Contracts for the International Sale of Goods shall not apply to this Agreement and is expressly disclaimed. |