This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:ade9430 [07 Mar 2024 21:55] – remove mention of Phase integrator David Smith | resources:eval:user-guides:ade9430 [09 Apr 2024 16:32] (current) – Fixed voltage transfer function equation John Stuart | ||
---|---|---|---|
Line 2328: | Line 2328: | ||
The current transfer function is 20/3000 = 0.0067 V rms/A rms. | The current transfer function is 20/3000 = 0.0067 V rms/A rms. | ||
- | The voltage transfer function is 1/(900 + 1) = 0.001 V rms/A rms. | + | The voltage transfer function is 1/(990 + 1) = 0.001 V rms/A rms. |
The input at the current ADC pins is 0.0067 × 10 = 0.067 V rms. | The input at the current ADC pins is 0.0067 × 10 = 0.067 V rms. |