This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad9656:reference_hdl [11 Dec 2020 12:40] – edited download support Dan Hotoleanu | resources:eval:user-guides:ad9656:reference_hdl [07 Jan 2021 12:40] (current) – modified the AD9656EBZ in the introduction section. added a link to the AD9656 board evaluation page to the more information section. added link to the ad9656 board to the supported devices section. deleted part of the build section and added a link to th Dan Hotoleanu | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD9656 HDL Reference Design ====== | ====== AD9656 HDL Reference Design ====== | ||
+ | |||
+ | ===== Introduction ===== | ||
+ | |||
+ | The [[adi> | ||
+ | |||
+ | ===== Supported Devices ===== | ||
+ | |||
+ | * [[adi> | ||
+ | |||
+ | ===== Supported Carriers ===== | ||
+ | |||
+ | Until now our recommended plaform is the Zynq based system: | ||
+ | |||
+ | * [[xilinx> | ||
===== Functional Overview ===== | ===== Functional Overview ===== | ||
Line 25: | Line 39: | ||
The device control and monitor signals are interfaced to a GPIO module. The SPI signals are controlled by a separate AXI based SPI core. | The device control and monitor signals are interfaced to a GPIO module. The SPI signals are controlled by a separate AXI based SPI core. | ||
- | ===== Supported Carriers | + | ===== Building the HDL ====== |
- | These are the supported carriers for the HDL - not the complete package (software and HDL). Typically | + | ADI does not distribute |
- | Our recommended plaforms are the Zynq based systems: | + | **Linux** |
- | | + | < |
+ | dhotolea@analog: | ||
+ | dhotolea@analog: | ||
+ | </ | ||
+ | |||
+ | A more comprehensive build guide can be found in the [[/ | ||
+ | |||
+ | ===== More information ===== | ||
+ | |||
+ | | ||
+ | * [[resources/ | ||
===== Download ====== | ===== Download ====== | ||
Line 38: | Line 62: | ||
{{page> | {{page> | ||
- | {{navigation AD9656# |