This is an old revision of the document!
The reference design is a processor based ARM embedded system. A functional block diagram of the system is given below for the Xilinx FPGAs. The cores are programmable through an AXI-lite interface. The data path consists of a DMA interface for the receive path.
The digital interface consists of 4 transmit and 4 receive lanes running at 10Gbps (default). The transceivers then interfaces to the cores at 128bits@250MHz. The data is sent or received based on the configuration (programmable) from separate transmit and receive chains.
When using Qsys, implementing JESD204B protocol requires several IPs. AVL_XCVR is a wrapper which instantiates all the required IPs and configures them according to the desired data rate. One AVL_XCVR must be instantiated for the transmit path and one for the receive path. It adds clock bridges, PLL and reconfiguration IP, proper reset, lane PLL for the transmit path, a JESD204B IP instantiating the JESD204B base and a JESD204B IP for each lane instantiating the PHY.
AXI_XCVR allows resetting and monitoring the transceiver path.
One important aspect for AD-FMCDAQ2-EBZ is that the reference clock needed for the FPGA transceiver calibration is generated only after the AD9523-1 clock generator is configured. The programming is done only after the FPGA is configured and software is running. Because of this, the software needs to perform a transceiver re-calibration after the transceiver reference clock is stable and before taking AXI_XCVR cores out of reset.
The DAC data may be sourced from an internal data generator (DDS, pattern or PRBS) or from the external DDR via DMA. The internal DDS phase and frequency are programmable.
The ADC data is sent to the DDR via DMA. The core also supports PN monitoring at the sample level. This is different from the JESD204B specific PN sequence (though they both claim to be from the same equation).
The device control and monitor signals are interfaced to a GPIO module. The SPI signals are controlled by a separate AXI based SPI core.
These are the supported carriers for the HDL - not the complete package (software and HDL). Typically the software lags behind the HDL, so if you don't see the these listed on the main project page - it is not yet done.
Our recommended plaforms are the Zynq based systems:
but it also works on the following fabric only systems:
For Altera systems:
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD-FMCDAQ2-EBZ | daq2 | a10soc | NA | ad_ip_jesd204_tpl_adc |
kc705 | daq2_kc705 | ad_ip_jesd204_tpl_dac | ||
kcu105 | daq2_kcu105 | axi_adxcvr | ||
zc706 | daq2_zc706 | axi_clkgen | ||
zcu102 | daq2_zcu102 | axi_dmac | ||
axi_hdmi_tx | ||||
axi_jesd204_rx | ||||
axi_jesd204_tx | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
data_offload | ||||
jesd204_rx | ||||
jesd204_tx | ||||
sysid_rom | ||||
util_adcfifo | ||||
util_adxcvr | ||||
util_axis_fifo | ||||
util_cdc | ||||
util_cpack2 | ||||
util_do_ram | ||||
util_hbm |