This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad9208_dual_ebz:ad9208_dual_ebz_hdl [10 May 2019 12:07] – [Block Diagram] Laszlo Nagy | resources:eval:user-guides:ad9208_dual_ebz:ad9208_dual_ebz_hdl [26 Apr 2021 16:38] (current) – [More Information] Laszlo Nagy | ||
---|---|---|---|
Line 4: | Line 4: | ||
==== Functional Overview ==== | ==== Functional Overview ==== | ||
The AD9208-DUAL-EBZ reference design is a processor based (e.g. Microblaze) embedded system. The device interfaces to the FPGA transceivers followed by the individual JESD204B and ADC cores. The cores are programmable through an AXI-Lite interface. The samples are passed to the system memory (DDR). | The AD9208-DUAL-EBZ reference design is a processor based (e.g. Microblaze) embedded system. The device interfaces to the FPGA transceivers followed by the individual JESD204B and ADC cores. The cores are programmable through an AXI-Lite interface. The samples are passed to the system memory (DDR). | ||
+ | |||
+ | <WRAP center round download> | ||
+ | https:// | ||
+ | </ | ||
+ | |||
The reference design supports the following evaluation board: | The reference design supports the following evaluation board: | ||
^Hardware ^Evaluation Document ^ | ^Hardware ^Evaluation Document ^ | ||
- | |[[adi>dual-AD9208|DUAL-AD9208]] | + | |[[adi> |
Line 14: | Line 19: | ||
* [[xilinx> | * [[xilinx> | ||
+ | |||
+ | ==== Building the HDL project ==== | ||
+ | General build instructions can be found here: [[resources: | ||
==== Block Diagram ==== | ==== Block Diagram ==== | ||
Line 44: | Line 52: | ||
+ | |||
+ | |||
+ | ==== More Information ==== | ||
+ | * [[: | ||
+ | * [[: | ||
+ | * [[: | ||
+ | * [[: | ||
+ | * [[: | ||
==== Support ==== | ==== Support ==== | ||
- | Analog Devices will provide limited online support for anyone using the core with Analog Devices components (ADC, DAC, Video, Audio, etc) via the [[https://ez.analog.com/ | + | Analog Devices will provide limited online support for anyone using the core with Analog Devices components (ADC, DAC, Video, Audio, etc) via the [[ez>community/ |