This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:ad7616-sdz [08 Mar 2017 15:26] – [No-OS Downloads] Add Support section Istvan Csomortani | resources:eval:user-guides:ad7616-sdz [20 Mar 2018 16:44] – Fix a few grammar mistakes Istvan Csomortani | ||
---|---|---|---|
Line 4: | Line 4: | ||
The [[adi> | The [[adi> | ||
- | The input clamp protection circuitry can tolerate voltages up to ±20 V. The [[adi> | + | The input clamp protection circuitry can tolerate voltages up to ±20 V. The [[adi> |
- | Each device contains analog input clamp protection, a dual, 16-bit charge redistribution successive approximation analog-to-digital converter (ADC), a flexible digital filter, a 2.5 V reference and reference buffer, and high speed serial and parallel interfaces. | + | Each device contains analog input clamp protection, a dual, 16-bit charge redistribution successive approximation analog-to-digital converter (ADC), a flexible digital filter, a 2.5 V reference and reference buffer, and high-speed serial and parallel interfaces. |
Applications: | Applications: | ||
- | * Power line monitoring | + | * Powerline |
* Protective relays | * Protective relays | ||
* Multiphase motor control | * Multiphase motor control | ||
Line 28: | Line 28: | ||
==== Required software ==== | ==== Required software ==== | ||
- | * We' | + | * We' |
* An UART terminal (Tera Term/ | * An UART terminal (Tera Term/ | ||
Line 42: | Line 42: | ||
* all the control pins of the device are driven by GPIO's | * all the control pins of the device are driven by GPIO's | ||
- | In order to build the HDL design the user have to go through the following steps: | + | In order to build the HDL design the user has to go through the following steps: |
- Confirm that you have the right tools (see [[https:// | - Confirm that you have the right tools (see [[https:// | ||
- | - Clone the HDL github | + | - Clone the HDL GitHub |
- Choose the required interface (see caption **Switching between interface types**) | - Choose the required interface (see caption **Switching between interface types**) | ||
- Build the project (see https:// | - Build the project (see https:// | ||
Line 50: | Line 50: | ||
==== Switching between interface types ==== | ==== Switching between interface types ==== | ||
- | Before power-up the board, the user has to choose the required device interface and setup, in function of the required interface mode some hardware modification needs to be done on the board and/ | + | Before power-up the board, the user has to choose the required device interface and setup, in function of the required interface mode some hardware modification needs to be done on the board and/ |
1) In case of the **SERIAL** interface: | 1) In case of the **SERIAL** interface: | ||
Line 184: | Line 184: | ||
===== Create the SDK Project ===== | ===== Create the SDK Project ===== | ||
- | To run the application the user have to create | + | To run the application the user has to create |